xWRL1432 MMWAVE-L-SDK  05.03.00

Detailed Description

HWA Paramset Config for Output Formatter/Destination block.

HWA paramset config parameters for the Output Formatter/Destination block inside HWA_ParamConfig which is used with the HWA_ConfigParamSet() call.

Data Fields

uint16_t dstAddr
 
uint16_t dstAcnt
 
int16_t dstAIdx
 
int16_t dstBIdx
 
uint8_t dstRealComplex
 
uint8_t dstWidth
 
uint8_t dstSign
 
uint8_t dstConjugate
 
uint8_t dstScale
 
uint16_t dstSkipInit
 

Field Documentation

◆ dstAddr

uint16_t HWA_DestConfig::dstAddr

16 bit value: specifies the starting address of the output samples in the accelerator memory. Value of 0x0000 points to the first byte of accelerator memory and 16-bit value covers the entire address space of the four memories (4x16KB=64 KB) Sets the DSTADDR bits of PARAM1_1

◆ dstAcnt

uint16_t HWA_DestConfig::dstAcnt

12 bit value: specifies the number of samples (minus 1) from the destination memory to process for every iteration. Note: The unit is samples and not bytes. Sets the DSTACNT bits of PARAM1_2

◆ dstAIdx

int16_t HWA_DestConfig::dstAIdx

16 bit value: specifies the number of bytes separating successive samples in the destination memory Sets the DSTAINDX bits of PARAM1_3

◆ dstBIdx

int16_t HWA_DestConfig::dstBIdx

16 bit value: Specifies the number of bytes separating the start address of samples for successive iterations in the destination memory (in bytes, signed value) Sets the DSTBIDX bits in PARAM1_4

◆ dstRealComplex

uint8_t HWA_DestConfig::dstRealComplex

1 bit value: See HWA_SAMPLES_FORMAT macros for correct values. Real or Complex data in the destination memory. Sets the DSTREAL bits in PARAM1_2

◆ dstWidth

uint8_t HWA_DestConfig::dstWidth

1 bit value: See HWA_SAMPLES_WIDTH macros for correct values. 16-bit or 32-bit alignment of data in destination memory. Sets the DST16b32b bits in PARAM1_2

◆ dstSign

uint8_t HWA_DestConfig::dstSign

1 bit value: See HWA_SAMPLES_SIGN macros for correct values. Signed or Unsigned data in the destination memory. This setting is only relevant for dstWidth=0, because that is when sign-extension may be required to convert to internal 24-bit width. Sets the DSTSIGNED bits in PARAM1_2

◆ dstConjugate

uint8_t HWA_DestConfig::dstConjugate

1 bit value: See HWA_FEATURE_BIT macros for correct values. Enable/Disable Conjugation of the output samples. 0: No conjugation 1: Enable conjugation This register only makes sense for dstRealComplex=0. It is useful in conjunction with DSTCONJ to derive an IFFT mode (by conjugating at both output and output) Sets the DSTCONJ bit of PARAM1_2

◆ dstScale

uint8_t HWA_DestConfig::dstScale

4 bit value: Specifies a programmable scaling, via right bit-shift, from 0 bits to 8 bits, for the output samples. Sets the DSTSCAL bits of PARAM1_5 (0-8) The 24-bit complex samples are first converted to 32-bit complex samples by zero padding 8 LSBs. Then, based on the REG_DSTSCAL register value, a right bit-shift of 0 to 8 bits is applied (with MSB sign filling, if required).

◆ dstSkipInit

uint16_t HWA_DestConfig::dstSkipInit

10 bit value: Number of samples to skip in the beginning (for each iteration) before writing samples to the destination memory. Sets the DST_SKIP_INIT bits of PARAM1_5