xWRL1432 MMWAVE-L-SDK  05.03.00

Detailed Description

HWA Debug statistics.

HWA debug - current paramset, loopcount, trigger status - that are output from the statistics block.

Data Fields

uint8_t currentParamSet
 
uint16_t currentLoopCount
 
uint16_t dmaTrigStatus
 
uint8_t dfePingPongStatus
 
uint8_t swTrigStatus
 

Field Documentation

◆ currentParamSet

uint8_t HWA_DebugStats::currentParamSet

Index of the current paramset that is under execution. useful for debug, where parameter-sets can be executed one-by-one using SW trigger mode for each of them. In such a debug, this register indicates which parameter-set is currently waiting for the SW trigger

◆ currentLoopCount

uint16_t HWA_DebugStats::currentLoopCount

the loop count that is presently running

◆ dmaTrigStatus

uint16_t HWA_DebugStats::dmaTrigStatus

indicates whether a trigger was received via DMA trigger method

◆ dfePingPongStatus

uint8_t HWA_DebugStats::dfePingPongStatus

the status of DFE ping-pong trigger

◆ swTrigStatus

uint8_t HWA_DebugStats::swTrigStatus

the status of software trigger