xWRL1432 MMWAVE-L-SDK  05.03.00

Introduction

Macros that define values for symmetric/non-symmetric property of the FFT window.

Macros

#define HWA_FFT_WINDOW_NONSYMMETRIC   ((uint8_t)0U)
 
#define HWA_FFT_WINDOW_SYMMETRIC   ((uint8_t)1U)
 

Macro Definition Documentation

◆ HWA_FFT_WINDOW_NONSYMMETRIC

#define HWA_FFT_WINDOW_NONSYMMETRIC   ((uint8_t)0U)

non-symmetric window for FFT windowing operation

◆ HWA_FFT_WINDOW_SYMMETRIC

#define HWA_FFT_WINDOW_SYMMETRIC   ((uint8_t)1U)

symmetric window for FFT windowing operation Only the first half the window coefficients are expected to be present in the window RAM. The same coefficients are read in reverse direction for the second half.