Empty Project
Introduction
This is an empty project provided for all cores present in the device. User can use this project to start their application by adding more SysConfig modules.
This application does driver and board init and just prints the pass string on the console. In case of the main core, the print is redirected to the UART console. For all other cores, CCS prints are used.
Supported Combinations
Parameter |
Value |
|---|---|
CPU + OS |
mcu-r5fss0-0 nortos |
CPU + OS |
mcu-r5fss0-0 freertos |
CPU + OS |
a53ss0-0 nortos |
CPU + OS |
a53ss0-0 freertos |
CPU + OS |
a53ss0-1 freertos |
CPU + OS |
a53ss1-0 freertos |
CPU + OS |
a53ss1-1 freertos |
CPU + OS |
c75ss0-0 freertos |
CPU + OS |
r5fss0-0 nortos |
CPU + OS |
r5fss0-0 freertos |
Toolchain |
ti-arm-clang |
Toolchain |
arm.gnu.aarch64-none |
Toolchain |
ti-c7000 |
Board |
am62dx-evm |
Example folder |
examples/empty/ |
Steps to Run the Example
When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
Sample Output
Shown below is a sample output when the application is run,
All tests have passed!!
FreeRTOS-AMP Sample Output
Attention
Output from a53ss0-1, a53ss1-0 and a53ss1-1 cores are log to the Shared memory, can be viewed via a53ss0-0 on which log reader is enabled
Shown below is a sample output on UART0 console when the application is run,
All tests have passed on a53_core0 !!
[a530-1] 0.002432s : All tests have passed on a53_core1 !!
[a531-0] 0.002189s : All tests have passed on a53_core2 !!
[a531-1] 0.002101s : All tests have passed on a53_core3 !!