Queue
Features Supported
APIs to create and destroy Queues
APIs to Put element in Queue
APIs to Get element from Queue
APIs to Check if Queue is Empty
Features NOT Supported
NA
Important Usage Guidelines
For creating the Queue application needs to provide the #QueueP_Object and it should not be modified by the applicaion.
A field of type #QueueP_Elem should be placed at the head of client structs passed as Queue Elements to function #QueueP_put.
It is recommended not to place the QueueP Object and QueueP Element objects in stack as they will be accessed by the driver till they are released.
Example Usage
Include the below file to access the APIs,
//! [include]
#include <kernel/dpl/QueueP.h>
//! [include]
#include <kernel/dpl/DebugP.h>
#include <drivers/hw_include/csl_types.h>
//! [define]
/* Define a client structure for the queue elements.
The object of type QueueP_Elem should be placed at the head of the structure. */
Example usage to define Queue Object and Elements:
{
QueueP_Elem lnk;
uint32_t index;
} Test_Queue_Elem;
Test_Queue_Elem elem1, elem2;
QueueP_Object qObj;
//! [define]
void samples()
{
{
//! [queue_usage]
QueueP_Handle handle;
Example to create and use the Queue:
/* Create the Queue. */
handle = QueueP_create(&qObj);
/* Put elements in a Queue. */
QueueP_put(handle, (QueueP_Elem *)&elem1);
QueueP_put(handle, (QueueP_Elem *)&elem2);
/* Get elements from the queue. */
pElem = (Test_Queue_Elem *)QueueP_get(handle);
pElem = (Test_Queue_Elem *)QueueP_get(handle);
/* Typically pElem would be processed by application.
* In sample typecast to void to kill warning
* regarding variable set but not used
*/
API Reference
Defines
-
QueueP_OBJECT_SIZE_MAX
Max size of task object across all OS’s.
Typedefs
-
typedef void *QueueP_Handle
Opaque client reference to an instance of a QueueP.
A QueueP_Handle returned from the QueueP_create represents that instance and is used in the other instance based functions
Functions
-
QueueP_Handle QueueP_create(QueueP_Object *obj)
Function to create a queue.
- Parameters:
obj – [in] Pointer to QueueP_Object.
- Returns:
A QueueP_Handle on success or a NULL on an error
-
int32_t QueueP_delete(QueueP_Handle handle)
Function to delete a queue.
- Parameters:
handle – [in] A QueueP_Handle returned from QueueP_create
- Returns:
Status of the functions
QueueP_OK: Deleted the queue instance
QueueP_FAILURE: Failed to delete the queue instance
-
void *QueueP_get(QueueP_Handle handle)
Function to Get the element at the front of the queue. This function removes an element from the front of a queue and returns it.
- Parameters:
handle – [in] A QueueP_Handle returned from QueueP_create
- Returns:
pointer to the element or pointer to queue itself incase of empty queue
-
int32_t QueueP_put(QueueP_Handle handle, void *elem)
Function to Put an element at end of queue.
- Parameters:
handle – [in] A QueueP_Handle returned from QueueP_create
elem – [in] Pointer to new queue element
- Returns:
Status of the functions
QueueP_OK: Put the element at end of queue
QueueP_FAILURE: Failed to Put the element at end of queue
-
uint32_t QueueP_isEmpty(QueueP_Handle handle)
Function to perform queue empty check.
- Parameters:
handle – [in] A QueueP_Handle returned from QueueP_create
- Returns:
Current state of the Queue
QueueP_NOTEMPTY: queue is not empty
QueueP_EMPTY: queue is empty
-
uint32_t QueueP_getSize(QueueP_Handle handle)
Function to get the number of elements in the queue.
- Parameters:
handle – [in] A QueueP_Handle returned from QueueP_create
- Returns:
Number of elements currently in the queue
-
void *QueueP_peekHead(QueueP_Handle handle)
Function to peek at the head element without removing it.
- Parameters:
handle – [in] A QueueP_Handle returned from QueueP_create
- Returns:
Pointer to the head element, or NULL if the queue is empty
-
struct QueueP_Elem
- #include <QueueP.h>
Opaque QueueP element.
Structure that defines a single queue element and/or a list of queue elements. A field of this type is placed at the head of client structs.