Buildsheet

Introduction

Build Sheet of supported features and modules for this SDK release. The following table lists the supported features and modules for the corresponding category, along with the support status for RTOS on all the cores.

The support status is indicated by the following codes:

Code Note
Yes The feature or module is supported
No The feature or module is not supported
SDKx.y The feature or module will be supported in a future version of the SDK
NA The feature or module is not applicable in the hardware

Software Buildsheet

Category Module SubModule RTOS
on MCU R5
RTOS
on WKUP R5
RTOS
on A53
RTOS
on C7X
System Interconnect Bandwidth regulator No No No No
CBASS auto-clock gating No No No No
Initialization I2C Bootloader Operation No No No No
SPI Bootloader Operation No No No No
QSPI Bootloader Operation NOR NA No NA NA
NAND NA No NA NA
OSPI Bootloader Operation NOR NA Yes NA NA
NAND (1-bit mode) NA No NA NA
NAND (8-bit mode) NA No NA NA
GPMC Bootloader Operation NOR NA No NA NA
NAND NA No NA NA
Ethernet Bootloader Operation NA No NA NA
USB Bootloader Operation Host NA No NA NA
Device NA No NA NA
MMCSD Bootloader Operation SD Card (no UHS) NA Yes NA NA
eMMC NA Yes NA NA
UART Bootloader Operation NA Yes NA NA
Device Configuration Power Supply Modules POK No No No No
POR No No No No
PRG No No No No
PGD No No No No
VTM Yes No No No
PMIC (Power Management IC) Yes NA NA NA
Power MaNAgement Deep Sleep Low Power Mode NA No No No
Deep Sleep LPM Wakeup Events RTC Timer NA No No No
GT Timers NA No No No
WKUP UART NA No No No
I2C NA No No No
MCU GPIO NA No No No
I/O Daisy Chain NA No No No
USB Connect/Disconnect NA No No No
USB Remote Wakeup NA No No No
MCU-Only Low Power Mode NA No No No
Standby Low Power Mode NA No No No
Partial I/O Low Power Mode NA No No No
IO + DDR low power mode NA No No No
Boot-time OPP configurations No No No No
Runtime Power MaNAgement NA No No No
DFS/CPUFreq NA No No No
CPUIdle (A53 WFI) NA No No No
CPUIdle (DDR in Self-Refresh) NA No No No
Interprocessor Communication Mailbox Yes Yes Yes Yes
Spinlock No No No No
Memory Controllers DDR Subsystem (DDRSS) DDR4 No No No No
LPDDR4 No Yes No No
Inline ECC (1bit err) No Yes No No
Inline ECC (mbit err) No No No No
Region-based Address Translation Yes Yes NA NA
Time Sync Time Sync Module (CPTS) No No No No
Timer MaNAger No No No No
Time Sync and Compare Events No No No No
Data Movement Architecture (DMA) Data Movement Subsystem (DMSS) Yes Yes Yes Yes
Peripheral DMA (PDMA) No No No No
RingAcc No No No No
BCDMA Yes Yes Yes Yes
DRU NA NA NA Yes
Packet Streaming Interface Link No No No No
General Connectivity Peripherals (MAIN domain) Multichannel Audio Serial Port (McASP) Input NA No Yes Yes
Output NA No Yes Yes
HDMI Output NA No No No
General-Purpose Interface (GPIO) Yes Yes Yes Yes
Inter-Integrated Circuit (I2C) Controller Yes Yes Yes Yes
Target Yes Yes Yes Yes
Multichannel Serial Peripheral Interface (McSPI) Controller Yes No Yes No
Peripheral Yes No Yes No
Universal Asynchronous Receiver/Transmitter (UART) UART Yes Yes Yes Yes
RS-485 NA No No No
IrDA NA No No No
General Connectivity Peripherals (MCU domain) General-Purpose Interface (GPIO) Yes Yes Yes No
Inter-Integrated Circuit (I2C) Controller Yes Yes Yes Yes
Target No No No No
Multichannel Serial Peripheral Interface (McSPI) Controller Yes No No No
Peripheral No No No No
Universal Asynchronous Receiver/Transmitter (UART) UART Yes Yes Yes Yes
RS-485 No No No No
IrDA No No No No
General Connectivity Peripherals (WKUP domain) Inter-Integrated Circuit (I2C) Controller Yes Yes Yes No
Target NA No No No
Universal Asynchronous Receiver/Transmitter (UART) UART NA Yes No No
RS-485 NA No No No
IrDA NA No No No
High-speed Serial Interfaces Gigabit Ethernet Switch (CPSW3G) Switch No No No No
EndPoint No No No No
TSN No No No No
TSN - VLAN No No No No
Universal Serial Bus Subsystem (USBSS) Host 3.1 No No No No
Device 3.1 No No No No
Host 2.0 No No No No
Device 2.0 No No No No
Memory Interfaces Flash Subsystem (FSS) No No No No
Quad Serial Peripheral Interface (QSPI) NOR No No No No
NAND No No No No
Octal Serial Peripheral Interface (OSPI) NOR Yes Yes Yes No
NAND No No No No
Expanded Serial Peripheral Interface (xSPI) No No No No
General-Purpose Memory Controller (GPMC) FPGA No No No No
NAND No No No No
NOR No No No No
etc. No No No No
Error Location Module (ELM) No No No No
Multimedia Card Secure Digital (MMCSD) Interface SD Card No Yes Yes No
eMMC No Yes Yes No
Industrial & Control Interfaces Controller Area Network (MCAN) - MAIN domain CAN No No Yes No
CAN FD No No Yes No
Controller Area Network (MCAN) - MCU domain CAN Yes No No No
CAN FD Yes No No No
Enhanced Capture (ECAP) Module Capture No No No No
PWM No No Yes Yes
Enhanced Pulse Width Modulation (EPWM) Module No No Yes Yes
Enhanced Quadrature Encoder Pulse (EQEP) Module No No Yes No
Camera Subsystem Camera Streaming Interface Receiver (CSI_RX_IF) NA No No No
MIPI D-PHY Receiver (DPHY_RX) NA No No No
Multiple Camera NA No No No
OV2312 RGB + IR sensor NA No No No
iMX219 sensor NA No No No
Timer Modules Global Timebase Cunter (GTC) No No No No
Windowed Watchdog Timer (WWDT) - MAIN domain No No Yes No
Windowed Watchdog Timer (WWDT) - MCU domain Yes No No No
Windowed Watchdog Timer (WWDT) - WKUP domain No Yes No No
Real-Time Clock (RTC) Yes Yes No No
Timers - MAIN domain Timer NA No Yes Yes
Capture NA No No No
Compare NA No No No
PWM NA No No No
Timers - MCU domain Timer Yes No No No
Capture No No No No
Compare No No No No
PWM No No No No
Timers - WKUP domain Timer NA Yes No No
Capture NA No No No
Compare NA No No No
PWM NA No No No
Internal Diagnostics Modules Dual Clock Comparator (DCC) Yes No No No
Error Signalling Module (ESM) Yes No No No
Memory Cyclic Redundancy Check (MCRC) Controller Yes No No No
SDL Driver Porting Layer(SDL DPL) Yes No No No
RTI(WWDG) Yes No No No
Voltage and Thermal Management(VTM) Yes No No No
Interconnect Isolation Gasket(STOG) Yes No No No
Interconnect Isolation Gasket(MTOG) Yes No No No
Power OK(POK) Yes No No No
PBIST(Built In Self Test) Yes No No No
ECC Aggregator Yes No No No
On-Die Temperature sensor NA No No No
On-Chip Debug NA NA NA NA
Crypto Accelerator (SA3UL) Advanced Encryption Standard (AES) AES-CBC NA No Yes No
AES-ECB NA No Yes No
SHA/MD5 Crypto Hardware-Accelerated Module (SHA/MD5) SHA-256 NA No Yes No
SHA-512 NA No Yes No
True Random Number Generator (TRNG) NA No Yes No
Board Specific (AM62D EVM) Audio Codec DAC NA No NA No
ADC NA No NA No