MCASP

The Multi Channel Audio Seiral Peripheral (MCASP) driver is a generic, full-duplex driver that transmits and receives data using the MCASP interface. This is specially designed to transmit and receive the digital audio data.

Features Supported

  • Interrupt mode operation

  • DMA mode operation

  • Internal Loopback

  • Transmit and Receive in TDM format with multi-serializer, multi-slot support.

  • SysConfig support for driver parameter configuration and initialization.

  • Different audio buffer formats for application

SysConfig Features

Attention

The instances for McASP needs to be selected the same for serializers for the instance. Syscfg will automatically assign different instances for all and user will be required to assign same instance and choose to ignore the warning.

Note

It is strongly recommend to use SysConfig where it is available instead of using direct SW API calls. This will help simplify the SW application and also catch common mistakes early in the development cycle.

Features NOT Supported

  • Transmit in DIT mode

  • Burst Mode

Usage Overview

Key Careabouts in Driver Usage

Note

The changes pulled in for the driver starting release 10.0 requires some changes in the Driver usage from application

  • All transactions submitted from the applications must be of the same size.

    • The TX and RX can be of seperate size.

  • The Loopjob buffer size can be configured from the sysconfig.

  • Application can provide an external buffer for loopjob buffer from Sysconfig

    • This enables application to provide the transaction buffer itself as loopjob

  • #MCASP_stopTransferRx() and #MCASP_stopTransferTx() are blocking calls that should not be called from an ISR context.

API Sequence

To use the MCASP driver to send data over the MCASP interface, the application calls the following APIs:

  • #MCASP_init(): Initialize the MCASP driver.

  • #MCASP_open(): Open an instance of the MCASP driver

  • #MCASP_submitRx(): Submit buffers to MCASP driver for reception

  • #MCASP_submitTx(): Submit buffers to MCASP driver for transmission

  • #MCASP_startTransferRx(): Start MCASP receive.

  • #MCASP_startTransferTx(): Start MCASP transmit.

  • #MCASP_stopTransferRx(): Stop MCASP receive.

  • #MCASP_stopTransferTx(): Stop MCASP transmit.

  • #MCASP_withdrawRx(): withdraw buffers submitted to driver for reception

  • #MCASP_withdrawTx(): withdraw buffers submitted to driver for transmission

  • #MCASP_close(): De-initialize the MCASP instance.

  • #MCASP_deinit(): De-Initialize the MCASP driver.

MCASP migration guide 11.02 to 12.00

Note

This section highlights key features that have changed or got added from 11.02 to 12.00 SDK.

Note

Different Audio Buffer Formats feature was added.

Note

For multi-serializer RX/TX, you should select multi-serializer audio buffer formats only.

Supported Application Audio Buffer Formats

The McASP driver provides various buffer formats for sending the data to/from the audio device. The differences between these formats arise from the way the audio samples are collected from various serializers and their timeslots and arranged in the system’s memory. This way the application can choose to run audio processing algorithms over the data without the need for re-arranging those data every frame. This section provides an overview of the various formats . In the explanatory diagrams in each section, McASP controller recieves samples in frame intervals denoted by t1,t2..tn. The McASP driver collects these and arranges those samples in the memory in various formats in to the host’s System memory. We have chosen 32 bit samples and 32-bit word addresses throughout for simplicity.

  • 1-Serializer Multi-Slot Interleaved: This is applicable if multiple slots are used with one serializer. The samples from the different timeslots are stored interleaved in the memory as below. Different timeslots’ samples are denoted by different colors and are labelled t1,t2..tn according to the time they arrive at the serializer.

1-Serializer Multi-Slot Interleaved

1-Serializer Multi-Slot Interleaved Buffer Format

  • 1-Serializer Multi-Slot NonInterleaved: This is applicable if multiple slots are used with one serializer. The samples from the different timeslots are grouped together on the basis of the timeslot and stored in the memory as shown below. Different timeslots’ samples are denoted by different colors and are labelled t1,t2..tn according to the time they arrive at the serializer.

1-Serializer Multi-Slot NonInterleaved

1-Serializer Multi-Slot NonInterleaved Buffer Format

  • Multi-Serializer Multi-Slot Interleaved Type1: This is applicable if multiple serializers are used and each serializer containing multiple timeslots. The samples are stored in the memory interleaved based on serializer and timeslots as shown below. In this example, there are 3 serializers and 2 timeslots per serializers whose samples are noted by Ln (left) and Rn (right). Different serializers’ samples are denoted by different colors.

Multi-Serializer Multi-Slot Interleaved Type1

Multi-Serializer Multi-Slot Interleaved Type1 Buffer Format

  • Multi-Serializer Multi-Slot Interleaved Type2: This is applicable if multiple serializers are used and each serializer containing multiple timeslots. The samples are grouped based on the serializer and within one serializer, the timeslots are interleaved as shown below. In this example, there are 3 serializers and 2 timeslots per serializers whose samples are noted by Ln (left) and Rn (right).Different serializers’ samples are denoted by different colors.

Multi-Serializer Multi-Slot Interleaved Type2

Multi-Serializer Multi-Slot Interleaved Type2 Buffer Format

  • Multi-Serializer Multi-Slot NonInterleaved: This is applicable if multiple serializers are used and each serializer containing multiple timeslots. The samples are grouped based on the serializer and slot within one serializer, the timeslots are interleaved as shown below. In this example, there are 3 serializers and 2 timeslots per serializers whose samples are noted by Ln (left) and Rn (right).Different serializers’ samples are denoted by different colors.

Multi-Serializer Multi-Slot NonInterleaved

Multi-Serializer Multi-Slot NonInterleaved Buffer Format

Loopjob Configuration

Mcasp driver allows loopjob enabled/disabled configuration to handle delayed application buffer submission at run time. Loopjob is a default buffer that gets transmitted / received into if the application fails to submit the buffers in time. When loopjob is disabled the last 2 application buffers will be re programmed and re used. The application callback corresponding to the re programmed buffers is not called.

  • Loopjob buffer is programmed in sys config. Sys config will define a uint8_t array and initialize it to 0.

  • Application can access the buffer and optionally initialize the data.

  • If the loopjob buffer is programmed, after sending the full loopjob buffer next submitted buffer is programmed.

Buffer Queuing

  • The application buffers need to be programmed before starting the transfer.

  • If the loopjob is enabled application can start without queuing any buffers, Driver will work with the loopjob buffers till application queues the actual buffers.

  • If loopjob is disabled at least 2 buffers should be queued before starting the mcasp transfer. New buffer will be programmed in the interrupt callback corresponding to current transfer. the application is expected to submit the new buffer before that else the same buffer is re programmed, so it is recommended to start the transfer with at least 3 buffers queued.

Example Usage

Include the below file to access the APIs

#include <drivers/mcasp.h>

Instance Open Example

    MCASP_OpenParams     mcaspParams;
    MCASP_openParamsInit(&mcaspParams); /* Initialize mcasp parameters */
    mcaspParams.edmaInst  = 0;
    mcaspParams.edmaInst     = CONFIG_EDMA0,
    mcaspParams.transferMode = MCASP_TRANSFER_MODE_DMA,
    mcaspParams.txCallbackFxn = mcasp_loopback_txcb,
    mcaspParams.rxCallbackFxn = mcasp_loopback_rxcb,

    gMcaspHandle = MCASP_open(CONFIG_MCASP0, &mcaspParams);
    DebugP_assert(gMcaspHandle != NULL);

Instance Close Example

    MCASP_close(gMcaspHandle);

Start McASP Transfer Example

    MCASP_Transaction   txnTx[APP_MCASP_MSG_COUNT] = {0};
    MCASP_Transaction   txnRx[APP_MCASP_MSG_COUNT] = {0};
    uint8_t mcaspTxBuffer[APP_MCASP_MSG_COUNT][APP_MCASP_MSGSIZE];
    uint8_t mcaspRxBuffer[APP_MCASP_MSG_COUNT][APP_MCASP_MSGSIZE];
    uint32_t i;

    for (i = 0U; i < APP_MCASP_MSG_COUNT; i++)
    {
        txnTx[i].buf = (void*) &mcaspTxBuffer[i][0];
        txnTx[i].count = APP_MCASP_MSGSIZE/4;
        txnTx[i].timeout = 0xFFFFFF;
        MCASP_submitTx(gMcaspHandle, &txnTx[i]);
    }
    for (i = 0U; i < APP_MCASP_MSG_COUNT; i++)
    {
        txnRx[i].buf = (void*) &mcaspRxBuffer[i][0];
        txnRx[i].count = APP_MCASP_MSGSIZE/4;
        txnRx[i].timeout = 0xFFFFFF;
        MCASP_submitRx(gMcaspHandle,  &txnRx[i]);
    }

    MCASP_startTransferRx(gMcaspHandle);
    MCASP_startTransferTx(gMcaspHandle);

Stop McASP Transfer Example

    MCASP_stopTransferTx(gMcaspHandle);
    MCASP_stopTransferRx(gMcaspHandle);

    /* withdraw the buffers submitted to driver. */
    {
        MCASP_Transaction *transaction;
        do {
            transaction = MCASP_withdrawRx(gMcaspHandle);
        }while (transaction != NULL);
        do {
            transaction = MCASP_withdrawTx(gMcaspHandle);
        }while (transaction != NULL);
    }

MCASP Callback Functions

void mcasp_loopback_txcb (MCASP_Handle handle,
                          MCASP_Transaction *transaction)
{
    /* Sample Tx callback function. Submit the same buffer again to driver. */
    MCASP_submitTx(handle, transaction);
}

void mcasp_loopback_rxcb (MCASP_Handle handle,
                          MCASP_Transaction *transaction)
{
    /* Sample Rx callback function. Submit the same buffer again to driver. */
    MCASP_submitRx(handle, transaction);
}

SysConfig migration guide 11.01 to 11.02

Note

This section highlights key features that have changed or got added from 11.01 to 11.02 SDK

AUX clock selection

  • This version of SDK (11.02) gives the configurability to choose between different sources of AUXCLK

MCASP AUX Clock Selection

MCASP AUX Clock Selection

  • The specific option for AUXCLK will vary from device to device. View long description in Syscfg view for more details on the AUXCLK options to select from.

  • The frequency for the configurable AUX clock options can be choosen at a global level as this will be applicable across all instances of MCASP.

MCASP AUX Clock Frequency

MCASP AUX Clock Frequency

  • Some option in the AUX clock selections might expect the aux clock to be supplied externally to the SoC. Refer the TRM of the specific device to check if the clock is supplied externally or generated interally.

  • When using an internally generated auxiliary clock source, not all frequency values are achievable due to hardware limitations. If the user-specified frequency cannot be generated, the system will throw a runtime error.

Clock Divider Configurability

  • This version of SDK (11.02) gives configurability of the High Clock Divider (HCLK Divider), and the BCLK divider.

MCASP Clock Divider Configuration

MCASP Clock Divider Configuration

  • The “Re-Calculate” button can be used to calculate the divider values that would result in the closest FSYNC value required.

  • The “Apply” button needs to be pressed to view the frequencies for any change in the Sysconfig GUI that have resulted in a change of frequencies.

  • Press the “Apply” button to update the frequency information displayed in the Syscfg GUI for all configuration parameters that affect frequency settings.

  • User have to ensure all the frequencies that is displayed is as expected in the system after pressing “Apply”.

  • User can adjust the Divider values and press the “Apply” button to achieve any specific clock frequencies.

API Reference

MCASP Driver API/interface file.

Transfer Status Code

Status codes that are set by the MCASP driver

MCASP_TRANSFER_STATUS_COMPLETED

I/O completed successfully.

MCASP_TRANSFER_STATUS_STARTED

I/O queued and pending.

MCASP_TRANSFER_STATUS_CANCELLED

I/O cancelled. Returned by incomplete read or write requests.

MCASP_TRANSFER_STATUS_FAILED

Generic failure condition.

MCASP_TRANSFER_STATUS_TIMEOUT

I/O timeout occurred.

McASP Transfer Mode

MCASP_TRANSFER_MODE_POLLING

MCASP read/write APIs blocks execution. This mode can only be used when called within a Task context.

MCASP_TRANSFER_MODE_INTERRUPT

MCASP read/write APIs does not block code execution and will call a MCASP_TxCallbackFxn or MCASP_RxCallbackFxn. This mode can be used in a Task, Swi, or Hwi context.

MCASP_TRANSFER_MODE_DMA

MCASP read/write APIs does not block code execution and will use DMA for transfers.

McASP Operating Mode

OPerating Modes that are supported by the MCASP driver

MCASP_OPMODE_MASTER

I/O completed successfully.

MCASP_OPMODE_SLAVE

I/O queued and pending.

MCASP Channel Direction

the channel modes supported by Mcasp

MCASP_CHANNEL_INPUT

MCASP Channel will receive data.

MCASP_CHANNEL_OUTPUT

MCASP Channel will transmit data.

MCASP_CHANNEL_INOUT

McASP channel transmits & recieves data.

MCASP Driver State

Mcasp driver state enums used to track the driver state

MCASP_DRIVER_STATE_DELETED
MCASP_DRIVER_STATE_CREATED
MCASP_DRIVER_STATE_INITIALIZED
MCASP_DRIVER_STATE_OPENED
MCASP_DRIVER_STATE_CLOSED
MCASP_DRIVER_STATE_DEINITIALIZED
MCASP_DRIVER_STATE_POWERED_DOWN
MCASP_DRIVER_STATE_PWRM_SUSPEND

MCASP Serializer Status

Enumeration for serializer status

MCASP_SERIALIZER_STATUS_FREE
MCASP_SERIALIZER_STATUS_XMT
MCASP_SERIALIZER_STATUS_RCV

MCASP Channel Mode

Enumeration for channel mode

MCASP_CHANNEL_MODE_FREE
MCASP_CHANNEL_MODE_XMT_DIT
MCASP_CHANNEL_MODE_XMT_TDM
MCASP_CHANNEL_MODE_RCV

MCASP Word Select

Enumerated constant for selecting MSB/LSB word in the slot bits

MCASP_WORD_SELECT_LSW
MCASP_WORD_SELECT_MSW

Enumerated constants to specify the supported buffer formats.

Interleaved and non-interleaved is standard format, this enumeration captures the standard and custom data formats.

MCASP_AUDBUFF_FORMAT_1SER_MULTISLOT_NON_INTERLEAVED

This is used for transfer of data on a single serializer with multiple slots.please note that the slot data is not interleaved in this format. TDM with single serializer and slots > 1 uses this format.

MCASP_AUDBUFF_FORMAT_1SER_MULTISLOT_INTERLEAVED

This is used for transfer of data on a single serializer with multiple slots.please note that the slot data is interleaved in this format. TDM with single serializer and slots > 1 uses this format.

MCASP_AUDBUFF_FORMAT_MULTISER_MULTISLOT_SEMI_INTERLEAVED_1

This is used for transfer of data with multiple serializers and also multiple slots enabled.please note that the serializer data is interleaved in this format. The slot data is also interleaved Refer to the user guide to view the sample data format.

MCASP_AUDBUFF_FORMAT_MULTISER_MULTISLOT_SEMI_INTERLEAVED_2

This is used for transfer of data with multiple serializers and also multiple slots enabled.please note that the serializer data is NOT interleaved in this format. The slot data is interleaved. Refer to the user guide to view the sample data format.

MCASP_AUDBUFF_FORMAT_MULTISER_MULTISLOT_NON_INTERLEAVED

This is used for transfer of data with multiple serializers and also multiple slots enabled.please note that niether serializer data nor slot data is interleaved in this format. Refer to the user guide to view the sample data format.

Transmit State for McASP transfer

Enumeration for McASP transmit state

MCASP_TRANSMIT_STATE_TX_RESET
MCASP_TRANSMIT_STATE_TX_FLUSH
MCASP_TRANSMIT_STATE_LOAD_INIT_BUFFER
MCASP_TRANSMIT_STATE_RELEASE_FROM_RESET
MCASP_TRANSMIT_STATE_WAIT_EVENT
MCASP_TRANSMIT_STATE_PROCESS_EVENT
MCASP_TRANSMIT_STATE_LOAD_ACTIVE_BUFFER
MCASP_TRANSMIT_STATE_DONE
MCASP_TRANSMIT_STATE_SPIN_IDLE
MCASP_TRANSMIT_STATE_ERROR
MCASP_TRANSMIT_STATE_EXIT

Receive State for McASP transfer

Enumeration for McASP receive state

MCASP_RECEIVE_STATE_RX_RESET
MCASP_RECEIVE_STATE_RX_FLUSH
MCASP_RECEIVE_STATE_RELEASE_FROM_RESET
MCASP_RECEIVE_STATE_WAIT_EVENT
MCASP_RECEIVE_STATE_PROCESS_EVENT
MCASP_RECEIVE_STATE_DONE
MCASP_RECEIVE_STATE_SPIN_IDLE
MCASP_RECEIVE_STATE_ERROR
MCASP_RECEIVE_STATE_EXIT

Defines

MCASP_GBLCTL_TIMEOUT

The time to try (in Msec) before the GBLCTL register setting timeouts if the setting/resetting is done in a context other than a task this will be used as a retry count rather than the MSec timeout.

MCASP_DATA_TIMEOUT

The time to try (in Msec) to check the XDTATA/RDATA flags in status register. if the setting/resetting is done in a context other than a task this will be used as a retry count rather than the MSec timeout.

MCASP_RESET

McASP macros for enable/reset.

MCASP_ENABLE
MCASP_DISABLE
MCASP_REG_OFFSET
MCASP_DIR_OUT
MCASP_DIR_IN
MCASP_TRPD_INVALID_PTR

Typedefs

typedef void *MCASP_Handle

A handle that is returned from a MCASP_open() call.

typedef void (*MCASP_TxCallbackFxn)(MCASP_Handle handle, MCASP_Transaction *transaction)

The definition of a callback function used by the MCASP driver when used in Callback Mode.

Param handle:

MCASP_Handle

Param transaction*:

Pointer to a MCASP_Transaction

typedef void (*MCASP_RxCallbackFxn)(MCASP_Handle handle, MCASP_Transaction *transaction)

Functions

void MCASP_init(void)

This function initializes the MCASP module.

void MCASP_deinit(void)

This function de-initializes the MCASP module.

static inline void MCASP_openParamsInit(MCASP_OpenParams *openPrms)

Function to initialize the MCASP_OpenParams struct to its defaults.

Parameters:

openPrms – Pointer to MCASP_OpenParams structure for initialization

MCASP_Handle MCASP_open(uint32_t index, const MCASP_OpenParams *openParams)

This function opens a given MCASP peripheral.

See also

MCASP_init()

See also

MCASP_close()

Parameters:
  • index – Index of config to use in the MCASP_Config array

  • openParams – Pointer to parameters to open the driver with

Pre:

MCASP controller has been initialized using MCASP_init()

Returns:

A MCASP_Handle on success or a NULL on an error or if it has been opened already

void MCASP_close(MCASP_Handle handle)

Function to close a MCASP peripheral specified by the MCASP handle.

See also

MCASP_open()

Parameters:

handle – MCASP_Handle returned from MCASP_open()

Pre:

MCASP_open() has to be called first

MCASP_Handle MCASP_getHandle(uint32_t index)

This function returns the handle of an open MCASP Instance from the instance index.

See also

MCASP_init()

See also

MCASP_open()

Parameters:

index – Index of config to use in the MCASP_Config array

Pre:

MCASP controller has been opened using MCASP_open()

Returns:

A MCASP_Handle if it has been opened already or NULL otherwise

int32_t MCASP_submitTx(MCASP_Handle handle, MCASP_Transaction *txn)

Function to submit the buffer to McASP driver for transmission. Transaction object is held by the driver till it is returned in the callback function. It is recommended not to allocate the transaction object in stack to avoid corruption.

Parameters:
Returns:

Success/Failure for configuration

int32_t MCASP_submitRx(MCASP_Handle handle, MCASP_Transaction *txn)

Function to submit the buffer to McASP driver for reception. Transaction object is held by the driver till it is returned in the callback function. It is recommended not to allocate the transaction object in stack to avoid corruption.

Parameters:
Returns:

Success/Failure for configuration

MCASP_Transaction *MCASP_withdrawTx(MCASP_Handle handle)

Function to withdraw the buffer submitted to McASP driver for transmission. This should be called after the MCASP_stopTransferTx. These buffers are not transmitted.

Parameters:

handle – MCASP_Handle

Returns:

Pointer to a MCASP_Transaction. NULL if no more buffers are there with driver.

MCASP_Transaction *MCASP_withdrawRx(MCASP_Handle handle)

Function to withdraw the buffer submitted to McASP driver for reception. This should be called after the MCASP_stopTransferRx. These buffers are not transmitted.

Parameters:

handle – MCASP_Handle

Returns:

Pointer to a MCASP_Transaction. NULL if no more buffers are there with driver.

int32_t MCASP_startTransferTx(MCASP_Handle handle)

Function to start McASP transmission.

Parameters:

handle – MCASP_Handle

Returns:

Success/Failure for configuration

int32_t MCASP_startTransferRx(MCASP_Handle handle)

Function to start McASP reception.

Parameters:

handle – MCASP_Handle

Returns:

Success/Failure for configuration

int32_t MCASP_stopTransferTx(MCASP_Handle handle)

Function to stop McASP transmission.

Caution: This API is blocking. Hence cannot be called from ISR context!!

Parameters:

handle – MCASP_Handle

Returns:

Success/Failure for configuration

int32_t MCASP_stopTransferRx(MCASP_Handle handle)

Function to stop McASP reception.

Caution: This API is blocking. Hence cannot be called from ISR context!!

Parameters:

handle – MCASP_Handle

Returns:

Success/Failure for configuration

int32_t MCASP_setTxTxnCount(MCASP_Handle handle, uint32_t txnCount)

Function to set the Tx transaction count.

Caution: This API should be called before MCASP_startTransferTx. User needs to ensure the transaction count is matching with the loopjob size.

Parameters:
  • handle – MCASP_Handle

  • txnCount – Tx transaction count

Returns:

Success/Failure for configuration

int32_t MCASP_setRxTxnCount(MCASP_Handle handle, uint32_t txnCount)

Function to set the Rx transaction count.

Caution: This API should be called before MCASP_startTransferRx. User needs to ensure the transaction count is matching with the loopjob size.

Parameters:
  • handle – MCASP_Handle

  • txnCount – Rx transaction count

Returns:

Success/Failure for configuration

int32_t MCASP_getTxQueueStatus(MCASP_Handle handle, MCASP_QueueStatus *qStatus)

Function to get current Tx queue status.

Returns information about pending Tx transactions including number of buffers and total samples awaiting transmission. Used for presentation time calculation.

Parameters:
  • handle – MCASP_Handle

  • qStatus – Pointer to MCASP_QueueStatus to receive queue information

Returns:

Success (0) or error code if handle or pointer is invalid

int32_t MCASP_getTxPresentationTime(MCASP_Handle handle, MCASP_PresentationTime *pTime)

Compute the TX presentation time offset.

Returns the time in microseconds until the first sample currently queued will reach the TDM TX pins. This accounts for all bytes sitting in the software queues (reqQueue + curentQueue) plus any bytes already handed to the DMA but not yet transmitted.

Parameters:
  • handle – MCASP_Handle returned by MCASP_open

  • pTime – Pointer to MCASP_PresentationTime; on success receives:

    • offsetUs &#8212; microseconds of audio data pending

    • samplesRemaining &#8212; 32-bit word count pending in software queues

Returns:

SystemP_SUCCESS, or SystemP_FAILURE if any argument is NULL or the DMA statistics query fails

Variables

MCASP_Config gMcaspConfig[]

Externally defined driver configuration array.

uint32_t gMcaspConfigNum

Externally defined driver configuration array size.

struct MCASP_Transaction
#include <mcasp.h>

Data structure used with transfer call.

Public Members

QueueP_Elem qElem

[IN] This should be the first parameter. this is the queue element used by driver.

void *buf

[IN] void * to a buffer with data to be transferred . This parameter can’t be NULL

uint32_t count

[IN/OUT] Number of bytes for this transaction. This is input incase of read/write call and on API return this represents number of bytes actually read by the API

uint32_t timeout

[IN] Timeout for this transaction in units of system ticks

int32_t status

[OUT] MCASP_TransferStatus code

void *args

[IN] Argument to be passed to the callback function

struct MCASP_QueueStatus
#include <mcasp.h>

Queue status structure for MCASP presentation time tracking.

This structure contains information about pending transactions in the MCASP queue, used for calculating presentation time and latency.

Public Members

uint32_t numPendingBufs

Number of buffers in queue

uint32_t totalPendingSamples

Total samples across all pending buffers

uint32_t sampleSize

[IN] Bytes per sample used to compute totalPendingSamples; equals slot size for single-channel or slotCount x slot size for a TDM frame;

struct MCASP_PresentationTime
#include <mcasp.h>

Presentation time structure for MCASP timing calculations.

This structure contains timing information for when samples will be transmitted on the TDM pins, used for accurate audio synchronization.

Public Members

uint32_t offsetUs

Microseconds until next sample transmission

uint32_t samplesRemaining

Samples until start of transmission

struct MCASP_ClockConfig
#include <mcasp.h>

Hardware setup data clock structure.

Public Members

uint32_t aClk

Clock details ACLK(R/X)CTL

uint32_t hiClk

High clock details AHCLK(R/X)CTL

uint32_t clkChk

Configures RX/TX CLK fail detect

uint8_t isHClkExt

Flag for if HCLK is from external source

uint32_t hClkExt

External HCLK (TX/RX) source

struct MCASP_GlobalConfig
#include <mcasp.h>

Hardware setup global structure.

Public Members

uint32_t pfunc

Pin function register

uint32_t pdir

Pin direction register

uint32_t gblCtl

Global control register - GBLCTL

uint32_t ditCtl

whether McASP operates in DIT mode

uint32_t dlbCtl

Digital loopback mode setup

uint32_t amute

Mute control register - AMUTE

uint32_t serSetup[16u]

Setup serializer control register

struct MCASP_FifoConfig
#include <mcasp.h>

Hardware fifo setup structure.

Public Members

uint32_t fifoCtl

FIFO control register

uint32_t fifoStatus

FIFO status register (read only)

struct MCASP_DataConfig
#include <mcasp.h>

Hardware setup data structure.

Public Members

uint32_t mask

To mask or not to mask - R/XMASK

uint32_t fmt

Format details as per - R/XFMT

uint32_t frSyncCtl

Configure the rcv/xmt frame sync

uint32_t tdm

Specifies which TDM slots are active

uint32_t intCtl

Controls generation of interrupts

uint32_t stat

Status register (controls writable fields of STAT register)-R/XSTAT

uint32_t evtCtl

Event control register - R/XEVTCTL

MCASP_ClockConfig clk

Clock settings for rcv/xmt

MCASP_FifoConfig fifoCfg

Clock settings for rcv/xmt

struct MCASP_HwConfig
#include <mcasp.h>

Hardware setup structure.

Public Members

MCASP_GlobalConfig gbl

Value to be loaded in module setup regs

MCASP_DataConfig rx

Receiver settings

MCASP_DataConfig tx

Transmitter settings

struct MCASP_DmaChConfig
#include <mcasp.h>

Public Members

void *txChHandle

UDMA channel tx handle

void *rxChHandle

UDMA channel rx handle

void *cqTxEvtHandle

UDMA cq tx event handle

void *cqRxEvtHandle

UDMA cq rx event handle

void *txTrpdMem

UDMA TX TRPD memory pointers

void *rxTrpdMem

UDMA RX TRPD memory pointers

uint32_t trpdMemSize

Size of TR PD memory

void *txRingMem

UDMA TX Ring memory pointers

void *rxRingMem

UDMA RX Ring memory pointers

void *txCbParams

UDMA TX callback params

void *rxCbParams

UDMA RX callback params

uint32_t rxEvtNum

UDMA Event number used for Rx

uint32_t txEvtNum

UDMA Event number used for Tx

uint32_t isOpen

Flag to indicate whether the DMA instance is opened already

struct MCASP_OpenParams
#include <mcasp.h>

MCASP Parameters.

MCASP Parameters are used to with the MCASP_open() call. Default values for these parameters are set using MCASP_openParamsInit().

If NULL is passed for the parameters, MCASP_open() uses default parameters.

Public Members

uint32_t transferMode

Polling, Blocking or Callback mode.

uint8_t txBufferFormat

Audio buffer format for app tx buffer

uint8_t rxBufferFormat

Audio buffer format for app rx buffer

uint8_t txSerUsedCount

Number of allocated transmit serializers

uint8_t rxSerUsedCount

Number of allocated receive serializers

uint8_t *txSerUsedArray

POinter to the array of allocated transmit serializer indices

uint8_t *rxSerUsedArray

POinter to the array of allocated receive serializer indices

uint8_t txSlotCount

Number of slots for trasnmit operation

uint8_t rxSlotCount

Number of slots for receive operation

MCASP_TxCallbackFxn txCallbackFxn

Read callback function pointer

MCASP_RxCallbackFxn rxCallbackFxn

Write callback function pointer

uint32_t txLoopjobEnable

Flag to enable loopjob for transmit

uint8_t *txLoopjobBuf

Loopjob buffer address for transmit

uint32_t txLoopjobBufLength

Loopjob buffer length for transmit

uint32_t rxLoopjobEnable

Flag to enable loopjob for receive

uint8_t *rxLoopjobBuf

Loopjob buffer address for receive

uint32_t rxLoopjobBufLength

Loopjob buffer length for receive

MCASP_DmaChConfig *dmaChCfg

DMA channel config

void *mcaspDmaDrvObj

BCDMA Handle

uint8_t skipDriverOpen

Flag to indicate if driver open should be skipped

struct MCASP_HwIntConfig
#include <mcasp.h>

McASP Interrupt structures.

Public Members

uint32_t intrNum

Receive interrupt number

uint16_t evntNum

Receive event number (Used for C7x only)

uint8_t intrPriority

Interrupt priority

struct MCASP_TransferObj
#include <mcasp.h>

McASP Transfer Data structure stored in driver object.

Public Members

uint32_t inProgress

Flag to indicate if the transfer is ongoing

uint32_t state

MCASP Transfer State

int32_t status

MCASP_Transfer Status

uint32_t count

MCASP Transfer count

uint8_t slotCount

number of slots in transaction

uint8_t slotIndex

current slot index in ongoing transfer

uint8_t frameCount

number of frames in transaction

uint8_t frameIndex

current frame index in ongoing transfer

uint8_t serCount

Number of allocated serializers

uint8_t *serArray

Pointer to the array of allocated serializer indices

uint8_t bufferFormat

Audio buffer format for app buffer

MCASP_Transaction *transaction

Pointer to current transaction struct

MCASP_TxCallbackFxn cbFxn

callback function provided by the app to be called by DMA or Host Audio buffer format for app buffer

MCASP_Transaction txnLoopjob

transaction struct object for loopjob buffer

uint32_t loopjobEnable

Flag to enable loopjob. when enabled loopjob buffer is transmitted if application fails to load buffers. If disabled minimum of 2 buffers need to be submitted before start and atleast one buffer should be queued before each ISR call.

struct MCASP_DmaIcnt
#include <mcasp.h>

Public Members

uint8_t initDone

Flag to indicate if the ICNT is initialized

uint32_t txnByteCnt

Byte count for the TR

uint16_t icnt0

ICNT0 value for the TR

uint16_t icnt1

ICNT1 value for the TR

uint16_t icnt2

ICNT2 value for the TR

uint16_t icnt3

ICNT3 value for the TR

int32_t dim1

Signed dimension for loop level 1

int32_t dim2

Signed dimension for loop level 2

int32_t dim3

Signed dimension for loop level 3

struct MCASP_Object
#include <mcasp.h>

MCASP driver object.

Public Members

MCASP_Handle handle

Instance handle

uint16_t instNum

Instance number in port

uint32_t drvState

stores the current state of the driver

uint32_t transferMode

Polling, Blocking or Callback mode.

void *mcaspDmaHandle

BCDMA Handle

void *mcaspPktDmaHandle

PKTDMA Handle

MCASP_DmaChConfig *dmaChCfg

DMA Channel configuration

MCASP_TransferObj XmtObj

Holds transmit channel to the McASP.

MCASP_TransferObj RcvObj

Holds receive channel to the McASP.

uint32_t isOpen

Flag to indicate if the instance is already open

uint32_t isTxStarted

Flag to indicate if the Tx is started

uint32_t isRxStarted

Flag to indicate if the Rx is started

SemaphoreP_Object lockObj

Driver lock object

SemaphoreP_Object transferSemObj

Transfer Sync Semaphore object

HwiP_Object hwiObjTx

Transmit Interrupt object

HwiP_Object hwiObjRx

Receive Interrupt object number of slots used by the mcasp

QueueP_Object reqQueueObjTx
QueueP_Object curentQueueObjTx
QueueP_Object reqQueueObjRx
QueueP_Object curentQueueObjRx

Queue Obj to store the application buffers

QueueP_Handle reqQueueHandleTx
QueueP_Handle curentQueueHandleTx
QueueP_Handle reqQueueHandleRx
QueueP_Handle curentQueueHandleRx

Queue handle used for storing the application buffers

QueueP_Object completedQueueObjRx

Queue object to store completed Rx transactions

QueueP_Handle completedQueueHandleRx

Queue handle used for storing completed Rx transactions

uint32_t lastPlayed

Last played ring element index

uint32_t lastFilled

Last filled ring element index int TX

uint32_t lastReceived

Last received ring element index

uint32_t lastRecQueued

Last receive txn queued index

uint8_t txFifoEnable

Flag to indicate Tx fifo enable

uint8_t rxFifoEnable

Flag to indicate Rx fifo enable

MCASP_DmaIcnt txDmaIcnt

DMA Icnt values for Tx

MCASP_DmaIcnt rxDmaIcnt

DMA Icnt values for Rx

uint32_t txSampleRate

sample rate for Tx (samples/sec)

uint32_t rxSampleRate

sample rate for Rx (samples/sec)

void *txDmaChHandle

UDMA TX channel handle

void *rxDmaChHandle

UDMA RX channel handle

struct MCASP_Attrs
#include <mcasp.h>

MCASP instance attributes - used during init time.

Public Members

uint32_t instNum

MCASP instance number

uintptr_t baseAddr

Peripheral base address

uintptr_t dataBaseAddr

Peripheral data port base address

uint8_t isSynchronous

Tx and Rx is operating in synchronous mode

uint16_t numOfSerializers

Number of serializers

uint16_t serStatus[16]

Holds status information for both the serializers

MCASP_HwConfig hwCfg

Register information for initialising the Mcasp hardware.

MCASP_HwIntConfig intCfgTx

Transmit interrupt configuration

MCASP_HwIntConfig intCfgRx

Receive interrupt configuration

uint32_t txSlotSize

slot size for transmission

uint32_t rxSlotSize

slot size for reception

uint8_t txFifoWaterLevel

FIFO waterlevel for TX

uint8_t rxFifoWaterLevel

FIFO waterlevel for RX

uint32_t txFsRate

TX frame sync frequency in Hz

uint32_t rxFsRate

RX frame sync frequency in Hz

struct MCASP_Config
#include <mcasp.h>

Public Members

const MCASP_Attrs *attrs

Pointer to driver specific hardware attributes

MCASP_Object *object

Pointer to driver specific data object