IPC RPMessage

Note

These APIs are to be used from NORTOS/RTOS. When working with Linux on A53 refer to Linux documentation for Linux side APIs.

Features Supported

  • RP Message + VRING protocol implementation

  • Uses IPC Notify underneath for interrupts and uses shared memory (VRING) for message buffers

  • Uses ‘IPC Notify’ underneath for interrupts and uses shared memory (VRING) for message buffers

  • Supports message passing between NORTOS, FreeRTOS and Linux based CPUs

  • Logical communication channels can be created using unique “end points”. This allows multiple tasks on a CPU to talk to multiple tasks on another CPU using the same underlying HW mailbox and shared memory.

  • Between NORTOS and RTOS, below can be configured in RP Message to control the shared memory size,

    • Max message size, default is 128 bytes

    • Number of buffers in a VRING, default is 8 messages. Number of buffers should be powers of 2.

    • VRING shared memory buffer address can be configured, can be DDR or internal memory address.

  • Between Linux and NORTOS/RTOS, the VRING parameters are fixed as below

    • Max message is 512B

    • Number of messages in a VRING is 256

    • VRING shared memory address is determined by value in Linux device tree and is placed in DDR.

  • APIs to send and receive messages to user specified end points

  • Blocking, as well as non-blocking APIs with time out based blocking.

  • APIs to announce a created end point, needed when talking to Linux

  • API to sync and wait for LInux to be ready, needed when talking to Linux

  • APIs to use callback to receive message notifications instead of blocking, see RPMessage_CreateParams for more details.

  • APIs to use callback to receive and handle messages in callback itself, see RPMessage_CreateParams for more details.

  • Logging to Linux shared memory when IPC with Linux is enabled. Allows to view logs from RTOS/NORTOS on Linux using Linux debugfs.

SysConfig Features

Note

It is strongly recommend to use SysConfig where it is available instead of using direct SW API calls. This will help simplify the SW application and also catch common mistakes early in the development cycle. - Enable/Disable IPC RPMessage between different CPUs - Enable IPC RPMessage between NORTOS/RTOS and Linux. When enabled, SysConfig generates the resource table that is needed to talk with Linux. - Select RP Message max message size, number of buffer in a VRING - Enable IPC RPMessage between NORTOS/RTOS and Linux. When enabled, SysConfig generates the resource table that is needed to talk with Linux.

Features NOT Supported

NA

Important Usage Guidelines

Note

It is strongly recommended to refer to the IPC examples examples/drivers/ipc to understand the linker command file setup for IPC applications.

  • When Linux runs along side RTOS/NORTOS, do below to make sure NORTOS/RTOS can talk to Linux.

  • Make sure to call RPMessage_waitForLinuxReady() before starting communication with Linux.

  • Also for any RPMessage point created on NORTOS/RTOS, make sure to announce it to Linux using RPMessage_announce()

  • Make sure to assign the shared memory used for VRING between Linux and this CPU as mentioned in the Linux device tree. Also make sure to mark this section as non-cached

  • If the CPU code will run out of DDR, make sure to setup a MPU entry for the code/data section in DDR. This can be marked as cached.

  • Again refer to Linux device tree to find out the space in DDR and MSMC where the NORTOS/RTOS applications can execute from.

  • Make sure to assign the shared memory used for VRINGs between NORTOS/RTOS in a common memory section in each CPUs linker command file and make sure to mark this section as non-cached in the R5F MPU.

  • Maximum Message size is limited to 1152 Bytes in Syscfg and the maximum number of buffers is limited to 16. The recommended approach is to keep the number of buffers and message size within this limit.

  • If larger messages need to be passed, the data should be kept in a shared memory and a pointer to the same should be passed via IPC.

Example Usage

Include the below files to access the APIs

#include <stdio.h>
#include <string.h>
#include <drivers/ipc_rpmsg.h>
#include <kernel/dpl/DebugP.h>

Setup VRING shared memory for IPC RPMessage

This snippet is for reference and is generated by SysConfig when SysConfig is used for IPC.


/* Below code is for reference, recommened to use SysCfg to generate this code */

/* Below is common code for all the CPUs participating in this IPC */

#define NUM_CPUS            (2u) /* R5FSS0-0 and R5FSS0-1 in this example */
#define VRING_NUM           (NUM_CPUS*(NUM_CPUS-1))
#define VRING_NUM_BUF       (8u)
#define VRING_MAX_MSG_SIZE  (128u)   

/* Size of each VRING is
 *     number of buffers x ( size of each buffer + space for data structures of one buffer (32B) ) 
 */ 
#define VRING_SIZE          RPMESSAGE_VRING_SIZE(VRING_NUM_BUF, VRING_MAX_MSG_SIZE) 

/* Make sure of below,  
 * - The section defined below should be placed at the exact same location in memory for all the CPUs
 * - the memory should be marked as non-cached for all the CPUs
 * - the section should be marked as NOLOAD in all the CPUs linker command file
 */ 
uint8_t gVringMem[VRING_NUM][VRING_SIZE] __attribute__((aligned(128), section(".bss.sharedmemory")));

Define RPMessage_Object objects for receive and ack endpoints

/* IMPORTANT: 
 * - Below code is for Core 0
 * - All RPMessage_Object MUST be global 
 */
RPMessage_Object gAckReplyMsgObject;
/* IMPORTANT: 
 * - Below code is for Core 1
 * - All RPMessage_Object MUST be global 
 */
RPMessage_Object gRecvMsgObject;

Initialize IPC RPMessage

This snippet is for reference and is generated by SysConfig when SysConfig is used for IPC.

/* Below code is for reference, recommened to use SysCfg to generate this code */

    /* IMPORTANT: 
     * - Below code is for Core 0
     * - Make sure IPC Notify is enabled before enabling IPC RPMessage
     */
    int32_t status;
    RPMessage_Params initParams;

    RPMessage_Params_init(&initParams);
    initParams.vringTxBaseAddr[CSL_CORE_ID_R5FSS0_1] = (uintptr_t)gVringMem[0];
    initParams.vringRxBaseAddr[CSL_CORE_ID_R5FSS0_1] = (uintptr_t)gVringMem[1];
    initParams.vringNumBuf = VRING_NUM_BUF;
    initParams.vringMsgSize = VRING_MAX_MSG_SIZE;
    initParams.vringSize = VRING_SIZE;
    status = RPMessage_init(&initParams);
    DebugP_assert(status==SystemP_SUCCESS);
/* Below code is for reference, recommened to use SysCfg to generate this code */

    /* IMPORTANT: 
     * - Below code is for Core 1
     * - Make sure IPC Notify is enabled before enabling IPC RPMessage
     */
    int32_t status;
    RPMessage_Params initParams;

    RPMessage_Params_init(&initParams);
    initParams.vringTxBaseAddr[CSL_CORE_ID_R5FSS0_0] = (uintptr_t)gVringMem[1];
    initParams.vringRxBaseAddr[CSL_CORE_ID_R5FSS0_0] = (uintptr_t)gVringMem[0];
    initParams.vringNumBuf = VRING_NUM_BUF;
    initParams.vringMsgSize = VRING_MAX_MSG_SIZE;
    initParams.vringSize = VRING_SIZE;
    status = RPMessage_init(&initParams);
    DebugP_assert(status==SystemP_SUCCESS);

Create RPMessage end points for receive and ack endpoints

    /* IMPORTANT: 
     * - Below code is for Core 0
     */ 
    RPMessage_CreateParams createParams;
    
    RPMessage_CreateParams_init(&createParams);
    createParams.localEndPt = 12; /* pick any unique value on that core between 0..RPMESSAGE_MAX_LOCAL_ENDPT-1 
                                   * the value need not be unique across cores 
                                   */
    RPMessage_construct(&gAckReplyMsgObject, &createParams);
    /* IMPORTANT: 
     * - Below code is for Core 1
     */ 
    RPMessage_CreateParams createParams;
    
    RPMessage_CreateParams_init(&createParams);
    createParams.localEndPt = 13; /* pick any unique value on that core between 0..RPMESSAGE_MAX_LOCAL_ENDPT-1 
                                   * the value need not be unique across cores 
                                   */
    RPMessage_construct(&gRecvMsgObject, &createParams);

Send message from Core 0 to Core 1 and wait for reply from Core 1

    /* IMPORTANT: 
     * - Below code is for Core 0
     */ 

    char sendMsg[64] = "hello, world!!!";
    char replyMsg[64];
    uint16_t replyMsgSize, remoteCoreId, remoteCoreEndPt;

    RPMessage_send( 
        sendMsg, strlen(sendMsg), 
        CSL_CORE_ID_R5FSS0_1, 13, 
        RPMessage_getLocalEndPt(&gAckReplyMsgObject),
        SystemP_WAIT_FOREVER);

    /* set 'replyMsgSize' to size of recv buffer, 
     * after return `replyMsgSize` contains actual size of valid data in recv buffer 
     */
    replyMsgSize = sizeof(replyMsg); /*  */
    RPMessage_recv(&gAckReplyMsgObject, 
        replyMsg, &replyMsgSize, 
        &remoteCoreId, &remoteCoreEndPt, 
        SystemP_WAIT_FOREVER);

Receive message at Core 1 from Core 0 and send ack to Core 0

    /* IMPORTANT: 
     * - Below code is for Core 1
     */ 
    while(1)
    {
        char recvMsg[64];
        char replyMsg[64];
        uint16_t recvMsgSize, remoteCoreId, remoteCoreEndPt;

        /* wait for messages forever in a loop */

        /* set 'recvMsgSize' to size of recv buffer, 
        * after return `recvMsgSize` contains actual size of valid data in recv buffer 
        */
        recvMsgSize = sizeof(recvMsg);
        RPMessage_recv(&gRecvMsgObject, 
            recvMsg, &recvMsgSize, 
            &remoteCoreId, &remoteCoreEndPt, 
            SystemP_WAIT_FOREVER);

        /* echo the message string as reply, we know this is null terminating string
         * so strcpy is safe to use.
         */
        strcpy(replyMsg, recvMsg);

        /* send ack to sender CPU at the sender end point */
        RPMessage_send( 
            replyMsg, strlen(replyMsg), 
            remoteCoreId, remoteCoreEndPt, 
            RPMessage_getLocalEndPt(&gRecvMsgObject),
            SystemP_WAIT_FOREVER);
    }

Include the below files to access the APIs

#include <stdio.h>
#include <string.h>
#include <drivers/ipc_rpmsg.h>
#include <kernel/dpl/DebugP.h>

Define the following macros

/* This is used to run the echo test with user space kernel */
#define IPC_RPMESSAGE_SERVICE_CHRDEV      "rpmsg_chrdev"
#define IPC_RPMESSAGE_ENDPT_CHRDEV_PING   (14U)

/* maximum size that message can have in this example */
#define IPC_RPMESSAGE_MAX_MSG_SIZE        (96u)

Setup resource table to be used by Linux, this snippet is for reference and is generated by SysConfig when SysConfig is used for IPC.

/* Buffer used for trace, address and size of this buffer is put in the resource table so that Linux can read it */
char gDebugMemLog[DebugP_MEM_LOG_SIZE] __attribute__ ((section (".bss.debug_mem_trace_buf"), aligned (128)));
uint32_t gDebugMemLogSize = DebugP_MEM_LOG_SIZE;

const RPMessage_ResourceTable gRPMessage_linuxResourceTable __attribute__ ((section (".resource_table"), aligned (4096))) =
{
    {
        1U,         /* we're the first version that implements this */
        2U,         /* number of entries, MUST be 2 */
        { 0U, 0U, } /* reserved, must be zero */
    },
    /* offsets to the entries */
    {
        offsetof(RPMessage_ResourceTable, vdev),
        offsetof(RPMessage_ResourceTable, trace),
    },
    /* vdev entry */
    {
        RPMESSAGE_RSC_TYPE_VDEV, RPMESSAGE_RSC_VIRTIO_ID_RPMSG,
        0U, 1U, 0U, 0U, 0U, 2U, { 0U, 0U },
    },
    /* the two vrings */
    { RPMESSAGE_RSC_VRING_ADDR_ANY, 4096U, 256U, 1U, 0U },
    { RPMESSAGE_RSC_VRING_ADDR_ANY, 4096U, 256U, 2U, 0U },
    {
        (RPMESSAGE_RSC_TRACE_INTS_VER0 | RPMESSAGE_RSC_TYPE_TRACE),
        (uint32_t)gDebugMemLog, DebugP_MEM_LOG_SIZE,
        0, "trace:m4fss0_0",
    },
};

Initialize IPC RPMessage, this snippet is for reference and is generated by SysConfig when SysConfig is used for IPC.

/* Below code is for reference, recommened to use SysCfg to generate this code */

    /* IMPORTANT:
     * - Make sure IPC Notify is enabled before enabling IPC RPMessage
     */

    RPMessage_Params rpmsgParams;
    int32_t status;

    /* initialize parameters to default */
    RPMessage_Params_init(&rpmsgParams);

    rpmsgParams.linuxResourceTable = &gRPMessage_linuxResourceTable;
    rpmsgParams.linuxCoreId = CSL_CORE_ID_A53SS0_0;

    /* initialize the IPC RP Message module */
    status = RPMessage_init(&rpmsgParams);
    DebugP_assert(status==SystemP_SUCCESS);

    /* This API MUST be called by applications when its ready to talk to Linux */
    status = RPMessage_waitForLinuxReady(SystemP_WAIT_FOREVER);
    DebugP_assert(status==SystemP_SUCCESS);

Define RPMessage_Object objects for receive endpoints

/* IMPORTANT:
 * - Below code is for Core 1
 * - All RPMessage_Object MUST be global
 */
RPMessage_Object gRecvMsgObject;

Create RPMessage end points for receive endpoints

    /* IMPORTANT:
     * - Below code is for Core 0
     */
    RPMessage_CreateParams createParams;
    int32_t status;

    RPMessage_CreateParams_init(&createParams);
    createParams.localEndPt = IPC_RPMESSAGE_ENDPT_CHRDEV_PING;
    status = RPMessage_construct(&gRecvMsgObject, &createParams);
    DebugP_assert(status==SystemP_SUCCESS);

    /* We need to "announce" to Linux client else Linux does not know a service exists on this CPU
     * This is not mandatory to do for RTOS clients
     */
    status = RPMessage_announce(CSL_CORE_ID_A53SS0_0, IPC_RPMESSAGE_ENDPT_CHRDEV_PING, IPC_RPMESSAGE_SERVICE_CHRDEV);
    DebugP_assert(status==SystemP_SUCCESS);

Receive message at MCU core from A53 Linux and send ack to A53 Linux

    /* IMPORTANT:
     * - Below code is for Core 1
     */
    while(1)
    {
        char recvMsg[IPC_RPMESSAGE_MAX_MSG_SIZE + 1];
        char replyMsg[IPC_RPMESSAGE_MAX_MSG_SIZE + 1];
        uint16_t recvMsgSize, remoteCoreId;
        uint32_t remoteCoreEndPt;

        /* wait for messages forever in a loop */

        /* set 'recvMsgSize' to size of recv buffer,
        * after return `recvMsgSize` contains actual size of valid data in recv buffer
        */
        recvMsgSize = sizeof(recvMsg);
        RPMessage_recv(&gRecvMsgObject,
            recvMsg, &recvMsgSize,
            &remoteCoreId, &remoteCoreEndPt,
            SystemP_WAIT_FOREVER);

        /* echo the message string as reply, we know this is null terminating string
         * so strcpy is safe to use.
         */
        strcpy(replyMsg, recvMsg);

        /* send ack to sender CPU at the sender end point */
        RPMessage_send(
            replyMsg, strlen(replyMsg),
            remoteCoreId, remoteCoreEndPt,
            RPMessage_getLocalEndPt(&gRecvMsgObject),
            SystemP_WAIT_FOREVER);
    }

API Reference

Defines

RPMESSAGE_MAX_LOCAL_ENDPT

Users can create RPMessage_Object with local end value in the range of 0 .. RPMESSAGE_MAX_LOCAL_ENDPT - 1.

This limit is put to allow fast indexing of end point object to recevied messages and the value is kept small to save memory space

RPMESSAGE_VRING_ADDR_INVALID

Value to indicate if vring ID is valid or NOT.

When a core does not participate in IPC RPMessage set the vring ID in RPMessage_Params to this value

RPMESSAGE_VRING_SIZE(numBuf, bufSize)

Returns the size needed for each VRING.

This is approximate size that is >= to actual required size. Approximate size is returned to allow compile time macro for size calculation. Actual required size is calculated in the internal run-time function RPMessage_vringGetSize. However this can be ignored by end users. During initialization, a assert is used to check if user provided size is >= actual required size.

Parameters:
  • numBuf – [in] Number of buffer in the VRING

  • bufSize – [in] Size of each buffer, in units of bytes

Returns:

VRING size in bytes

RPMESSAGE_VRING_SIZE_PDK(numBuf, bufSize)

Returns the size needed for each VRING.

This is approximate size that is >= to actual required size. Approximate size is returned to allow compile time macro for size calculation. Actual required size is calculated in the internal run-time function RPMessage_vringGetSize. However this can be ignored by end users. During initialization, a assert is used to check if user provided size is >= actual required size.

Parameters:
  • numBuf – [in] Number of buffer in the VRING

  • bufSize – [in] Size of each buffer, in units of bytes

Returns:

VRING size in bytes

RPMESSAGE_OBJECT_SIZE_MAX

Size of RPMessage_Object.

Typedefs

typedef void (*RPMessage_RecvCallback)(RPMessage_Object *handle, void *arg, void *data, uint16_t dataLen, uint16_t remoteCoreId, uint16_t remoteEndPt)

Callback that is invoked when a message is received from any CPU at the specified local end point.

The callback can be optionally registered during RPMessage_construct

Note

All message contents MUST be consumed in the callback. When callback returns the message buffer is released back to the sender. If the message contents are needed for deferred processing then take a copy of the message contents

Param handle:

[in] RPMessage end point object created with RPMessage_construct

Param arg:

[in] Arguments specified by user during RPMessage_construct

Param data:

[in] Pointer to message

Param dataLen:

[in] Length of message

Param remoteCoreId:

[in] Core ID of sender

Param remoteEndPt:

[in] End point of sender

typedef void (*RPMessage_RecvNotifyCallback)(RPMessage_Object *handle, void *arg)

Callback that is invoked when a message is received from any CPU at the specified local end point.

The callback can be optionally registered during RPMessage_construct

Note

Unlike RPMessage_RecvCallback, this callback only notifies that there is one or more messages to be read, but the message itself is not read by the driver unless RPMessage_recv is called in this callback or later within a task.

Note

If RPMessage_RecvCallback is set, then RPMessage_RecvNotifyCallback callback is not used.

Param handle:

[in] RPMessage end point object created with RPMessage_construct

Param arg:

[in] Arguments specified by user during RPMessage_construct

typedef void (*RPMessage_ControlEndPtCallback)(void *arg, uint16_t remoteCoreId, uint16_t remoteEndPt, const char *remoteServiceName)

Callback that is invoked when a annoucement message is received on the control end point.

The callback can be optionally registered during RPMessage_init

Note

All message contents MUST be consumed in the callback. When callback returns the message buffer is released back to the sender. If the message contents are needed for deferred processing then take a copy of the message contents

Param arg:

[in] Arguments specified by user during RPMessage_init

Param remoteCoreId:

[in] Core ID of sender

Param remoteEndPt:

[in] End point of sender that has annoucned the service over the control end point

Param remoteServiceName:

[in] Name of the remote service that is annoucned

Functions

void RPMessage_Params_init(RPMessage_Params *params)

Set default values to RPMessage_Params.

Parameters:

params – [out] default intialized structure

void RPMessage_CreateParams_init(RPMessage_CreateParams *params)

Set default values to RPMessage_CreateParams.

Parameters:

params – [out] default intialized structure

int32_t RPMessage_init(const RPMessage_Params *params)

Initialize RPMessage module.

Parameters:

params – [in] Initialization parameters

void RPMessage_deInit(void)

De-Initialize RPMessage module.

int32_t RPMessage_waitForLinuxReady(uint32_t timeout)

Wait for linux side RPMessage to be ready.

Messages should not be sent to Linux, if enabled, until this function return success.

Note

When using RPMessage between RTOS/no-RTOS cores then this API needed not be called.

Parameters:

timeout – [in] Timeout in units of system ticks

Returns:

SystemP_SUCCESS, linux has initialized its side of RPMessage

void RPMessage_controlEndPtCallback(RPMessage_ControlEndPtCallback controlEndPtCallback, void *controlEndPtCallbackArgs)

Callback to call when a control message is received on a control end point.

Parameters:
  • controlEndPtCallback – [in] User callback to invoke

  • controlEndPtCallbackArgs – [in] Arguments pass to the user control end point callback

int32_t RPMessage_construct(RPMessage_Object *handle, const RPMessage_CreateParams *createParams)

Create a RPMessage object to receive messages at a specified end-point.

Note

Each new object that is created MUST have a unique local end point.

Note

Local end point MUST be < RPMESSAGE_MAX_LOCAL_ENDPT

Note

User MUST choose a value and ANY is not supported

Note

When callback is registered in RPMessage_CreateParams, RPMessage_recv MUST not be used.

Parameters:
  • handle – [out] Created object

  • createParams – [in] parameters

Returns:

SystemP_SUCCESS on success, else failure.

void RPMessage_destruct(RPMessage_Object *handle)

Delete a previously created RPMessage object.

Parameters:

handle – [in] object

void RPMessage_unblock(RPMessage_Object *handle)

Unblocks RPMessage_recv, for the input object, if it is blocked waiting on messages and users want to exit that task.

Parameters:

handle – [in] object

uint16_t RPMessage_getLocalEndPt(const RPMessage_Object *handle)

Return local end point of a RPMessage_Object.

The value will be same as that was used to create the object earlier.

Parameters:

handle – [in] object

Returns:

local end point of input object

int32_t RPMessage_announce(uint16_t remoteCoreId, uint16_t localEndPt, const char *name)

Announce a local end point at which a service is created to a remote core.

Note

Announcing end points is optional and is not used internally by IPC RPmessage in any way.

Note

User MUST announce one by one to all remote core’s of interest. There is no announce to ALL option

Note

To handle announcement messages, make sure user handler is registered during RPMessage_init via RPMessage_Params

Note

It is upto the end user to use the callback to signal or wait until a remote service is announced.

Parameters:
  • remoteCoreId – [in] The remote core to annouce to.

  • localEndPt – [in] Local end point of the service that is being announced

  • name – [in] Name of the service that is being announced

Returns:

SystemP_SUCCESS, when the annouce message was sent, else failure

int32_t RPMessage_send(void *data, uint16_t dataLen, uint16_t remoteCoreId, uint16_t remoteEndPt, uint16_t localEndPt, uint32_t timeout)

Send a message to a remote core at a specified remote end point.

Note

dataLen MUST be <= RPMessage_Params::vringMsgSize - 16 bytes for internal header

Note

In order for a remote core to receive the message, a end point should be created on the remote core at the same value as remoteEndPt

Note

localEndPt, is strictly not needed, however this is available to the user on the remote core and can be used as a reply end point. Use RPMessage_getLocalEndPt to set to the RPMessage object at which to listen for replies

Note

When timeout is 0, then if a free buffer is not available to transmit, it will return will immediately SystemP_TIMEOUT. Else it will wait for specified timeout ticks for a free buffer to be available.

Parameters:
  • data – [in] Pointer to message data to send

  • dataLen – [in] size of message data to send

  • remoteCoreId – [in] Remote core ID to whom the message is being sent

  • remoteEndPt – [in] Remote core end point ID to which the message is being sent

  • localEndPt – [in] Local end point that is sending the message

  • timeout – [in] Amount of time to wait, in units of system ticks

Returns:

SystemP_SUCCESS, when the send message was successful

Returns:

SystemP_TIMEOUT, message not sent since free transmit buffer not available and timeout happened.

int32_t RPMessage_recv(RPMessage_Object *handle, void *data, uint16_t *dataLen, uint16_t *remoteCoreId, uint32_t *remoteEndPt, uint32_t timeout)

Blocking API to wait till a message is received from any CPU at the specified local end point.

Note

Local end point is specified during RPMessage_construct

Note

When callback is registered this API should not be used.

Note

dataLen when passed by user contains the user message buffer size, i.e size of buffer pointer to by ‘data`. If received message size exceeds *dataLen then it is truncated. If received message size is <= *dataLen then all received bytes are copied to data and *dataLen indicates the size of valid bytes in data

Parameters:
  • handle – [in] RPMessage end point object created with RPMessage_construct

  • data – [in] Pointer to received message contents

  • dataLen –

    [in] Length of user message buffer, in bytes

    [out] Size of received message, in bytes

  • remoteCoreId – [out] Core ID of sender

  • remoteEndPt – [out] End point of sender

  • timeout – [in] Time in system ticks to block for a message receive

Returns:

SystemP_SUCCESS, new message received, all output parameters are valid

Returns:

SystemP_TIMEOUT, API unblocked due to timeout and output parameters should not be used.

struct RPMessage_Object
#include <ipc_rpmsg.h>

Opaque RPMessage object used with the RPMessage APIs.

Public Members

uintptr_t rsv[RPMESSAGE_OBJECT_SIZE_MAX / sizeof(uint32_t)]

reserved, should NOT be modified by end users

struct RPMessage_CreateParams
#include <ipc_rpmsg.h>

Parameters passed to RPMessage_construct.

It is recommended to set defaults using RPMessage_CreateParams_init and then override with user specified parameters.

Note

When recvCallback is enabled, RPMessage_recv API should not be used and will always return failure. In this case, the received message is read and made available in the callback itself and the message needs to be consumed in the callback itself.

Note

When recvNotifyCallback is enabled, RPMessage_recv API still needs to used to read the message. The callback just informs there are one or more messages are pending.

Public Members

uint16_t localEndPt

local end point at which to listen for received mesages

RPMessage_RecvCallback recvCallback

Optional callback to invoke when a message is received at this end point

void *recvCallbackArgs

Arguments to pass to the recvCallback callback

RPMessage_RecvNotifyCallback recvNotifyCallback

Optional callback to notify user when a message is received at this end point. If recvCallback is set, then this callback is not used

void *recvNotifyCallbackArgs

Arguments to pass to the recvNotifyCallback callback

struct RPMessage_Params
#include <ipc_rpmsg.h>

Parameters passed to RPMessage_init, these are generated via SysCfg.

Note

Set vringTxBaseAddr[], vringTxBaseAddr[] to RPMESSAGE_VRING_ADDR_INVALID for cores that are not needed for IPC RPMessage. You can use RPMessage_Params_init to set valid defaults.

Note

All cores MUST set the same value for vringSize, vringNumBuf, vringMsgSize.

Note

Set vringTxBaseAddr, vringRxBaseAddr, based on source and destination cores.

Note

VRING memory is shared across all cores AND this memory MUST be marked as non-cached at all the cores.

Public Members

uintptr_t vringTxBaseAddr[CSL_CORE_ID_MAX]

VRING address of transmit rings to each core

uintptr_t vringRxBaseAddr[CSL_CORE_ID_MAX]

VRING address of receive rings to each core

uint32_t vringSize

Size of memory assigned to one VRING, use RPMESSAGE_VRING_SIZE to find the size needed

uint32_t vringNumBuf

Max number of buffers in one VRING

uint32_t vringMsgSize

Size of each message in one VRING

const RPMessage_ResourceTable *linuxResourceTable

Linux resoruce table for self core, when non-NULL Cortex A* is assumed to run Linux. And VRING info for message exchange with LInux is specified in the resource table

uint16_t linuxCoreId
uint8_t vringAllocationPDK

ID of linux core

uint8_t vringAllocationQNX

Vring allocation follows PDK or not