Using SDK with CCS Projects
Note
The steps on this page show screen shots and description based on Linux. However the steps in Windows would remain the same, unless mentioned otherwise.
Note
By default, CCS import of SDK example projects performs a copy of example files to CCS workspace. User are free to modify the example files without affecting the files in the SDK installed location.
Note
Deleting the CCS project, deletes the project files from CCS workspace. User should be careful especially when the copied example files are modified by user.
Note
The screen shots shown on this page are for AM64x MCU+ SDK v7.3.0. You would see your specific SOC and SDK version that is installed. However the instructions and steps mentioned remain the same, unless mentioned otherwise.
Introduction
All SDK examples can be built using CCS projects. Using CCS projects one can also open SysConfig from within CCS itself to configure the example. This section provides basic instructions and tips on using CCS projects.
Note
To re-build libraries you need to use makefiles, see Using SDK with Makefiles
CCS Projectspec and CCS Projects
When a example project is imported into CCS, what is really getting imported is a
projectspecfile.This file is a definition or blueprint of a CCS project, like compiler options, files to compile, libraries to link.
CCS takes the projectspec as input and then generates CCS project files in the user workspace.
Default workspace is,
C:/Users/{user name}/workspace_v{CCS major version}/{project name}/
The
projectspecis also human readable, i.e you can open it in a text editor to see all the different options for that project.
Import a Project in CCS
First click on “Import Project(s)” as shown below
Import Project(s)
Click on “Browse” in the “Import Projects” window to import a project
Project Import
Click “Browse” and go to ${SDK_INSTALL_PATH}/examples/ folder
Select Examples Folder
This will list all example projects, now you can select one or more or all projects to import into CCS.
Select Project
All examples follow below naming convention to help you easily pick the example you need {example name}{soc board}{cpu}{os}{compiler toolchain}
You can also navigate to the example folder to pick a specific example. All examples are organized as below in the examples folder. examples/{component or module}/{optional sub-module or sub-component}/ | + – {example name}/{board on which this example can run}/ | + – {cpu}_{os}/{compiler toolchain} | + – example.projectspec –> This is the file that CCS imports.
Browse a Project in CCS
Once a example project is imported, you can learn more about the example, by clicking the “README.html” file
Example Readme
You can also open the SysConfig GUI by double-clicking the “example.syscfg” file, (see also Using SDK with SysConfig)
Example SysConfig
You can explore other project files by clicking on them.
Build a Project in CCS
To build a project “right-click” on the project name and select “Build Project” to build it
By default it builds in “debug” profile, i.e without compiler optimizations. To build with compiler optimizations, select “release” profile by clicking, “Build Configurations > Set Active > Release” as shown below.
Build a Project
You can explore additional project options in the same menu.
Build System Projects in CCS
Some examples, to run correctly, need multiple binaries on different CPUs to be built, loaded and run. Such examples have “system projects” associated with them. One such example is inter-processor communication example, which shows multiple CPUs communicating among each other.
System project have a naming convention as below
{example name}_{soc board}_system_{os or tag}_{compiler toolchain}
And the project file is located at
examples/{component or module}/{optional sub-module or sub-component}/ | + -- {example name}/{board on which this example can run}/ | + -- system_{os or tag}/ | + -- system.projectspec --> This is the file that CCS imports.
Load and Run Executables Built with CCS Projects
Simply load and run binary .out on EVM using CCS (see CCS Launch, Load and Run)
In case of “system” examples, you need to load the binaries for each CPU one by one in CCS and then run each CPU. Typically the order of load and run of different CPUs is not important.
Delete a Project in CCS
To delete a imported project “right-click” on the project name and select “Delete” to delete it.
It is recommended to check the box as shown below, else you will have trouble re-importing the project
Delete a Project
Note, that deleting a project, only deletes it from your CCS workspace, the .c, .h and other project files are located with the ${SDK_INSTALL_PATH}/examples and these are not deleted.
You can reimport a project later as needed.