TI-RTOS for SimpleLink Wireless MCUs
2.14.01.20
|
CCamera_Config | Camera Global configuration |
CCamera_FxnTable | The definition of a Camera function table that contains the required set of functions to control a specific Camera driver implementation |
CCamera_Params | Camera Parameters |
CCameraCC3200DMA_HWAttrs | CameraCC3200DMA Hardware attributes |
CCameraCC3200DMA_Object | CameraCC3200DMA Object |
CClockP_FreqHz | Frequency-in-hertz struct |
CClockP_Params | Basic ClockP Parameters |
CCryptoCC26XX_AESCCM_Transaction | CryptoCC26XX AES-CCM Transaction |
CCryptoCC26XX_AESECB_Transaction | CryptoCC26XX AES-ECB Transaction |
CCryptoCC26XX_Config | CryptoCC26XX Global Configuration |
CCryptoCC26XX_HWAttrs | CryptoCC26XX Hardware Attributes |
CCryptoCC26XX_Object | CryptoCC26XX Object |
CCryptoCC26XX_Params | CryptoCC26XX Parameters |
CCryptoCC26XX_Transaction | CryptoCC26XX Transaction |
CGPIOCC3200_Config | GPIO device specific driver configuration structure |
CGPIOMSP430_Config | GPIO device specific driver configuration structure |
CGPIOMSP432_Config | GPIO device specific driver configuration structure |
CGPIOTiva_Config | GPIO device specific driver configuration structure |
CHwiP_Params | Basic HwiP Parameters |
CI2C_Config | I2C Global configuration |
CI2C_FxnTable | The definition of a I2C function table that contains the required set of functions to control a specific I2C driver implementation |
CI2C_Params | I2C Parameters |
CI2C_Transaction | I2C transaction |
CI2CCC26XX_HWAttrs | I2CCC26XX Hardware attributes |
CI2CCC26XX_I2CPinCfg | I2CCC26XX Pin Configuration |
CI2CCC26XX_Object | I2CCC26XX Object |
CI2CCC3200_HWAttrs | I2CCC3200 Hardware attributes |
CI2CCC3200_Object | I2CCC3200 Object |
CI2CEUSCIB_HWAttrs | I2CEUSCIB Hardware attributes |
CI2CEUSCIB_Object | I2CEUSCIB Object |
CI2CMSP432_HWAttrs | I2CMSP432 Hardware attributes These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP430Ware these definitions are found in: |
CI2CMSP432_Object | I2CMSP432 Object |
CI2CTiva_HWAttrs | I2CTiva Hardware attributes |
CI2CTiva_Object | I2CTiva Object |
CI2CUSCIB_HWAttrs | I2CUSCIB Hardware attributes |
CI2CUSCIB_Object | I2CUSCIB Object |
CI2S_BufDesc | I2S buffer descriptor for issue/reclaim mode |
CI2S_Config | I2S Global configuration |
CI2S_FxnTable | The definition of a I2S function table that contains the required set of functions to control a specific I2S driver implementation |
CI2S_Params | Basic I2S Parameters |
CI2SCC3200DMA_HWAttrs | I2SCC3200DMA Hardware attributes |
CI2SCC3200DMA_Object | I2SCC3200DMA Object |
CI2SCC3200DMA_SerialPinConfig | CC3200 Serial Pin Configuration |
CI2SCC3200DMA_SerialPinParams | CC3200 specific I2S Parameters |
CI2SCC3200DMA_SerialPinVars | I2SCC3200DMA Serial pin variables |
CLCD_Buffer | LCD_Buffer used to store data to be printed on the LCD display |
CLCD_Command | Format of LCD commands used by the LCD controller |
CLCD_Config | The LCD_Config structure contains a set of pointers used to characterize the LCD driver implementation |
CLCD_HWAttrs | LCD Hardware attributes |
CLCD_Object | LCD Object |
CLCD_Params | LCD Parameters are used to with the LCD_open() call. Default values for these parameters are set using LCD_Params_init() |
CMutexP_Params | Basic MutexP Parameters |
CPIN_State_s | Underlying data structure for type PIN_State |
CPower_NotifyObj | Power notify object structure |
CPowerCC3200_Config | Power global configuration |
CPowerCC3200_MCURegisters | MCU core registers that need to be save on entering LPDS |
CPowerCC3200_ModuleState | Internal module state |
CPowerCC3200_NVICRegisters | NVIC registers that need to be save on entering LPDS |
CPowerCC3200_SaveRegisters | Struct of context registers to save on entering LPDS |
CPowerCC3200_Wakeup | For wakeup from LPDS or shutdown configuration |
CPowerMSP432_Config | Power global configuration (MSP432-specific) |
CPowerMSP432_Freqs | Structure holding device frequencies (in Hz) |
CPWM_Config | PWM Global configuration |
CPWM_FxnTable | The definition of a PWM function table that contains the required set of functions to control a specific PWM driver implementation |
CPWM_Params | PWM Parameters |
CPWMTimerCC3200_HWAttrs | PWMTimerCC3200 Hardware attributes |
CPWMTimerCC3200_Object | PWMTimerCC3200 Object |
CPWMTimerMSP432_HWAttrs | PWMTimerMSP432 Hardware attributes |
CPWMTimerMSP432_Object | PWMTimerMSP432 Object |
CPWMTimerMSP432_Status | PWMTimerMSP432_Status |
CPWMTimerTiva_HWAttrs | PWMTimerCC3200 Hardware attributes |
CPWMTimerTiva_Object | PWMTimerTiva Object |
CPWMTiva_HWAttrs | PWMTiva Hardware attributes |
CPWMTiva_Object | PWMTiva Object |
CPWMTiva_Status | PWMTiva_Status |
CRF_Mode | Struct defining operating mode of RF driver |
CRF_Object | Struct used to store RF client state and configuration Pointer to an RF_Object is used as handles (RF_Handle) in interactions with the RF driver |
CRF_Params | RF parameter struct RF parameters are used with the RF_open() and RF_Params_init() call |
CRF_RadioSetup | Union of the different flavors of RADIO_SETUP commands |
CSDSPI_Config | SDSPI Global configuration |
CSDSPI_FxnTable | The definition of a SDSPI function table that contains the required set of functions to control a specific SDSPI driver implementation |
CSDSPI_Params | SDSPI Parameters |
CSDSPICC3200_HWAttrs | SDSPICC3200 Hardware attributes |
CSDSPICC3200_Object | SDSPICC3200 Object |
CSDSPIEUSCIA_HWAttrs | SDSPIEUSCIA Hardware attributes |
CSDSPIEUSCIA_Object | SDSPIEUSCIA Object |
CSDSPIEUSCIB_HWAttrs | SDSPIEUSCIB Hardware attributes |
CSDSPIEUSCIB_Object | SDSPIEUSCIB Object |
CSDSPIMSP432_HWAttrs | SDSPIMSP432 Hardware attributes |
CSDSPIMSP432_Object | SDSPIMSP432 Object |
CSDSPITiva_HWAttrs | SDSPITiva Hardware attributes |
CSDSPITiva_Object | SDSPITiva Object |
CSDSPIUSCIA_HWAttrs | SDSPIUSCIA Hardware attributes |
CSDSPIUSCIA_Object | SDSPIUSCIA Object |
CSDSPIUSCIB_HWAttrs | SDSPIUSCIB Hardware attributes |
CSDSPIUSCIB_Object | SDSPIUSCIB Object |
CSemaphoreP_Params | Basic SemaphoreP Parameters |
CSPI_Config | SPI Global configuration |
CSPI_FxnTable | The definition of a SPI function table that contains the required set of functions to control a specific SPI driver implementation |
CSPI_Params | SPI Parameters |
CSPI_Transaction | A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat frames are sent and received from the buffers pointed to txBuf and rxBuf. The arg variable is an user-definable argument which gets passed to the SPI_CallbackFxn when the SPI driver is in SPI_MODE_CALLBACK |
CSPICC26XX_HWAttrs | SPICC26XXDMA Hardware attributes |
CSPICC26XX_Object | SPICC26XXDMA Object |
CSPICC3200DMA_HWAttrs | SPICC3200DMA Hardware attributes |
CSPICC3200DMA_Object | SPICC3200DMA Object |
CSPIEUSCIADMA_HWAttrs | SPIEUSCIADMA Hardware attributes |
CSPIEUSCIADMA_Object | SPIEUSCIADMA Object |
CSPIEUSCIBDMA_HWAttrs | SPIEUSCIBDMA Hardware attributes |
CSPIEUSCIBDMA_Object | SPIEUSCIBDMA Object |
CSPIMSP432DMA_HWAttrs | SPIMSP432DMA Hardware attributes These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP430Ware these definitions are found in: |
CSPIMSP432DMA_Object | SPIMSP432DMA Object |
CSPITivaDMA_HWAttrs | SPITivaDMA Hardware attributes |
CSPITivaDMA_Object | SPITivaDMA Object |
CSPIUSCIADMA_HWAttrs | SPIUSCIADMA Hardware attributes |
CSPIUSCIADMA_Object | SPIUSCIADMA Object |
CSPIUSCIBDMA_HWAttrs | SPIUSCIBDMA Hardware attributes |
CSPIUSCIBDMA_Object | SPIUSCIBDMA Object |
CUART_Config | UART Global configuration |
CUART_FxnTable | The definition of a UART function table that contains the required set of functions to control a specific UART driver implementation |
CUART_Params | UART Parameters |
CUARTCC26XX_HWAttrs | UARTCC26XX Hardware attributes |
CUARTCC26XX_Object | UARTCC26XX Object |
CUARTCC3200_FxnSet | Complement set of read functions to be used by the UART ISR and UARTCC3200_read(). Internal use only |
CUARTCC3200_HWAttrs | UARTCC3200 Hardware attributes |
CUARTCC3200_Object | UARTCC3200 Object |
CUARTCC3200DMA_HWAttrs | UARTCC3200DMA Hardware attributes |
CUARTCC3200DMA_Object | UARTCC3200DMA Object |
CUARTEUSCIA_BaudrateConfig | UARTEUSCIA Baudrate configuration |
CUARTEUSCIA_HWAttrs | UARTEUSCIA Hardware attributes |
CUARTEUSCIA_Object | UARTEUSCIA Object |
CUARTMSP432_BaudrateConfig | UARTMSP432 Baudrate configuration |
CUARTMSP432_FxnSet | Complement set of read functions to be used by the UART ISR and UARTMSP432_read(). Internal use only |
CUARTMSP432_HWAttrs | UARTMSP432 Hardware attributes |
CUARTMSP432_Object | UARTMSP432 Object |
CUARTTiva_FxnSet | Complement set of read functions to be used by the UART ISR and UARTTiva_read(). Internal use only |
CUARTTiva_HWAttrs | UARTTiva Hardware attributes |
CUARTTiva_Object | UARTTiva Object |
CUARTTivaDMA_HWAttrs | UARTTivaDMA Hardware attributes |
CUARTTivaDMA_Object | UARTTivaDMA Object |
CUARTUSCIA_BaudrateConfig | UARTUSCIA Baudrate configuration |
CUARTUSCIA_HWAttrs | UARTUSCIA Hardware attributes |
CUARTUSCIA_Object | UARTUSCIA Object |
CUDMACC26XX_Config | UDMACC26XX Global configuration |
CUDMACC26XX_HWAttrs | UDMACC26XX hardware attributes |
CUDMACC26XX_Object | UDMACC26XX object |
CWatchdog_Config | Watchdog Global configuration |
CWatchdog_FxnTable | The definition of a Watchdog function table that contains the required set of functions to control a specific Watchdog driver implementation |
CWatchdog_Params | Watchdog Parameters |
CWatchdogCC26XX_HWAttrs | Watchdog hardware attributes for CC26XX |
CWatchdogCC26XX_Object | Watchdog Object for CC26XX |
CWatchdogCC3200_HWAttrs | Watchdog hardware attributes for CC3200 |
CWatchdogCC3200_Object | Watchdog Object for CC3200 |
CWatchdogMSP430_HWAttrs | Watchdog hardware attributes for MSP430 |
CWatchdogMSP430_Object | Watchdog Object for MSP430 |
CWatchdogMSP432_HWAttrs | Watchdog hardware attributes for MSP432 These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP432Ware these definitions are found in: |
CWatchdogMSP432_Object | Watchdog Object for MSP432 |
CWatchdogTiva_HWAttrs | Watchdog hardware attributes for Tiva |
CWatchdogTiva_Object | Watchdog Object for Tiva |