7.7.6.113. OnHalt¶
GEL callback function called after a halt operation is performed on the current target
Syntax
OnHalt();
Parameters
None
Description
If defined in a loaded GEL file, OnHalt() is called after the target is halted.
Example
OnHalt() {GEL_TextOut("OnHalt called …n")}