7.7.6.57. GEL_PinConnect()ΒΆ

For simulator only, connects a data file to an external interrupt pin.

Syntax

GEL_PinConnect( "pinName", "fileName" );

Parameters

pinName names the external interrupt pin. The pinName must be enclosed in quotation marks.

fileNamenames the data file that specifies interrupt intervals. The fileName must be enclosed in quotation marks.

Description

The simulator allows you to simulate external interrupt signals. This function connects a data file that specifies interrupt intervals to the specified external interrupt pin.

If the file is not in the current directory, provide a full path name within the string. A double backslash escape sequence is required to ensure that you get a backslash into the fileName Parameters.

Synchronous

Synchronous from GEL: Yes

Completely synchronous: Yes

Example

GEL_PinConnect("INT0", "c:\mydir\myfile.dat");

Related Topics

GEL_PinDisconnect()