7.7.6.6. GEL_AsmStepOver()ΒΆ
Steps over the next assembly instruction.
Syntax GEL_AsmStepOver([count]?**);**
Parameters
count:(optional) specifies the number of times the command is to be repeated. If no count is specified, steps over a single assembly instruction.
Description
In the Assembly or mixed mode, steps over a single assembly instruction. Repeats count times. If the instruction is an assembly subroutine, executes the assembly subroutine and then halts after the assembly function returns. In source mode, may not appear to move the source cursor at all.
Synchronous
Synchronous from GEL: No
Completely synchronous: No
Related Topics