7.7.6.5. GEL_AsmStepInto()ΒΆ
Executes the next assembly instruction.
Syntax
GEL_AsmStepInto([count] );
Parameters
count(optional) specifies the number of times the command is to be repeated. If no count is specified, GEL_ASMStepInto executes a single assembly instruction.
Description
Executes the next assembly instruction, whether source is available or not. Repeats count times. Optionally, you can enable/disable automatic focus change to a Disassembly window, in assembly or mixed mode, to show the current assembly instruction.
Synchronous
Synchronous from GEL: No
Completely synchronous: No
Example
GEL_AsmStepInto();
Related Topics