7.7.6.16. GEL_EnableClock()ΒΆ

Enables or disables the profile clock.

Syntax

GEL_EnableClock([bool enable]);

Parameters

[optional]

0 disables the clock.

1 enables the clock

blank enables the clock

Description

This function is used to enable or disable the profile clock.

Synchronous

Synchronous from GEL: Yes

Completely synchronous: Yes

Example

GEL_EnableClock(); //Enable Clock

GEL_EnableClock(0); //Disable Clock

GEL_EnableClock(1); //Enable Clock