7.7.6.30. GEL_Go()ΒΆ

Runs to specified address.

Syntax

GEL_Go( [address] );

Parameters

address(optional) is the stop address.

Description

The GEL_Go function executes code up to a specific point in the program. The address Parameters is treated as a program-memory address. If you do not supply an address, then GEL_Go becomes equivalent to the GEL_Run GEL function.

Synchronous

Synchronous from GEL: Yes, only if location is given

Completely synchronous: Yes, only if location is given

Example

GEL_Go();
GEL_Go(main);

Related Topics

GEL_Run

GEL_Halt