7.7.6.68. GEL_RemoveInputFile()ΒΆ
Removes input file from the breakpoint at the specified address.
Syntax
GEL_RemoveInputFile(programAddr, "connectFileName");
Removes input file from the breakpoint in the specified file.
Syntax
GEL_RemoveInputFile("srcFileName", lineNumber, "connectFileName");
Parameters
programAddran expression specifying the memory location of the breakpoint to be removed. This expression should not be enclosed in quotation marks.
srcFileNamea string value specifying the filename (without path) of the source file in which the breakpoint to be removed is located. A double backslash escape sequence is required to ensure that a backslash is inserted into the filename; for example: "c:\ti\myprojects\sine.dat".
lineNumbera long integer value specifying the line number in said file at which the breakpoint to be removed is located.
connectFileNamea string value specifying the full path and filename of the file connected with the breakpoint. This connection will be severed and the file closed. A double backslash escape sequence is required to ensure that a backslash is inserted into the filename; for example: "c:\ti\myprojects\sine.dat".
Description
This function disconnects the specified file from the appropriate breakpoint, puts the corresponding input FileI/O object into the Stopped state, closes the input file, and removes the breakpoint (whether or not it was originally added by a call to GEL_AddInputFile).
Synchronous
Synchronous from GEL: Yes
Completely synchronous: No
Related Topics