PMBus¶
The PMBus software library is a C28x target mode only communications software stack. The PMBus target communication stack is based on PMBus specification (Part I, II) v1.2.
Within the communications software stack, the PMBus target state machine is implemented and is provided as pre-built binary as well as source code. Additionally, device-specific controller and target examples are provided to demonstrate usage of the software stack. PMBus library can be found in the folder libraries/communications/PMBus/c28 of the C2000Ware installation.