TI-RTOS for SimpleLink Wireless MCUs  2.14.02.22
File List
Here is a list of all files with brief descriptions:
 Camera.hCamera driver interface
 CameraCC3200DMA.hCamera driver implementation for a CC3200 Camera controller
 ClockP.hClock interface for the RTOS Porting Interface
 CryptoCC26XX.hCrypto driver implementation for a CC26XX Crypto controller
 DebugP.hDebug support
 GPIO.hGPIO driver
 GPIOCC3200.hCC3200 GPIO driver
 GPIOMSP430.hMSP430 GPIO driver
 GPIOMSP432.hMSP432 GPIO driver
 GPIOTiva.hTiva GPIO driver
 HwiP.hHardware Interrupt module for the RTOS Porting Interface
 I2C.hI2C driver interface
 I2CCC26XX.hI2C driver implementation for a CC26XX I2C controller
 I2CCC3200.hI2C driver implementation for a CC3200 I2C controller
 I2CEUSCIB.hI2CEUSCIB driver implementation for a USCIB controller
 I2CMSP432.hI2C driver implementation for the EUSCI controller on MSP432
 I2CTiva.hI2C driver implementation for a Tiva I2C controller
 I2CUSCIB.hI2CUSCIB driver implementation for a USCIB controller
 I2S.hI2S driver interface
 I2SCC3200DMA.hI2S driver implementation for a CC3200 I2S controller
 LCDDogm1286.hLCD driver implementation for a DOGM128W-6 LCD display
 LCDDogm1286_util.h
 MutexP.hMutex module for the RTOS Porting Interface
 PIN.hGeneric PIN & GPIO driver
 PINCC26XX.hDevice-specific pin & GPIO driver for CC26xx family [def]
 Power.hPower manager interface
 PowerCC3200.hPower manager interface for the CC3200
 PowerMSP432.hPower manager interface for the MSP432
 PWM.hPWM driver interface
 PWMTimerCC3200.hPWM driver implementation using CC3200 General Purpose Timer peripherals
 PWMTimerMSP432.hPWM driver implementation
 PWMTimerTiva.hPWM driver implementation using Tiva General Purpose Timer peripherals
 PWMTiva.hPWM driver implementation for Tiva PWM perhiperals
 RF.hRF driver for the CC26/13xx family
 SDSPI.hSDSPI driver interface
 SDSPICC3200.hSDSPI driver implementation for a CC3200 SPI peripheral used with the SDSPI driver
 SDSPIEUSCIA.hSDSPI driver implementation for a USCI SPI peripheral used with the SDSPI driver
 SDSPIEUSCIB.hSDSPI driver implementation for a USCI SPI peripheral used with the SDSPI driver
 SDSPIMSP432.hSDSPI driver implementation using an EUSCI SPI peripheral for MSP432
 SDSPITiva.hSDSPI driver implementation for a Tiva SPI peripheral used with the SDSPI driver
 SDSPIUSCIA.hSDSPI driver implementation for a USCI SPI peripheral used with the SDSPI driver
 SDSPIUSCIB.hSDSPI driver implementation for a USCI SPI peripheral used with the SDSPI driver
 SemaphoreP.hSemaphore module for the RTOS Porting Interface
 SPI.hSPI driver interface
 SPICC26XXDMA.hSPI driver implementation for a CC26XX SPI controller using the UDMA controller
 SPICC3200DMA.hSPI driver implementation for a CC3200 SPI controller using the micro DMA controller
 SPIEUSCIADMA.hSPI driver implementation for a USCIA peripheral using the micro DMA controller
 SPIEUSCIBDMA.hSPI driver implementation for a USCIB peripheral using the micro DMA controller
 SPIMSP432DMA.hSPI driver implementation for a EUSCI peripheral on MSP432 using the micro DMA controller
 SPITivaDMA.hSPI driver implementation for a TivaSPIcontroller using the micro DMA controller
 SPIUSCIADMA.hSPI driver implementation for a USCIA peripheral using the micro DMA controller
 SPIUSCIBDMA.hSPI driver implementation for a USCIB peripheral using the micro DMA controller
 UART.hUART driver interface
 UARTCC26XX.hUART driver implementation for a CC26XX UART controller
 UARTCC3200.hUART driver implementation for a CC3200 UART controller
 UARTCC3200DMA.hUART driver implementation for a CC3200 UART controller, using the micro DMA controller
 UARTEUSCIA.hUART driver implementation for a EUSCIA peripheral
 UARTMSP432.hUART driver implementation for a EUSCIA peripheral for MSP432
 UARTTiva.hUART driver implementation for a Tiva UART controller
 UARTTivaDMA.hUART driver implementation for a Tiva UART controller thay uses DMA
 UARTUSCIA.hUART driver implementation for a USCIA peripheral
 UDMACC26XX.hUDMACC26XX driver implementation
 Watchdog.hWatchdog driver interface
 WatchdogCC26XX.hWatchdog driver implementation for CC26XX
 WatchdogCC3200.hWatchdog driver implementation for CC3200
 WatchdogMSP430.hWatchdog driver implementation for MSP430
 WatchdogMSP432.hWatchdog driver implementation for MSP432
 WatchdogTiva.hWatchdog driver implementation for Tiva
Copyright 2015, Texas Instruments Incorporated