50 #ifndef ti_drivers_sdspi_SDSPIUSCIB__include
51 #define ti_drivers_sdspi_SDSPIUSCIB__include
66 #include <ti/sysbios/fatfs/ff.h>
67 #include <ti/sysbios/fatfs/diskio.h>
SDSPIUSCIB_CardType
SD Card type inserted.
Definition: SDSPIUSCIB.h:75
DSTATUS diskState
Definition: SDSPIUSCIB.h:154
uint8_t portMOSI
Definition: SDSPIUSCIB.h:140
uint32_t pinSCK
Definition: SDSPIUSCIB.h:137
Definition: SDSPIUSCIB.h:77
struct SDSPIUSCIB_HWAttrs SDSPIUSCIB_HWAttrs
Definition: SDSPIUSCIB.h:78
SDSPIUSCIB Object.
Definition: SDSPIUSCIB.h:152
struct SDSPIUSCIB_Object * SDSPIUSCIB_Handle
The definition of a SDSPI function table that contains the required set of functions to control a spe...
Definition: SDSPI.h:222
FATFS filesystem
Definition: SDSPIUSCIB.h:157
uint32_t pinMOSI
Definition: SDSPIUSCIB.h:141
uint16_t driveNumber
Definition: SDSPIUSCIB.h:153
SDSPIUSCIB Hardware attributes.
Definition: SDSPIUSCIB.h:132
uint32_t pinCS
Definition: SDSPIUSCIB.h:144
struct SDSPIUSCIB_Object SDSPIUSCIB_Object
SDSPIUSCIB Object.
uint8_t portCS
Definition: SDSPIUSCIB.h:143
uint8_t portMISO
Definition: SDSPIUSCIB.h:138
uint32_t bitRate
Definition: SDSPIUSCIB.h:156
SDSPIUSCIB_CardType cardType
Definition: SDSPIUSCIB.h:155
Definition: SDSPIUSCIB.h:76
uint32_t pinMISO
Definition: SDSPIUSCIB.h:139
const SDSPI_FxnTable SDSPIUSCIB_fxnTable
uint32_t baseAddr
Definition: SDSPIUSCIB.h:133
uint8_t portSCK
Definition: SDSPIUSCIB.h:136
uint8_t clockSource
Definition: SDSPIUSCIB.h:134
Definition: SDSPIUSCIB.h:79