TI-RTOS for SimpleLink Wireless MCUs  2.14.02.22
Data Structures
Here are the data structures with brief descriptions:
 CCamera_ConfigCamera Global configuration
 CCamera_FxnTableThe definition of a Camera function table that contains the required set of functions to control a specific Camera driver implementation
 CCamera_ParamsCamera Parameters
 CCameraCC3200DMA_HWAttrsCameraCC3200DMA Hardware attributes
 CCameraCC3200DMA_ObjectCameraCC3200DMA Object
 CClockP_FreqHzFrequency-in-hertz struct
 CClockP_ParamsBasic ClockP Parameters
 CCryptoCC26XX_AESCCM_TransactionCryptoCC26XX AES-CCM Transaction
 CCryptoCC26XX_AESECB_TransactionCryptoCC26XX AES-ECB Transaction
 CCryptoCC26XX_ConfigCryptoCC26XX Global Configuration
 CCryptoCC26XX_HWAttrsCryptoCC26XX Hardware Attributes
 CCryptoCC26XX_ObjectCryptoCC26XX Object
 CCryptoCC26XX_ParamsCryptoCC26XX Parameters
 CCryptoCC26XX_TransactionCryptoCC26XX Transaction
 CGPIOCC3200_ConfigGPIO device specific driver configuration structure
 CGPIOMSP430_ConfigGPIO device specific driver configuration structure
 CGPIOMSP432_ConfigGPIO device specific driver configuration structure
 CGPIOTiva_ConfigGPIO device specific driver configuration structure
 CHwiP_ParamsBasic HwiP Parameters
 CI2C_ConfigI2C Global configuration
 CI2C_FxnTableThe definition of a I2C function table that contains the required set of functions to control a specific I2C driver implementation
 CI2C_ParamsI2C Parameters
 CI2C_TransactionI2C transaction
 CI2CCC26XX_HWAttrsI2CCC26XX Hardware attributes
 CI2CCC26XX_I2CPinCfgI2CCC26XX Pin Configuration
 CI2CCC26XX_ObjectI2CCC26XX Object
 CI2CCC3200_HWAttrsI2CCC3200 Hardware attributes
 CI2CCC3200_ObjectI2CCC3200 Object
 CI2CEUSCIB_HWAttrsI2CEUSCIB Hardware attributes
 CI2CEUSCIB_ObjectI2CEUSCIB Object
 CI2CMSP432_HWAttrsI2CMSP432 Hardware attributes These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP430Ware these definitions are found in:
 CI2CMSP432_ObjectI2CMSP432 Object
 CI2CTiva_HWAttrsI2CTiva Hardware attributes
 CI2CTiva_ObjectI2CTiva Object
 CI2CUSCIB_HWAttrsI2CUSCIB Hardware attributes
 CI2CUSCIB_ObjectI2CUSCIB Object
 CI2S_BufDescI2S buffer descriptor for issue/reclaim mode
 CI2S_ConfigI2S Global configuration
 CI2S_FxnTableThe definition of a I2S function table that contains the required set of functions to control a specific I2S driver implementation
 CI2S_ParamsBasic I2S Parameters
 CI2SCC3200DMA_HWAttrsI2SCC3200DMA Hardware attributes
 CI2SCC3200DMA_ObjectI2SCC3200DMA Object
 CI2SCC3200DMA_SerialPinConfigCC3200 Serial Pin Configuration
 CI2SCC3200DMA_SerialPinParamsCC3200 specific I2S Parameters
 CI2SCC3200DMA_SerialPinVarsI2SCC3200DMA Serial pin variables
 CLCD_BufferLCD_Buffer used to store data to be printed on the LCD display
 CLCD_CommandFormat of LCD commands used by the LCD controller
 CLCD_ConfigThe LCD_Config structure contains a set of pointers used to characterize the LCD driver implementation
 CLCD_HWAttrsLCD Hardware attributes
 CLCD_ObjectLCD Object
 CLCD_ParamsLCD Parameters are used to with the LCD_open() call. Default values for these parameters are set using LCD_Params_init()
 CMutexP_ParamsBasic MutexP Parameters
 CPIN_State_sUnderlying data structure for type PIN_State
 CPower_NotifyObjPower notify object structure
 CPowerCC3200_ConfigPower global configuration
 CPowerCC3200_MCURegistersMCU core registers that need to be save on entering LPDS
 CPowerCC3200_ModuleStateInternal module state
 CPowerCC3200_NVICRegistersNVIC registers that need to be save on entering LPDS
 CPowerCC3200_SaveRegistersStruct of context registers to save on entering LPDS
 CPowerCC3200_WakeupFor wakeup from LPDS or shutdown configuration
 CPowerMSP432_ConfigPower global configuration (MSP432-specific)
 CPowerMSP432_FreqsStructure holding device frequencies (in Hz)
 CPWM_ConfigPWM Global configuration
 CPWM_FxnTableThe definition of a PWM function table that contains the required set of functions to control a specific PWM driver implementation
 CPWM_ParamsPWM Parameters
 CPWMTimerCC3200_HWAttrsPWMTimerCC3200 Hardware attributes
 CPWMTimerCC3200_ObjectPWMTimerCC3200 Object
 CPWMTimerMSP432_HWAttrsPWMTimerMSP432 Hardware attributes
 CPWMTimerMSP432_ObjectPWMTimerMSP432 Object
 CPWMTimerMSP432_StatusPWMTimerMSP432_Status
 CPWMTimerTiva_HWAttrsPWMTimerCC3200 Hardware attributes
 CPWMTimerTiva_ObjectPWMTimerTiva Object
 CPWMTiva_HWAttrsPWMTiva Hardware attributes
 CPWMTiva_ObjectPWMTiva Object
 CPWMTiva_StatusPWMTiva_Status
 CRF_ModeStruct defining operating mode of RF driver
 CRF_ObjectStruct used to store RF client state and configuration Pointer to an RF_Object is used as handles (RF_Handle) in interactions with the RF driver
 CRF_ParamsRF parameter struct RF parameters are used with the RF_open() and RF_Params_init() call
 CRF_RadioSetupUnion of the different flavors of RADIO_SETUP commands
 CSDSPI_ConfigSDSPI Global configuration
 CSDSPI_FxnTableThe definition of a SDSPI function table that contains the required set of functions to control a specific SDSPI driver implementation
 CSDSPI_ParamsSDSPI Parameters
 CSDSPICC3200_HWAttrsSDSPICC3200 Hardware attributes
 CSDSPICC3200_ObjectSDSPICC3200 Object
 CSDSPIEUSCIA_HWAttrsSDSPIEUSCIA Hardware attributes
 CSDSPIEUSCIA_ObjectSDSPIEUSCIA Object
 CSDSPIEUSCIB_HWAttrsSDSPIEUSCIB Hardware attributes
 CSDSPIEUSCIB_ObjectSDSPIEUSCIB Object
 CSDSPIMSP432_HWAttrsSDSPIMSP432 Hardware attributes
 CSDSPIMSP432_ObjectSDSPIMSP432 Object
 CSDSPITiva_HWAttrsSDSPITiva Hardware attributes
 CSDSPITiva_ObjectSDSPITiva Object
 CSDSPIUSCIA_HWAttrsSDSPIUSCIA Hardware attributes
 CSDSPIUSCIA_ObjectSDSPIUSCIA Object
 CSDSPIUSCIB_HWAttrsSDSPIUSCIB Hardware attributes
 CSDSPIUSCIB_ObjectSDSPIUSCIB Object
 CSemaphoreP_ParamsBasic SemaphoreP Parameters
 CSPI_ConfigSPI Global configuration
 CSPI_FxnTableThe definition of a SPI function table that contains the required set of functions to control a specific SPI driver implementation
 CSPI_ParamsSPI Parameters
 CSPI_TransactionA SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat frames are sent and received from the buffers pointed to txBuf and rxBuf. The arg variable is an user-definable argument which gets passed to the SPI_CallbackFxn when the SPI driver is in SPI_MODE_CALLBACK
 CSPICC26XX_HWAttrsSPICC26XXDMA Hardware attributes
 CSPICC26XX_ObjectSPICC26XXDMA Object
 CSPICC3200DMA_HWAttrsSPICC3200DMA Hardware attributes
 CSPICC3200DMA_ObjectSPICC3200DMA Object
 CSPIEUSCIADMA_HWAttrsSPIEUSCIADMA Hardware attributes
 CSPIEUSCIADMA_ObjectSPIEUSCIADMA Object
 CSPIEUSCIBDMA_HWAttrsSPIEUSCIBDMA Hardware attributes
 CSPIEUSCIBDMA_ObjectSPIEUSCIBDMA Object
 CSPIMSP432DMA_HWAttrsSPIMSP432DMA Hardware attributes These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP430Ware these definitions are found in:
 CSPIMSP432DMA_ObjectSPIMSP432DMA Object
 CSPITivaDMA_HWAttrsSPITivaDMA Hardware attributes
 CSPITivaDMA_ObjectSPITivaDMA Object
 CSPIUSCIADMA_HWAttrsSPIUSCIADMA Hardware attributes
 CSPIUSCIADMA_ObjectSPIUSCIADMA Object
 CSPIUSCIBDMA_HWAttrsSPIUSCIBDMA Hardware attributes
 CSPIUSCIBDMA_ObjectSPIUSCIBDMA Object
 CUART_ConfigUART Global configuration
 CUART_FxnTableThe definition of a UART function table that contains the required set of functions to control a specific UART driver implementation
 CUART_ParamsUART Parameters
 CUARTCC26XX_HWAttrsUARTCC26XX Hardware attributes
 CUARTCC26XX_ObjectUARTCC26XX Object
 CUARTCC3200_FxnSetComplement set of read functions to be used by the UART ISR and UARTCC3200_read(). Internal use only
 CUARTCC3200_HWAttrsUARTCC3200 Hardware attributes
 CUARTCC3200_ObjectUARTCC3200 Object
 CUARTCC3200DMA_HWAttrsUARTCC3200DMA Hardware attributes
 CUARTCC3200DMA_ObjectUARTCC3200DMA Object
 CUARTEUSCIA_BaudrateConfigUARTEUSCIA Baudrate configuration
 CUARTEUSCIA_HWAttrsUARTEUSCIA Hardware attributes
 CUARTEUSCIA_ObjectUARTEUSCIA Object
 CUARTMSP432_BaudrateConfigUARTMSP432 Baudrate configuration
 CUARTMSP432_FxnSetComplement set of read functions to be used by the UART ISR and UARTMSP432_read(). Internal use only
 CUARTMSP432_HWAttrsUARTMSP432 Hardware attributes
 CUARTMSP432_ObjectUARTMSP432 Object
 CUARTTiva_FxnSetComplement set of read functions to be used by the UART ISR and UARTTiva_read(). Internal use only
 CUARTTiva_HWAttrsUARTTiva Hardware attributes
 CUARTTiva_ObjectUARTTiva Object
 CUARTTivaDMA_HWAttrsUARTTivaDMA Hardware attributes
 CUARTTivaDMA_ObjectUARTTivaDMA Object
 CUARTUSCIA_BaudrateConfigUARTUSCIA Baudrate configuration
 CUARTUSCIA_HWAttrsUARTUSCIA Hardware attributes
 CUARTUSCIA_ObjectUARTUSCIA Object
 CUDMACC26XX_ConfigUDMACC26XX Global configuration
 CUDMACC26XX_HWAttrsUDMACC26XX hardware attributes
 CUDMACC26XX_ObjectUDMACC26XX object
 CWatchdog_ConfigWatchdog Global configuration
 CWatchdog_FxnTableThe definition of a Watchdog function table that contains the required set of functions to control a specific Watchdog driver implementation
 CWatchdog_ParamsWatchdog Parameters
 CWatchdogCC26XX_HWAttrsWatchdog hardware attributes for CC26XX
 CWatchdogCC26XX_ObjectWatchdog Object for CC26XX
 CWatchdogCC3200_HWAttrsWatchdog hardware attributes for CC3200
 CWatchdogCC3200_ObjectWatchdog Object for CC3200
 CWatchdogMSP430_HWAttrsWatchdog hardware attributes for MSP430
 CWatchdogMSP430_ObjectWatchdog Object for MSP430
 CWatchdogMSP432_HWAttrsWatchdog hardware attributes for MSP432 These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP432Ware these definitions are found in:
 CWatchdogMSP432_ObjectWatchdog Object for MSP432
 CWatchdogTiva_HWAttrsWatchdog hardware attributes for Tiva
 CWatchdogTiva_ObjectWatchdog Object for Tiva
Copyright 2015, Texas Instruments Incorporated