127 #ifndef ti_drivers_spi_SPIUSCIBDMA__include
128 #define ti_drivers_spi_SPIUSCIBDMA__include
137 #include <ti/sysbios/knl/Semaphore.h>
Semaphore_Struct transferComplete
Definition: SPIUSCIBDMA.h:206
SPI_Transaction * transaction
Definition: SPIUSCIBDMA.h:211
void(* SPI_CallbackFxn)(SPI_Handle handle, SPI_Transaction *transaction)
The definition of a callback function used by the SPI driver when used in SPI_MODE_CALLBACK.
Definition: SPI.h:264
SPI_TransferMode
SPI transfer mode determines the whether the SPI controller operates synchronously or asynchronously...
Definition: SPI.h:298
SPIUSCIBDMA Object.
Definition: SPIUSCIBDMA.h:203
uint8_t rxDMASourceTrigger
Definition: SPIUSCIBDMA.h:191
uint8_t * scratchBufPtr
Definition: SPIUSCIBDMA.h:182
The definition of a SPI function table that contains the required set of functions to control a speci...
Definition: SPI.h:384
SPI_TransferMode transferMode
Definition: SPIUSCIBDMA.h:208
struct SPIUSCIBDMA_Object SPIUSCIBDMA_Object
SPIUSCIBDMA Object.
struct SPIUSCIBDMA_Object * SPIUSCIBDMA_Handle
uint8_t rxDMAChannelIndex
Definition: SPIUSCIBDMA.h:189
A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat f...
Definition: SPI.h:244
uint32_t baseAddr
Definition: SPIUSCIBDMA.h:176
uint8_t defaultTxBufValue
Definition: SPIUSCIBDMA.h:184
const SPI_FxnTable SPIUSCIBDMA_fxnTable
SPI_CallbackFxn transferCallbackFxn
Definition: SPIUSCIBDMA.h:209
uint8_t bitOrder
Definition: SPIUSCIBDMA.h:180
uint32_t dmaBaseAddr
Definition: SPIUSCIBDMA.h:187
uint8_t txDMAChannelIndex
Definition: SPIUSCIBDMA.h:193
bool isOpen
Definition: SPIUSCIBDMA.h:204
uint8_t clockSource
Definition: SPIUSCIBDMA.h:178
struct SPIUSCIBDMA_HWAttrs SPIUSCIBDMA_HWAttrs
SPIUSCIBDMA Hardware attributes.
uint8_t txDMASourceTrigger
Definition: SPIUSCIBDMA.h:195
SPIUSCIBDMA Hardware attributes.
Definition: SPIUSCIBDMA.h:174