TI-RTOS for SimpleLink Wireless MCUs
2.14.02.22
|
I2C driver implementation for a CC3200 I2C controller.
============================================================================
The I2C header file should be included in an application as follows:
#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/I2C.h>
#include <ti/drivers/ports/HwiP.h>
#include <ti/drivers/ports/SemaphoreP.h>
#include <ti/drivers/Power.h>
Go to the source code of this file.
Data Structures | |
struct | I2CCC3200_HWAttrs |
I2CCC3200 Hardware attributes. More... | |
struct | I2CCC3200_Object |
I2CCC3200 Object. More... | |
Typedefs | |
typedef enum I2CCC3200_Mode | I2CCC3200_Mode |
I2CCC3200 mode. More... | |
typedef struct I2CCC3200_HWAttrs | I2CCC3200_HWAttrs |
I2CCC3200 Hardware attributes. More... | |
typedef struct I2CCC3200_Object | I2CCC3200_Object |
I2CCC3200 Object. More... | |
Enumerations | |
enum | I2CCC3200_Mode { I2CCC3200_IDLE_MODE = 0, I2CCC3200_WRITE_MODE, I2CCC3200_READ_MODE, I2CCC3200_ERROR = 0xFF } |
I2CCC3200 mode. More... | |
Variables | |
const I2C_FxnTable | I2CCC3200_fxnTable |
typedef enum I2CCC3200_Mode I2CCC3200_Mode |
I2CCC3200 mode.
This enum defines the state of the I2C driver's state-machine. Do not modify.
typedef struct I2CCC3200_HWAttrs I2CCC3200_HWAttrs |
I2CCC3200 Hardware attributes.
These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For CC3200Ware these definitions are found in:
A sample structure is shown below:
typedef struct I2CCC3200_Object I2CCC3200_Object |
I2CCC3200 Object.
The application must not access any member variables of this structure!
enum I2CCC3200_Mode |
const I2C_FxnTable I2CCC3200_fxnTable |