73 #ifndef ti_drivers_i2c_I2CEUSCIB__include
74 #define ti_drivers_i2c_I2CEUSCIB__include
84 #include <ti/sysbios/knl/Semaphore.h>
uint32_t baseAddr
Definition: I2CEUSCIB.h:126
I2CEUSCIB Hardware attributes.
Definition: I2CEUSCIB.h:124
Semaphore_Struct transferComplete
Definition: I2CEUSCIB.h:140
uint8_t * writeBufIdx
Definition: I2CEUSCIB.h:149
I2C_CallbackFxn transferCallbackFxn
Definition: I2CEUSCIB.h:143
void(* I2C_CallbackFxn)(I2C_Handle, I2C_Transaction *, bool)
I2C callback function.
Definition: I2C.h:248
I2C_TransferMode
I2C transfer mode.
Definition: I2C.h:230
struct I2CEUSCIB_HWAttrs I2CEUSCIB_HWAttrs
I2CEUSCIB Hardware attributes.
The definition of a I2C function table that contains the required set of functions to control a speci...
Definition: I2C.h:328
I2CEUSCIB_Mode
I2CEUSCIB mode.
Definition: I2CEUSCIB.h:95
Semaphore_Struct mutex
Definition: I2CEUSCIB.h:139
struct I2CEUSCIB_Object I2CEUSCIB_Object
I2CEUSCIB Object.
I2CEUSCIB Object.
Definition: I2CEUSCIB.h:136
uint8_t * readBufIdx
Definition: I2CEUSCIB.h:152
I2C_Transaction * headPtr
Definition: I2CEUSCIB.h:156
Definition: I2CEUSCIB.h:96
Definition: I2CEUSCIB.h:97
I2C_TransferMode transferMode
Definition: I2CEUSCIB.h:142
size_t writeCountIdx
Definition: I2CEUSCIB.h:150
uint8_t clockSource
Definition: I2CEUSCIB.h:128
const I2C_FxnTable I2CEUSCIB_fxnTable
I2C_Transaction * tailPtr
Definition: I2CEUSCIB.h:157
I2C transaction.
Definition: I2C.h:210
volatile I2CEUSCIB_Mode mode
Definition: I2CEUSCIB.h:145
I2C_Transaction * currentTransaction
Definition: I2CEUSCIB.h:147
Definition: I2CEUSCIB.h:98
Definition: I2CEUSCIB.h:99
bool isOpen
Definition: I2CEUSCIB.h:137
size_t readCountIdx
Definition: I2CEUSCIB.h:153