50 #ifndef ti_drivers_sdspi_SDSPIUSCIA__include
51 #define ti_drivers_sdspi_SDSPIUSCIA__include
66 #include <ti/sysbios/fatfs/ff.h>
67 #include <ti/sysbios/fatfs/diskio.h>
uint32_t pinSCK
Definition: SDSPIUSCIA.h:137
FATFS filesystem
Definition: SDSPIUSCIA.h:157
Definition: SDSPIUSCIA.h:77
uint8_t portMOSI
Definition: SDSPIUSCIA.h:140
uint8_t portSCK
Definition: SDSPIUSCIA.h:136
SDSPIUSCIA Object.
Definition: SDSPIUSCIA.h:152
SDSPIUSCIA Hardware attributes.
Definition: SDSPIUSCIA.h:132
uint32_t pinMISO
Definition: SDSPIUSCIA.h:139
uint32_t pinCS
Definition: SDSPIUSCIA.h:144
SDSPIUSCIA_CardType cardType
Definition: SDSPIUSCIA.h:155
The definition of a SDSPI function table that contains the required set of functions to control a spe...
Definition: SDSPI.h:222
struct SDSPIUSCIA_HWAttrs SDSPIUSCIA_HWAttrs
uint32_t bitRate
Definition: SDSPIUSCIA.h:156
uint8_t clockSource
Definition: SDSPIUSCIA.h:134
Definition: SDSPIUSCIA.h:79
enum SDSPIUSCIA_CartType SDSPIUSCIA_CardType
SD Card type inserted.
uint32_t baseAddr
Definition: SDSPIUSCIA.h:133
struct SDSPIUSCIA_Object SDSPIUSCIA_Object
SDSPIUSCIA Object.
uint32_t pinMOSI
Definition: SDSPIUSCIA.h:141
DSTATUS diskState
Definition: SDSPIUSCIA.h:154
uint8_t portMISO
Definition: SDSPIUSCIA.h:138
const SDSPI_FxnTable SDSPIUSCIA_fxnTable
SDSPIUSCIA_CartType
SD Card type inserted.
Definition: SDSPIUSCIA.h:75
uint16_t driveNumber
Definition: SDSPIUSCIA.h:153
Definition: SDSPIUSCIA.h:76
Definition: SDSPIUSCIA.h:78
uint8_t portCS
Definition: SDSPIUSCIA.h:143
struct SDSPIUSCIA_Object * SDSPIUSCIA_Handle