TI-RTOS for SimpleLink Wireless MCUs
2.14.02.22
|
UART driver implementation for a EUSCIA peripheral for MSP432.
============================================================================
The UARTMSP432 driver is (ring) buffered driver where it stores data it may already received in a user-supplied background buffer.
While permitted, it is STRONGLY suggested to avoid implementations where you call UART_read() within it own callback function (when in UART_MODE_CALLBACK).
Doing so, will require additional (task and system) stack for each nested UART_read() call.
Tool chain | Number of bytes per nested UART_read() call |
---|---|
GNU | 96 bytes + callback function stack requirements |
IAR | 40 bytes + callback function stack requirements |
TI | 80 bytes + callback function stack requirements |
It is important to note a potential worst case scenario: A full ring buffer with data; say 32 bytes The callback function calls UART_read() with a size of 1 (byte) No other variables are allocated in the callback function No other function calls are made in the callback function
As a result, you need an additional task and system stack of: 32 bytes * (80 bytes for TI + 0 bytes by the callback function) = 2.5kB
The UART header file should be included in an application as follows:
This UART driver implementation is designed to operate on a EUSCI controller in UART mode for MSP432 devices.
#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/ports/ClockP.h>
#include <ti/drivers/ports/HwiP.h>
#include <ti/drivers/ports/SemaphoreP.h>
#include <ti/drivers/Power.h>
#include <ti/drivers/UART.h>
#include <ti/drivers/uart/RingBuf.h>
Go to the source code of this file.
Data Structures | |
struct | UARTMSP432_FxnSet |
Complement set of read functions to be used by the UART ISR and UARTMSP432_read(). Internal use only. More... | |
struct | UARTMSP432_BaudrateConfig |
UARTMSP432 Baudrate configuration. More... | |
struct | UARTMSP432_HWAttrs |
UARTMSP432 Hardware attributes. More... | |
struct | UARTMSP432_Object |
UARTMSP432 Object. More... | |
Typedefs | |
typedef struct UARTMSP432_FxnSet | UARTMSP432_FxnSet |
Complement set of read functions to be used by the UART ISR and UARTMSP432_read(). Internal use only. More... | |
typedef struct UARTMSP432_BaudrateConfig | UARTMSP432_BaudrateConfig |
UARTMSP432 Baudrate configuration. More... | |
typedef struct UARTMSP432_HWAttrs | UARTMSP432_HWAttrs |
UARTMSP432 Hardware attributes. More... | |
typedef struct UARTMSP432_Object | UARTMSP432_Object |
UARTMSP432 Object. More... | |
typedef struct UARTMSP432_Object * | UARTMSP432_Handle |
Variables | |
const UART_FxnTable | UARTMSP432_fxnTable |
typedef struct UARTMSP432_FxnSet UARTMSP432_FxnSet |
Complement set of read functions to be used by the UART ISR and UARTMSP432_read(). Internal use only.
These functions should not be used by the user and are solely intended for the UARTMSP432 driver. The UARTMSP432_FxnSet is a pair of complement functions that are design to operate with one another in a task context and in an ISR context. The readTaskFxn is called by UARTMSP432_read() to drain a circular buffer, whereas the readIsrFxn is used by the UARTMSP432_hwiIntFxn to fill up the circular buffer.
readTaskFxn: Function called by UART read These variables are set and available for use to the readTaskFxn. object->readBuf = buffer; //Pointer to a user buffer object->readSize = size; //Desired no. of bytes to read object->readCount = size; //Remaining no. of bytes to read
readIsrFxn: The required ISR counterpart to readTaskFxn
typedef struct UARTMSP432_BaudrateConfig UARTMSP432_BaudrateConfig |
UARTMSP432 Baudrate configuration.
This structure is used to specifiy the EUSCI controller's clock divider settings to achieve the desired baudrate given the a clock input frequency. Divider values can be determined by referring to the MSP430 baudrate calculator. https://software-dl.ti.com/msp430/msp430_public_sw/mcu/msp430/MSP430BaudRateConverter/index.html
A sample structure is shown below:
typedef struct UARTMSP432_HWAttrs UARTMSP432_HWAttrs |
UARTMSP432 Hardware attributes.
These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP432Ware these definitions are found in:
A sample structure is shown below:
typedef struct UARTMSP432_Object UARTMSP432_Object |
UARTMSP432 Object.
The application must not access any member variables of this structure!
typedef struct UARTMSP432_Object * UARTMSP432_Handle |
const UART_FxnTable UARTMSP432_fxnTable |