SOC

The SOC driver provides API to configure SOC specific features like clocks.

Features Supported

  • API to enable/disable a module clock

  • API to set clock frequency for module

  • Generic utility API like get CPU clock, get core name string, control module MMR lock/unlock API

SysConfig Features

  • SOC driver is integrated with each of the drivers. User need not perform any explicit configuration for this driver

Features NOT Supported

NA

Important Usage Guidelines

  • Most of these APIs are already integrated with SysConfig tool and the generated code does the required call to enable a module, set the required clock and so on. User need to use these APIs in their application only for exceptional scenarios.

Example Usage

Include the below file to access the APIs

#include <drivers/soc.h>

Get Core Name String

    const char *coreName;

    coreName = SOC_getCoreName(CSL_CORE_ID_R5FSS0_0);
    DebugP_log("Core name is: %s\r\n", coreName);

Get CPU Clock Frequency

    uint64_t cpuClockRate;

    cpuClockRate = SOC_getSelfCpuClk();
    DebugP_log("CPU Clock Frequency: %u\r\n", cpuClockRate);

Set CPU Clock Frequency

    #include <drivers/sciclient.h> /* For the device and clock macros */

    uint32_t moduleId = TISCI_DEV_FSS0_OSPI_0;
    uint32_t clkId = TISCI_DEV_FSS0_OSPI_0_OSPI_RCLK_CLK;
    uint64_t clkRate = 200000000U;

    SOC_moduleSetClockFrequency(moduleId, clkId, clkRate);

Set CPU Clock Frequency with a specific parent clock

    #include <drivers/sciclient.h> /* For the device and clock macros */

    uint32_t moduleId = TISCI_DEV_FSS0_OSPI_0;
    uint32_t clkId = TISCI_DEV_FSS0_OSPI_0_OSPI_RCLK_CLK;
    uint32_t clkParentId = TISCI_DEV_FSS0_OSPI_0_OSPI_RCLK_CLK_PARENT_HSDIV4_16FFT_MAIN_0_HSDIVOUT1_CLK;
    uint64_t clkRate = 200000000U;

    SOC_moduleSetClockFrequencyWithParent(moduleId, clkId, clkParentId, clkRate);

API

group APIs for SOC Specific Functions

For more details and example usage, see DRIVERS_SOC_PAGE

SOC Domain ID

SOC_DOMAIN_ID_MAIN
SOC_DOMAIN_ID_MCU
SOC_DOMAIN_ID_WKUP

Unnamed Group

SOC_PSC_DOMAIN_ID_MAIN

\ SOC PSC Domain ID

SOC_PSC_DOMAIN_ID_MCU

SOC PSC Module State

SOC_PSC_SYNCRESETDISABLE
SOC_PSC_SYNCRESET
SOC_PSC_DISABLE
SOC_PSC_ENABLE

SOC PSC Domain State

SOC_PSC_DOMAIN_OFF
SOC_PSC_DOMAIN_ON

Defines

SOC_BOOTMODE_MMCSD

Switch value for SD card boot mode.

SOC_H_IO_DRVSTRNGTH0

IO Drive Strength Register offsets.

SOC_H_IO_DRVSTRNGTH2
SOC_V_IO_DRVSTRNGTH0
SOC_V_IO_DRVSTRNGTH2
SOC_IO_DRVSTRNGTH_MASK

IO Drive Strength field definitions.

SOC_IO_DRVSTRNGTH_MAX

Functions

int32_t SOC_moduleClockEnable(uint32_t moduleId, uint32_t enable)

Enable clock to specified module.

Parameters:
  • moduleId – [in] see tisci_devices for list of device ID’s

  • enable – [in] 1: enable clock to the module, 0: disable clock to the module

Returns:

SystemP_SUCCESS Module clock is enabled

Returns:

SystemP_FAILURE Module clock could not be enabled

int32_t SOC_moduleSetClockFrequencyWithParent(uint32_t moduleId, uint32_t clkId, uint32_t clkParent, uint64_t clkRate)

Set module clock to specified frequency and with a specific parent.

Parameters:
  • moduleId – [in] see tisci_devices for list of module ID’s

  • clkId – [in] see tisci_clocks for list of clocks associated with the specified module ID

  • clkParent – [in] see tisci_clocks for list of clock parents associated with the specified module ID

  • clkRate – [in] Frequency to set in Hz

Returns:

SystemP_SUCCESS Module clock is enabled

Returns:

SystemP_FAILURE Module clock could not be enabled

int32_t SOC_moduleSetClockFrequency(uint32_t moduleId, uint32_t clkId, uint64_t clkRate)

Set module clock to specified frequency.

Parameters:
  • moduleId – [in] see tisci_devices for list of module ID’s

  • clkId – [in] see tisci_clocks for list of clocks associated with the specified module ID

  • clkRate – [in] Frequency to set in Hz

Returns:

SystemP_SUCCESS Module clock is enabled

Returns:

SystemP_FAILURE Module clock could not be enabled

int32_t SOC_moduleGetClockFrequency(uint32_t moduleId, uint32_t clkId, uint64_t *clkRate)

Get module clock frequency.

Parameters:
  • moduleId – [in] see tisci_devices for list of module ID’s

  • clkId – [in] see tisci_clocks for list of clocks associated with the specified module ID

  • clkRate – [out] Frequency of the clock

Returns:

SystemP_SUCCESS on success, else failure

const char *SOC_getCoreName(uint16_t coreId)

Convert a core ID to a user readable name.

Parameters:

coreId – [in] see CSL_CoreID

Returns:

name as a string

uint64_t SOC_getSelfCpuClk(void)

Get the clock frequency in Hz of the CPU on which the driver is running.

Returns:

Clock frequency in Hz

void SOC_controlModuleLockMMR(uint32_t domainId, uint32_t partition)

Lock control module partition to prevent writes into control MMRs.

Parameters:
  • domainId – [in] See SOC_DomainId_t

  • partition – [in] Partition number to unlock

void SOC_controlModuleUnlockMMR(uint32_t domainId, uint32_t partition)

Unlock control module partition to allow writes into control MMRs.

Parameters:
  • domainId – [in] See SOC_DomainId_t

  • partition – [in] Partition number to unlock

void SOC_setEpwmTbClk(uint32_t epwmInstance, uint32_t enable)

Enable or disable ePWM time base clock from Control MMR.

Parameters:
  • epwmInstance – [in] ePWM instance number [0 - (CSL_EPWM_PER_CNT-1)]

  • enable – [in] TRUE to enable and FALSE to disable

void SOC_unlockAllMMR(void)

Unlocks all the control MMRs.

void SOC_setDevStat(uint32_t bootMode)

Change boot mode by setting devstat register.

Parameters:

bootMode – [IN] Boot mode switch value

void SOC_generateSwWarmResetMainDomain(void)

Generate SW Warm Reset Main Domain.

void SOC_generateSwPORResetMainDomain(void)

Generate SW POR Reset Main Domain.

uint32_t SOC_getWarmResetCauseMainDomain(void)

Get the reset reason source for Main Domain.

Returns:

Reset Reason Source Main Domain

void SOC_generateSwWarmResetMcuDomain(void)

Generate SW WARM Reset Mcu Domain.

void SOC_generateSwWarmResetMainDomainFromMcuDomain(void)

Generate SW WARM Reset Main Domain from Mcu Domain.

void SOC_generateSwPORResetMainDomainFromMcuDomain(void)

Generate SW POR Reset Main Domain from Mcu Domain.

uint32_t SOC_getWarmResetCauseMcuDomain(void)

Get the reset reason source for Mcu Domain.

Returns:

Reset Reason Source Mcu Domain

void SOC_clearResetCauseMainMcuDomain(uint32_t resetCause)

Clears reason for Warm and Main/Mcu Domain Power On Resets. CTRLMMR_RST_SRC is just a mirror of CTRLMMR_MCU_RST_SRC register. It is read only. So we need to write 1 to CTRLMMR_MCU_RST_SRC to clear the reset reason.

Parameters:

resetCause – [IN] Reset reason value to clear.

void SOC_triggerMcuLpmWakeup()

Generates the MCU IPC interrupt to DM R5 to wakeup the main domain from MCU only LPM mode.

int32_t SOC_enableResetIsolation(uint32_t main2McuIsolation, uint32_t mcu2MainIsolation, uint32_t mcu2dmIsolation, uint32_t debugIsolationEnable)

Enable reset isolation of MCU domain for safety applications.

Parameters:
  • main2McuIsolation – [IN] Flag to enable isolation of mcu domain from main domain Setting this flag restricts the access of MCU resources by main domain

  • mcu2MainIsolation – [IN] Flag to enable isolation of main domain from mcu domain Setting this flag restricts the access of MCU resources by main domain

  • mcu2dmIsolation – [IN] Flag to enable isolation of DM from mcu domain Setting this flag restricts the access of DM resources by MCU domain

  • debugIsolationEnable – [IN] Enable debug isolation. Setting this would restrict JTAG access to MCU domain

void SOC_setMCUResetIsolationDone(uint32_t value)

Set MCU reset isolation done flag.

Parameters:

value – [IN] : 0 - Allow main domain reset to propogate : 1 - Do not allow main domain reset to propogate

void SOC_waitMainDomainReset(void)

Wait for main domain reset to complete.

int32_t SOC_getPSCState(uint32_t instNum, uint32_t domainNum, uint32_t moduleNum, uint32_t *domainState, uint32_t *moduleState)

Get PSC (Power Sleep Controller) state.

Parameters:
  • instNum – [IN] : PSC Instance. See SOC_PSCDomainId_t

  • domainNum – [IN] : Power domain number

  • moduleNum – [IN] : Module number

  • domainState – [OUT] : Domain state (1 : ON, 0 : OFF)

  • moduleState – [OUT] : Module State. See SOC_PSCModuleState_t

Returns:

SystemP_SUCCESS on success, else failure

int32_t SOC_setPSCState(uint32_t instNum, uint32_t domainNum, uint32_t moduleNum, uint32_t pscState)

Set PSC (Power Sleep Controller) state.

Parameters:
  • instNum – [IN] : PSC Instance. See SOC_PSCDomainId_t

  • domainNum – [IN] : Power domain number

  • moduleNum – [IN] : Module number

  • pscState – [IN] : PSC module state. See SOC_PSCModuleState_t

Returns:

SystemP_SUCCESS on success, else failure

void SOC_setFSSCtrlFlashBootSize(void)

Update the boot block size for FSS subsystem.

Selects the size of the boot block to be used for the OSPI flash interface. Default value is 1’b0 - S0_BOOT_SIZE_64MB for the MMR register. Set 1’b1 - S0_BOOT_SIZE_128MB to update the value.

uint64_t Soc_getPhyAddr(uint64_t virtAddr)

Get Physical Address from virtual address.

Parameters:

virtAddr – [IN] : Virtual Address(Alias)

Returns:

Physical Address

void SOC_fixFastDriveStrength(void)

Fix fast mode drive strength.

Some devices have all drive strengths hardcoded to the nominal value. This function updates the drive strength registers on boot to the right values for fast drive strength. Only fast mode is supported and fixed.