Region based Address Translate

Features Supported

  • APIs to setup region based address translation using RAT HW on supported SOCs

  • APIs to translate 48b SOC view system addr to 32b local CPU view address.

  • When no address mapping is specified, no translation is done.

Features NOT Supported

NA

Important Usage Guidelines

  • The translation API AddrTranslateP_getLocalAddr is meant to be used to translate SOC specified peripheral MMR base addresses to local CPU accesible addresses, within device drivers. The API internally searches through a small array to find the address translations, hence to be efficient, this API should typically be called once during driver init to find the local address that CPU should use.

Errata i2449 - RAT MMR Parity Workaround (R5F only)

Values stored in Pulsar RAT MMRs are not parity protected in hardware. A bit flip in a RAT MMR would not be detected, allowing an unnoticed address translation corruption. This affects both transient (soft) and permanent (hard) errors.

Workaround

The software workaround is to periodically read back the RAT MMR values and compare them against the intended configuration. The SDK implements this via AddrTranslateP_readbackVerify.

Automatic check at init: AddrTranslateP_readbackVerify is called automatically at the end of AddrTranslateP_init as a post-write check, confirming the initial register writes succeeded.

Periodic runtime check: Applications requiring functional safety must call AddrTranslateP_readbackVerify periodically at runtime (for example from a periodic timer task or watchdog service routine) to detect any bit flip that occurs after initialization.

/* Example: call from a 1ms periodic safety task */
int32_t status = AddrTranslateP_readbackVerify();
if(status != SystemP_SUCCESS)
{
    /* RAT MMR mismatch detected - handle the error */
}
  • This module is needed for M4F to access peripherals on the MainSS side of the SOC.

Example Usage

Include the below file to access the APIs,

Example to translate a system address to local CPU address:

API Reference

Defines

AddrTranslateP_MAX_REGIONS

Maximum regions in the address translate module.

Enums

enum AddrTranslateP_RegionSize

Enum’s to represent different possible region size for the address translate module.

Values:

enumerator AddrTranslateP_RegionSize_1
enumerator AddrTranslateP_RegionSize_2
enumerator AddrTranslateP_RegionSize_4
enumerator AddrTranslateP_RegionSize_8
enumerator AddrTranslateP_RegionSize_16
enumerator AddrTranslateP_RegionSize_32
enumerator AddrTranslateP_RegionSize_64
enumerator AddrTranslateP_RegionSize_128
enumerator AddrTranslateP_RegionSize_256
enumerator AddrTranslateP_RegionSize_512
enumerator AddrTranslateP_RegionSize_1K
enumerator AddrTranslateP_RegionSize_2K
enumerator AddrTranslateP_RegionSize_4K
enumerator AddrTranslateP_RegionSize_8K
enumerator AddrTranslateP_RegionSize_16K
enumerator AddrTranslateP_RegionSize_32K
enumerator AddrTranslateP_RegionSize_64K
enumerator AddrTranslateP_RegionSize_128K
enumerator AddrTranslateP_RegionSize_256K
enumerator AddrTranslateP_RegionSize_512K
enumerator AddrTranslateP_RegionSize_1M
enumerator AddrTranslateP_RegionSize_2M
enumerator AddrTranslateP_RegionSize_4M
enumerator AddrTranslateP_RegionSize_8M
enumerator AddrTranslateP_RegionSize_16M
enumerator AddrTranslateP_RegionSize_32M
enumerator AddrTranslateP_RegionSize_64M
enumerator AddrTranslateP_RegionSize_128M
enumerator AddrTranslateP_RegionSize_256M
enumerator AddrTranslateP_RegionSize_512M
enumerator AddrTranslateP_RegionSize_1G
enumerator AddrTranslateP_RegionSize_2G
enumerator AddrTranslateP_RegionSize_4G

Functions

void AddrTranslateP_Params_init(AddrTranslateP_Params *params)

Set default value for address translate parameters.

Parameters:

params – [out] Structure initialized with default parameters

void AddrTranslateP_init(AddrTranslateP_Params *params)

Initialize Address translate sub-system, called by SysConfig, not to be called by end users.

Parameters:

params – [in] Initialization parameters

void AddrTranslateP_setRegion(uint32_t ratBaseAddr, uint16_t regionNum, uint64_t systemAddr, uint32_t localAddr, uint32_t size, uint32_t enable)

Configure a single RAT region at runtime.

Parameters:
  • ratBaseAddr – [in] Base address of the RAT HW module

  • regionNum – [in] RAT region number to configure

  • systemAddr – [in] 48b system (SOC) address, aligned to region size

  • localAddr – [in] CPU local address, aligned to region size

  • size – [in] Region size, see AddrTranslateP_RegionSize

  • enable – [in] 1 to enable the region, 0 to disable

void *AddrTranslateP_getLocalAddr(uint64_t systemAddr)

Translate from 48b system address to a CPU address as seen via the RAT module.

Note

If no mapping is found then lower 32b are returned as the local address, i.e no translation is done for 32b address, and address truncation for > 32b input addresses.

Note

All drivers MUST call this API to translate peripheral MMR base addresses to CPU visible base addr. It is recommended to call this once to get the base address during driver module init.

Parameters:

systemAddr – [in] 48b system address or SOC view address

Returns:

void * CPU view or local address

struct AddrTranslateP_RegionConfig
#include <AddrTranslateP.h>

Region config structure, this is used by SysConfig and not to be used by end-users directly.

Public Members

uint64_t systemAddr

translated 48b system addr as seen by the SOC, MUST align to region size

uint32_t localAddr

region start address as seen by the CPU, MUST align to region size

uint32_t size

region size, see AddrTranslateP_RegionSize

struct AddrTranslateP_Params
#include <AddrTranslateP.h>

Parameters for AddrTranslateP_init, this is used by SysConfig and not to be used by end-users directly.

Public Members

uint32_t numRegions

Number of regions to configure

uint32_t ratBaseAddr

Base address of the RAT HW module

AddrTranslateP_RegionConfig *regionConfig

Pointer to array of region config, number of array element MUST be >= numRegions