Dhrystone Benchmark
Introduction
Dhrystone is a synthetic benchmark that measures and compares processor performance.
The Dhrystone benchmark program contains 52 assignments, 33 control statements and 17 procedures/ function calls. Unlike Whetstone benchmarking, the program doesn’t contain floating point operation and concentrates on string handling and standard code, heavily influenced by hardware and software design, compiler and linker options, code optimizing, cache memory, wait states and integer data types. 103 statements are dynamically executed.
Supported Combinations
Parameter |
Value |
|---|---|
CPU + OS |
a53ss0-0 freertos |
Toolchain |
arm.gnu.aarch64-none |
Boards |
am62x-sk, am62x-sip-sk, am62x-sk-lp |
Example folder |
examples/benchmarks/dhrystone_benchmark |
Steps to Run the Example
When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
Sample output for Dhrystone benchmark example
\code BENCHMARK START - DHRYSTONE
Dhrystone Benchmark, Version 2.1 (Language: C)
BEGIN cycle count: 14
END Cycle count: 99582466
USER cycle count: 99582452
BENCHMARK Using clock 1400000000
Usertime in sec: 0.071130
Microseconds for one run through Dhrystone: 0.1
Dhrystones per Second: 7029351.2
Normalized MIPS/MHz: 2.8577 BENCHMARK END
All tests have passed. \endcode