SDL R5F ECC TCM

Introduction

This example demonstrates the usage of the SDL ECC on R5F TCM module. The example shows how to setup and use the ECC Safety Diagnostic operation. Shows the generation of SEC and DED error on R5F TCM.

Note

DM swaps ATCM and BTCM addresses. ATCM starts at 0x41010000 and BTCM starts at 0x0.

Use Cases

Use Case

Description

UC-1

Double bit error injection.

UC-2

Single bit error injection.

Supported Combinations

Parameter

Value

CPU + OS

r5fss0-0 nortos

Toolchain

ti-arm-clang

Board

am62x-sk

Example folder

examples/sdl/ecc_tcm/

Steps to Run the Example

See Also

ECC

Sample Output

Shown below is a sample output when the application is run,

\code

ECC TCM Example Application

ECC_Example_init: Init MAIN ESM complete

ECC_Example_init: Init WKUP ESM complete

AGGR ECC Init complete

ECC Safety Example tests: starting

B0TCM0 Bank0 Double bit error self test: starting B0TCM0 Bank0 Double bit error self test: pErrMem 0x00000000 fixed location once test complete Waiting for ESM Interrupt

UC-1: Got High priority ESM Interrupt

B0TCM0 Bank0 Single bit error inject test: starting

B0TCM0 Bank0 Single bit error inject test: at pErrMem 0x00000000: fixed location once test complete Waiting for ESM Interrupt

UC-2: Got Low priority ESM Interrupt

ECC Safety Example tests: success

ECC UC-1 and UC-2 Test

All tests have passed.

\endcode