SDL MCU ESM

Introduction

This example demonstrates High and Low priority events received from the MCU_ESM through the application-registered callback. It also shows routing and clearing of events to the MCU_SAFETY_ERRORn pin.

This example displays setting up ESM to

* Enable/Disable input events to the ESM module for each ESM instance
* Registration of application callback for ESM error events for each ESM instance
* Designating input events as high priority or low priority for each ESM instance
* Designating direct pin routing to MCU_SAFETY_ERRORn pin for external monitor communication

Use Cases

Use Case

Description

UC-0

Configuration of High Priority ESM

UC-1

Configuration of Config Priority ESM

UC-2

Configuration of Low Priority ESM

Supported Combinations

Parameter      | Value
---------------|-----------
CPU + OS       | r5fss0-0 nortos
^				| m4fss0-0 nortos
Toolchain      | ti-arm-clang
Board          | {{ VAR_BOARD_NAME_LOWER }}
Example folder | examples/sdl/mcu_esm0/

Steps to Run the Example

Sample Output

Shown below is a sample output when the application is run,

ESM Example Application

TIMER_ESM_init: Init MCU ESM complete

ESM example init complete
  Any clear of MCU_SAFETY_ERRORn pin will first wait 10 usecs
  Minimum Time Interval is 2000 usecs
ESM timer initialization complete

Starting Test Case 0

Use Case 0 completed: Input Event Trigger = Step completed successfully,
                       Event Handler Complete = Step completed successfully,
                       MCU_SAFETY_ERRORn Pin Clear = Step completed successfully

Starting Test Case 1

Use Case 1 completed: Input Event Trigger = Step completed successfully,
                       Event Handler Complete = Step completed successfully,
                       MCU_SAFETY_ERRORn Pin Clear = Step completed successfully

Starting Test Case 2

Use Case 2 completed: Input Event Trigger = Step completed successfully,
                       Event Handler Complete = Step completed successfully,
                       MCU_SAFETY_ERRORn Pin Clear = Step completed successfully


ESM Example Application summary
-------------------------------
Completed 3 Test Cases
Received 1 High Priority Interrupts
Received 1 Low Priority Interrupts
Received 1 Config Priority Interrupts

Test Case Event Log
------------------

Test Case 0: ESM Call back function called : grpChannel 0x2, index 0x1, intSrc 0x41
  ESM instance #1, ESM interrupt type = High Priority ESM event

Test Case 1: ESM Call back function called : grpChannel 0x1, index 0x0, intSrc 0x0
  ESM instance #1, ESM interrupt type = Config ESM event

Test Case 2: ESM Call back function called : grpChannel 0x1, index 0x3, intSrc 0x23
  ESM instance #1, ESM interrupt type = Low Priority ESM event

ESM Example Application: Complete
 All tests have passed!!