DDR PERF Test
Introduction
This example prints the read, write and total DDR bandwidth during memcpy operation. The memcpy operation is done on source and destination buffers allocated from DDR scratch region. The cache is disabled for this memory region. The values are calculated using the DDR performance counter registers available in DDR Subsystem. First performance counter is configured to count write operations and second one is configured to count read operations. The idle thread updates the DDR performance load stats.
Supported Combinations
Parameter |
Value |
|---|---|
CPU + OS |
r5fss0-0 freertos |
Toolchain |
ti-arm-clang |
Board |
am62x-sk, am62x-sk-lp, am62x-sip-sk |
Example folder |
examples/drivers/ddr/ddr_perf/ |
Steps to Run the Example
When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
Attention
As the wake-up R5 is the device manager, it needs to be started by the SBL. So it can not be loaded through CCS. It should be flashed and booted through SBL.
Refer Flash a Hello World example for flashing the application.
See Also
Sample Output
Shown below is a sample output when the application is run,
DDR performance statistics
==========================
DDR: READ BW: AVG = 285 MiB/s
DDR: WRITE BW: AVG = 323 MiB/s
DDR: TOTAL BW: AVG = 608 MiB/s
totalTime = 2354274
totalRead = 671249664
totalWrite = 761457664