MCASP Loopback
Introduction
This example demonstrates the McASP in loopback mode operation.
Mcasp is configured in TDM mode
Transfers data on single channel
Supported Combinations
Parameter |
Value |
|---|---|
CPU + OS |
a53ss0-0 freertos |
Toolchain |
arm.gnu.aarch64-none |
Board |
am62x-sk, am62x-sk-lp, am62x-sip-sk |
Example folder |
examples/drivers/mcasp/mcasp_loopback |
Steps to Run the Example
When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
See Also
Sample Output
Shown below is a sample output when the application is run,
[MCASP] Loopback example started. Testing 2560 bytes ...
All bytes match!!
All tests have passed!!
[MCASP] Loopback example started. Testing 100 bytes ...
All 100 bytes match!!