SBL SD

Introduction

If the appimage files are found at the location, the SBL reads the files into a buffer, parses it. Each core is then initialized, RPRC image is loaded, entry points are set and the core is released from reset. For more on bootflow/bootloaders, please refer Understanding the bootflow and bootloaders

This bootloader does SOC initializations and attempts to boot MCU M4 image by the name “app”, DM R5 image by the name “dm”, A530-0 image by the name “app_a530_0” and A530-1 image by the name “app_a530_1” present in the first FAT partition found in the connected SD card. The file can be copied to the SD card by connecting it to the host PC using a card reader. Make sure that the images are named without any file extension. If the card is new, make sure that it is formatted with FAT32/16.

If the appimage files are found at the location, the SBL reads the files into a buffer, parses it. Each core is then initialized, RPRC image is loaded, entry points are set and the core is released from reset. For more on bootflow/bootloaders, please refer Understanding the bootflow and bootloaders

This bootloader does SOC initializations and attempts to boot a multicore appimage file named “app” present in the first FAT partition found in the connected SD card. The file can be copied to the SD card by connecting it to the host PC using a card reader. Make sure that it is named “app” without any file extension. If the card is new, make sure that it is formatted with FAT32/16.

If a multicore appimage file is found at the location, the SBL reads the file into a buffer, parses it, splits it into RPRCs for each core applicable. Each core is then initialized, RPRC image is loaded, entry points are set and the core is released from reset. For more on bootflow/bootloaders, please refer Understanding the bootflow and bootloaders

Note

The default appimages in the SDK are built with authentication type 0 and load address 0x84000000. The gAppimage section in the bootloader application also has to be linked to the same address (0x84000000). If gAppimage section address is changed or multiple gAppimage buffers are used in the bootloader application, please ensure application’s makefile is also updated with the corresponding load address.

Supported Combinations

Parameter

Value

CPU + OS

r5fss0-0 nortos

Toolchain

ti-arm-clang

Boards

am62x-sk, am62x-sip-sk, am62x-sk-lp

Example folder

examples/drivers/boot/sbl_sd

Steps to Run the Example

Since this is a bootloader, the example will be run every time you boot an application using this example. It is run from an SD card unlike other examples which are usually loaded with CCS. Nevertheless, you can build this example like you do for the others using makefile or build it via CCS by importing as a project.

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).

  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)

  • Refer to the page Basic steps to flash files to flash this bootloader along with the application to boot.

See Also

BOOTLOADER

Sample Output

SYSFW Firmware Version 9.2.7--v09.02.07 (Kool Koala)
SYSFW Firmware revision 0x9
SYSFW ABI revision 3.1

[KPI] Boot Media       : SD Card
[KPI] Boot Image Size  : 198 KB
[KPI] Cores present    :
m4f0-0
r5f0-0
a530-0
[KPI] System_init                      :      33665us
[KPI] Board_init                       :          0us
[KPI] Drivers_open                     :     108146us
[KPI] Board_driversOpen                :          0us
[KPI] File read from SD card           :      10341us
[KPI] App_loadImages(CSL_CORE_ID_M4FSS0_0) :     152950us
[KPI] App_loadImages(CSL_CORE_ID_R5FSS0_0) :     141854us
[KPI] App_loadImages(CSL_CORE_ID_A53SS0_0) :     138552us
[KPI] SBL End                          :        150us
[KPI] SBL Total Time Taken             :     585663us

Image loading done, switching to application ...
[IPC RPMSG ECHO] Remote Core waiting for messages from main core ... !!!
[IPC RPMSG ECHO] Received and echoed 10 messages ... !!!
All tests have passed!!

SYSFW Firmware Version 9.2.7--v09.02.07 (Kool Koala)
SYSFW Firmware revision 0x9
SYSFW ABI revision 3.1

[KPI] Boot Media       : SD Card
[KPI] Boot Image Size  : 198 KB
[KPI] Cores present    :
m4f0-0
r5f0-0
a530-0
[KPI] System_init                      :      33597us
[KPI] Board_init                       :          0us
[KPI] Drivers_open                     :     108073us
[KPI] Board_driversOpen                :          0us
[KPI] File read from SD card           :      10335us
[KPI] App_loadImages(CSL_CORE_ID_M4FSS0_0) :     152960us
[KPI] App_loadImages(CSL_CORE_ID_R5FSS0_0) :     162888us
[KPI] App_loadImages(CSL_CORE_ID_A53SS0_0) :     159556us
[KPI] SBL End                          :        150us
[KPI] SBL Total Time Taken             :     627564us

Image loading done, switching to application ...
[IPC RPMSG ECHO] Remote Core waiting for messages from main core ... !!!
[IPC RPMSG ECHO] Received and echoed 10 messages ... !!!
All tests have passed!!
[KPI] SYSFW Load                       :      17632us
[KPI] System_init                      :      12246us
[KPI] Drivers_open                     :      82499us
[KPI] Board_driversOpen                :          0us
[KPI] File read from SD card           :       6843us
[KPI] CPU load                         :       9501us
[KPI] SBL Total Time Taken             :     129399us

Image loading done, switching to application ...