MMCSD

Attention

Please note that this driver is supported only on DM R5(WKUP R5) as part SBL examples. It is not supported on MCU-M4.

Multi-Media Card Secure Digital (MMCSD) peripheral is a driver which provides an interface with storage devices which follows MMC/SD/SDIO protocol. The driver supports single bit, four bit and eight bit data lines to communicate with the connected media.

The MMCSD controller provides accessibility to external MMC/SD/SDIO devices using a programmed IO method or DMA data transfer method. There are two MMCSD modules inside the SOC - MMCSD0 ,MMCSD1 and MMCSD2.

Features Supported

  • Integrated DMA Controller supporting SD Advanced DMA - SDMA, ADMA2 and ADMA3

  • 64-bit data, address width System Bus Interface

  • One controller with 8-bit wide data bus

  • Two controllers with 4-bit wide data bus

  • MMCSD0 supports eMMC 5.1, and also backward compatible withe earlier eMMC standards

  • MMCSD1 supports SD card HC 4.10 and SD Physical Layer v3.01, SDIO v3.00

SysConfig Features

Note

It is strongly recommend to use SysConfig where it is available instead of using direct SW API calls. This will help simplify the SW application and also catch common mistakes early in the development cycle.

Features not Supported

  • MMCSD0 does not support SD card, SDIO and voltages 3.0V and 1.2V.

  • MMCSD0 does not support HS400 DDR.

  • MMCSD1 does not support MMC card, UHS-II SD card and SDR50, DDR50 and SDR104.

  • The MMCSD driver doesn’t support interrupt mode.

  • The MMCSD driver doesn’t support 4-bit and 1-bit bus width transfers for eMMC and 1-bit bus width transfer for SD.

  • The default source impedance of 50 Ohms (Driver Type 0) is only supported for eMMC cards. Other driver types are not supported.

Example Usage

Include the below file to access the APIs

#include <stdio.h>
#include <drivers/mmcsd.h>

Instance Open Example

    MMCSD_Params mmcsdParams;

    MMCSD_Params_init(&mmcsdParams);
    gMmcsdHandle = MMCSD_open(0, &mmcsdParams);
    DebugP_assert(gMmcsdHandle != NULL);

Instance Close Example

    MMCSD_close(gMmcsdHandle);

API Reference

Refer to the MMCSD driver header file for detailed API information.