AM273x MCU+ SDK  09.02.00
hwa/v0/hwa.h File Reference

Introduction

HWA driver interface for HWA2.0.

Go to the source code of this file.

Data Structures

struct  HWA_Attrs
 HWA H/W Parameters. More...
 
struct  HWA_RAMAttrs
 HWA RAM Parameters. More...
 
struct  HWA_SrcDMAConfig
 Source trigger DMA parameters. More...
 
struct  HWA_CommonConfig
 HWA Common Config. More...
 
struct  HWA_SourceConfig
 HWA Paramset Config for Input Formatter/Source block. More...
 
struct  HWA_DestConfig
 HWA Paramset Config for Output Formatter/Destination block. More...
 
struct  HWA_PostProcStat
 HWA Paramset Config for post-processing and the statistics control registers. More...
 
struct  HWA_ComplexMultiply
 HWA Paramset Config for ComplexMultiply block. More...
 
struct  HWA_PreProcessing
 HWA Paramset Config for pre-processing block. More...
 
struct  HWA_AccelModeFFT
 HWA Paramset Config for FFT block. More...
 
struct  HWA_AccelModeCFAR
 HWA Paramset Config for CFAR block. More...
 
struct  HWA_AccelModeLocalMax
 HWA Paramset Config for Local maxima block. More...
 
struct  HWA_AccelModeCompress
 HWA Paramset Config for compression and decompression. More...
 
struct  HWA_ParamConfig
 HWA Paramset Config. More...
 
struct  HWA_InterruptConfig
 HWA Interrupt Config. More...
 
struct  HWA_Stats
 HWA Statistics from the STATISTICS block. More...
 
struct  HWA_AccmulatorVal
 HWA Accumulator register value data structure. More...
 
struct  HWA_DebugStats
 HWA Debug statistics. More...
 
struct  HWA_MemInfo
 HWA Local memory Information. More...
 
struct  HWA_CdfThreshold
 HWA Histogram Threshold RAM data structure. More...
 
struct  HWA_InterruptPriority
 HWA interrupt priority for HWA background thread done, ALT thread done, paramset done interrupt 1 and paramset done 2 interrupt. More...
 
struct  HWA_OpenConfig
 HWA configuration structure, which describes the configuration information, needed for hwa handle open. More...
 
struct  HWA_InterruptCtx
 HWA Interrupt context structure for paramset done interrupt. More...
 
struct  HWA_DoneInterruptCtx
 HWA Interrupt context structure for done interrupt. More...
 
struct  HWA_Object
 HWA driver internal Config. More...
 

Macros

#define HWADRV_ADDR_TRANSLATE_CPU_TO_HWA(x)   (uint32_t)((uint32_t)(x) & 0x000FFFFFU)
 transfer the CPU address to HWA address More...
 
#define HWA_ERRNO_BASE   (-2800)
 HWA driver error base. More...
 
#define HWA_EINVAL   (HWA_ERRNO_BASE-1)
 Error Code: Invalid argument. More...
 
#define HWA_ENOINIT   (HWA_ERRNO_BASE-2)
 Error Code: Operation cannot be done as HWA_init is not done. More...
 
#define HWA_EOUTOFRANGE   (HWA_ERRNO_BASE-3)
 Error Code: input argument out of range. More...
 
#define HWA_EOUTOFMEM   (HWA_ERRNO_BASE-4)
 Error Code: out of memory. More...
 
#define HWA_ENOTSUPP   (HWA_ERRNO_BASE-5)
 Error Code: feature not supported. More...
 
#define HWA_EINUSE   (HWA_ERRNO_BASE-6)
 Error Code: channel or resource in use. More...
 
#define HWA_ENOTALIGNED   (HWA_ERRNO_BASE-7)
 Error Code: address is not aligned to the expected boundary. More...
 
#define HWA_EINVAL_COMMON_REGISTER_PARAMSET   (HWA_ERRNO_BASE-8)
 Error Code: Invalid argument: paramset Start/Stop Idx and numLoops in common register. More...
 
#define HWA_EINVAL_COMMON_REGISTER_PARAMSET_ALT   (HWA_ERRNO_BASE-9)
 Error Code: Invalid argument: paramset Start/Stop Idx and numLoops for context switching in common register. More...
 
#define HWA_EINVAL_COMMON_REGISTER_FFTCONFIG   (HWA_ERRNO_BASE-10)
 Error Code: Invalid argument: for FFT config in common register. More...
 
#define HWA_EINVAL_COMMON_REGISTER_DCEST   (HWA_ERRNO_BASE-11)
 Error Code: Invalid argument: for DC estimation in common register. More...
 
#define HWA_EINVAL_COMMON_REGISTER_CFAR   (HWA_ERRNO_BASE-12)
 Error Code: Invalid argument: for CFAR config in common register. More...
 
#define HWA_EINVAL_COMMON_REGISTER_INTERFERENCE   (HWA_ERRNO_BASE-13)
 Error Code: Invalid argument: for interference localization/mitigation in common register. More...
 
#define HWA_EINVAL_COMMON_REGISTER_COMPLEXMULT   (HWA_ERRNO_BASE-14)
 Error Code: Invalid argument: for complex multiply in common register. More...
 
#define HWA_EINVAL_COMMON_REGISTER_CHANCOMB   (HWA_ERRNO_BASE-15)
 Error Code: Invalid argument: for channel combine in common register. More...
 
#define HWA_EINVAL_COMMON_REGISTER_ZEROINSERT   (HWA_ERRNO_BASE-16)
 Error Code: Invalid argument: for zero insert in common register. More...
 
#define HWA_EINVAL_COMMON_REGISTER_ADVSTAT   (HWA_ERRNO_BASE-17)
 Error Code: Invalid argument: for advanced statistics in common register. More...
 
#define HWA_EINVAL_COMMON_REGISTER_COMPRESS   (HWA_ERRNO_BASE-18)
 Error Code: Invalid argument: for compress/decompression in common register. More...
 
#define HWA_EINVAL_COMMON_REGISTER_LOCALMAXIMUM   (HWA_ERRNO_BASE-19)
 Error Code: Invalid argument: for local maximum in common register. More...
 
#define HWA_EINVAL_PARAMSET_GENERALCONFIG   (HWA_ERRNO_BASE - 20)
 Error Code: Invalid argument: general config in paramset
More...
 
#define HWA_EINVAL_PARAMSET_SOURCE   (HWA_ERRNO_BASE - 21)
 Error Code: Invalid argument: source(input formatter) in paramset. More...
 
#define HWA_EINVAL_PARAMSET_DEST   (HWA_ERRNO_BASE - 22)
 Error Code: Invalid argument: destination(output formatter) in paramset. More...
 
#define HWA_EINVAL_PARAMSET_SRCDST_ADDRESS   (HWA_ERRNO_BASE - 23)
 Error Code: Invalid argument: src and dst address in paramset. More...
 
#define HWA_EINVAL_PARAMSET_FFTMODE_GENERALCONFIG   (HWA_ERRNO_BASE - 24)
 Error Code: Invalid argument: FFT mode: general config in paramset. More...
 
#define HWA_EINVAL_PARAMSET_FFTMODE_SIZE   (HWA_ERRNO_BASE - 25)
 Error Code: Invalid argument: FFT mode: FFT size in paramset. More...
 
#define HWA_EINVAL_PARAMSET_FFTMODE_POSTPROC   (HWA_ERRNO_BASE - 26)
 Error Code: Invalid argument: FFT mode: post processing in paramset. More...
 
#define HWA_EINVAL_PARAMSET_FFTMODE_PREPROC   (HWA_ERRNO_BASE - 27)
 Error Code: Invalid argument: FFT mode: pre-processing in paramset. More...
 
#define HWA_EINVAL_PARAMSET_FFTMODE_PREPROC_INTERF   (HWA_ERRNO_BASE - 28)
 Error Code: Invalid argument: FFT mode: pre-processing interference localization/statistics/mitigation in paramset. More...
 
#define HWA_EINVAL_PARAMSET_FFTMODE_PREPROC_COMPLEXMULT   (HWA_ERRNO_BASE - 29)
 Error Code: Invalid argument: FFT mode: pre-processing complex multiply block in paramset. More...
 
#define HWA_EINVAL_PARAMSET_CFARMODE_GENERALCONFIG   (HWA_ERRNO_BASE - 30)
 Error Code: Invalid argument: CFAR mode: general configuration in paramset. More...
 
#define HWA_EINVAL_PARAMSET_CFARMODE_OSCONFIG   (HWA_ERRNO_BASE - 31)
 Error Code: Invalid argument: CFAR mode: CFAR-OS configuration in paramset. More...
 
#define HWA_EINVAL_PARAMSET_CFARMODE_CACONFIG   (HWA_ERRNO_BASE - 32)
 Error Code: Invalid argument: CFAR mode: CFAR-CA configuration in paramset. More...
 
#define HWA_EINVAL_PARAMSET_COMPRESSMODE   (HWA_ERRNO_BASE - 33)
 Error Code: Invalid argument: compress/decompress mode: compress/decompress configuration in paramset. More...
 
#define HWA_EINVAL_PARAMSET_LOCALMAXMODE   (HWA_ERRNO_BASE - 34)
 Error Code: Invalid argument: local maxima mode: local maxima configuration in paramset. More...
 
#define HWA_PARAMSET_POLLINGNOTALLOWED   (HWA_ERRNO_BASE - 35)
 Error Code: if paramset interrupt is enabled, polling should be disabled. More...
 
#define HWA_EINVAL_COMMON_REGISTER_CFAR_DET_THR   (HWA_ERRNO_BASE - 36)
 Error Code: Invalid argument: for CFAR config in common register - CFAR_DET_THR. More...
 
#define HWA_NUM_RXCHANNELS   (12U)
 Number of RX channels in pre-processing block. More...
 
#define HWA_NUM_INTERFMITG_WINARRAY   (5U)
 Number of programmable array of window parameters in interference mitigation block. More...
 
#define HWA_BPMPATTERN_LENGTH_INWORDS   (8U)
 The length of BPM Pattern sequence in words. More...
 
#define HWA_CHANCOMB_LENGTH_INWORDS   (8U)
 The length of channel combining vector in words. More...
 
#define HWA_ZEROINSERT_LENGTH_INWORDS   (8U)
 The length of zero insert mask in words. More...
 
#define HWA_NUM_RAMS   (10U)
 The number of RAM types in HWA. More...
 
#define HWA_MAXNUM_LOOPS   (4095U)
 The maximum number of loops in HWA. More...
 
#define HWA_CMP_K_ARR_LEN   (8U)
 The length of EGE compression/decompression K-paramseters array. More...
 
#define HWA_DONE_INTERRUPT_PRIORITY   (1U)
 Default HWA background thread done interrupt priority. More...
 
#define HWA_ALTDONE_INTERRUPT_PRIORITY   (1U)
 Default HWA background thread done interrupt priority. More...
 
#define HWA_PARAMSETDONE_INTERRUPT1_PRIORITY   (1U)
 Default HWA paramset done interrupt 1 priority. More...
 
#define HWA_PARAMSETDONE_INTERRUPT2_PRIORITY   (1U)
 Default HWA paramset done interrupt 2 priority. More...
 
#define HWA_LOCAL_RAM_ERR_PRIORITY   (1U)
 Default HWA local ram error interrupt priority. More...
 
#define HWA_FEATURE_BIT_ENABLE   ((uint8_t)1U)
 
#define HWA_FEATURE_BIT_DISABLE   ((uint8_t)0U)
 
#define HWA_SAMPLES_WIDTH_16BIT   ((uint8_t)0U)
 
#define HWA_SAMPLES_WIDTH_32BIT   ((uint8_t)1U)
 
#define HWA_SAMPLES_FORMAT_COMPLEX   ((uint8_t)0U)
 
#define HWA_SAMPLES_FORMAT_REAL   ((uint8_t)1U)
 
#define HWA_SAMPLES_UNSIGNED   ((uint8_t)0U)
 
#define HWA_SAMPLES_SIGNED   ((uint8_t)1U)
 
#define HWA_FFT_WINDOW_NONSYMMETRIC   ((uint8_t)0U)
 
#define HWA_FFT_WINDOW_SYMMETRIC   ((uint8_t)1U)
 
#define HWA_FFT_WINDOW_INTERPOLATE_MODE_NONE   ((uint8_t)0U)
 
#define HWA_FFT_WINDOW_INTERPOLATE_MODE_4K   ((uint8_t)2U)
 
#define HWA_FFT_WINDOW_INTERPOLATE_MODE_8K   ((uint8_t)1U)
 
#define HWA_FFT_MODE_MAGNITUDE_LOG2_DISABLED   ((uint8_t)0U)
 
#define HWA_FFT_MODE_MAGNITUDE_ONLY_ENABLED   ((uint8_t)2U)
 
#define HWA_FFT_MODE_MAGNITUDE_LOG2_ENABLED   ((uint8_t)3U)
 
#define HWA_FFT_MODE_OUTPUT_DEFAULT   ((uint8_t)0U)
 
#define HWA_FFT_MODE_OUTPUT_MAX_STATS   ((uint8_t)2U)
 
#define HWA_FFT_MODE_OUTPUT_SUM_STATS   ((uint8_t)3U)
 
#define HWA_NOISE_AVG_MODE_CFAR_CA   ((uint8_t)0U)
 
#define HWA_NOISE_AVG_MODE_CFAR_CAGO   ((uint8_t)1U)
 
#define HWA_NOISE_AVG_MODE_CFAR_CASO   ((uint8_t)2U)
 
#define HWA_NOISE_AVG_MODE_CFAR_OS   ((uint8_t)3U)
 
#define HWA_TRIG_MODE_IMMEDIATE   ((uint8_t)0U)
 
#define HWA_TRIG_MODE_SOFTWARE   ((uint8_t)1U)
 
#define HWA_TRIG_MODE_RESERVED1   ((uint8_t)2U)
 
#define HWA_TRIG_MODE_DMA   ((uint8_t)3U)
 
#define HWA_TRIG_MODE_HARDWARE   ((uint8_t)4U)
 
#define HWA_TRIG_MODE_RESERVED2   ((uint8_t)5U)
 
#define HWA_TRIG_MODE_RESERVED3   ((uint8_t)6U)
 
#define HWA_TRIG_MODE_SOFTWARE2   ((uint8_t)7U)
 
#define HWA_CONTEXTSWITCH_TRIG_MODE_DMA   ((uint8_t)3U)
 
#define HWA_CONTEXTSWITCH_TRIG_MODE_HARDWARE   ((uint8_t)4U)
 
#define HWA_CONTEXTSWITCH_TRIG_MODE_SOFTWARE   ((uint8_t)5U)
 
#define HWA_THREAD_BACKGROUNDCONTEXT   ((uint8_t)0U)
 
#define HWA_THREAD_ALTCONTEXT   ((uint8_t)1U)
 
#define HWA_ACCELMODE_FFT   ((uint8_t)0U)
 
#define HWA_ACCELMODE_CFAR   ((uint8_t)1U)
 
#define HWA_ACCELMODE_COMPRESS   ((uint8_t)2U)
 
#define HWA_ACCELMODE_LOCALMAX   ((uint8_t)3U)
 
#define HWA_ACCELMODE_NONE   ((uint8_t)7U)
 
#define HWA_CFAR_OPER_MODE_LOG_INPUT_REAL   0U
 
#define HWA_CFAR_OPER_MODE_LOG_INPUT_COMPLEX   1U
 
#define HWA_CFAR_OPER_MODE_MAG_INPUT_REAL   2U
 
#define HWA_CFAR_OPER_MODE_MAG_INPUT_COMPLEX   3U
 
#define HWA_CFAR_OPER_MODE_MAG_SQR_INPUT_REAL   4U
 
#define HWA_CFAR_OPER_MODE_MAG_SQR_INPUT_COMPLEX   5U
 
#define HWA_CFAR_OPER_MODE_LOG_INPUT_COMPLEX_LINEARCFAR   6U
 
#define HWA_CFAR_OUTPUT_MODE_I_nAVG_ALL_Q_CUT   ((uint8_t)0U)
 
#define HWA_CFAR_OUTPUT_MODE_I_nAVG_ALL_Q_DET_FLAG   ((uint8_t)1U)
 
#define HWA_CFAR_OUTPUT_MODE_I_PEAK_IDX_Q_NEIGHBOR_NOISE_VAL   ((uint8_t)2U)
 
#define HWA_CFAR_OUTPUT_MODE_I_PEAK_IDX_Q_CUT   ((uint8_t)3U)
 
#define HWA_CFAR_OUTPUT_MODE_FILTER_LARGE_PEAK   ((uint8_t)4U)
 
#define HWA_RAM_TYPE_WINDOW_RAM   ((uint8_t)0U)
 
#define HWA_RAM_TYPE_VECTORMULTIPLY_RAM   ((uint8_t)1U)
 
#define HWA_RAM_TYPE_LUT_FREQ_DEROTATE_RAM   ((uint8_t)2U)
 
#define HWA_RAM_TYPE_SHUFFLE_RAM   ((uint8_t)3U)
 
#define HWA_RAM_TYPE_HIST_THRESH_RAM   ((uint8_t)4U)
 
#define HWA_RAM_TYPE_2DSTAT_ITER_VAL   ((uint8_t)5U)
 
#define HWA_RAM_TYPE_2DSTAT_ITER_IDX   ((uint8_t)6U)
 
#define HWA_RAM_TYPE_2DSTAT_SAMPLE_VAL   ((uint8_t)7U)
 
#define HWA_RAM_TYPE_2DSTAT_SAMPLE_IDX   ((uint8_t)8U)
 
#define HWA_RAM_TYPE_HISTOGRAM_RAM   ((uint8_t)9U)
 
#define HWA_CLIPREG_TYPE_DCACC   ((uint8_t)0U)
 
#define HWA_CLIPREG_TYPE_DCEST   ((uint8_t)1U)
 
#define HWA_CLIPREG_TYPE_DCSUB   ((uint8_t)2U)
 
#define HWA_CLIPREG_TYPE_INTFSTATS_MAGACC   ((uint8_t)3U)
 
#define HWA_CLIPREG_TYPE_INTFSTATS_MAGDIFFACC   ((uint8_t)4U)
 
#define HWA_CLIPREG_TYPE_INTFSTATS_MAGTHRESHOLD   ((uint8_t)5U)
 
#define HWA_CLIPREG_TYPE_INTFSTATS_MAGDIFFTHRESHOLD   ((uint8_t)6U)
 
#define HWA_CLIPREG_TYPE_INTFSTATS_MAGSUM   ((uint8_t)7U)
 
#define HWA_CLIPREG_TYPE_INTFSTATS_MAGDIFFSUM   ((uint8_t)8U)
 
#define HWA_CLIPREG_TYPE_TWIDINCR_DELTAFRAC   ((uint8_t)9U)
 
#define HWA_CLIPREG_TYPE_CHANCOMB   ((uint8_t)10U)
 
#define HWA_CLIPREG_TYPE_FFT   ((uint8_t)11U)
 
#define HWA_CLIPREG_TYPE_INPUTFORMAT   ((uint8_t)12U)
 
#define HWA_CLIPREG_TYPE_OUTPUTFORMAT   ((uint8_t)13U)
 
#define HWA_ACCUMULATORREG_TYPE_DC   ((uint8_t)0U)
 
#define HWA_ACCUMULATORREG_TYPE_INTERF_MAG   ((uint8_t)1U)
 
#define HWA_ACCUMULATORREG_TYPE_INTERF_MAGDIFF   ((uint8_t)2U)
 
#define HWA_ACCUMULATORREG_TYPE_INTERF   ((uint8_t)3U)
 
#define HWA_INTERFERENCE_THRESHOLD_TYPE_MAG   ((uint8_t)0U)
 
#define HWA_INTERFERENCE_THRESHOLD_TYPE_MAGDIFF   ((uint8_t)1U)
 
#define HWA_PARAMDONE_INTERRUPT_TYPE_CPU_INTR1   ((uint8_t)1U)
 
#define HWA_PARAMDONE_INTERRUPT_TYPE_CPU_INTR2   ((uint8_t)2U)
 
#define HWA_PARAMDONE_INTERRUPT_TYPE_DMA   ((uint8_t)4U)
 
#define HWA_COMMONCONFIG_MASK_STATEMACHINE_CFG   ((uint64_t)0x00000001U)
 
#define HWA_COMMONCONFIG_MASK_STATEMACHINE_CFG_ALT   ((uint64_t)0x00000002U)
 
#define HWA_COMMONCONFIG_CONTEXTSWITCH_TRIG_CFG   ((uint64_t)0x00000004U)
 
#define HWA_COMMONCONFIG_MASK_BPMCFG   ((uint64_t)0x00000008U)
 
#define HWA_COMMONCONFIG_MASK_TWIDDITHERENABLE   ((uint64_t)0x00000010U)
 
#define HWA_COMMONCONFIG_MASK_LFSRSEED   ((uint64_t)0x00000020U)
 
#define HWA_COMMONCONFIG_MASK_FFTSUMDIV   ((uint64_t)0x00000040U)
 
#define HWA_COMMONCONFIG_MASK_CFARTHRESHOLDSCALE   ((uint64_t)0x00000080U)
 
#define HWA_COMMONCONFIG_MASK_DCEST_SCALESHIFT   ((uint64_t)0x00000100U)
 
#define HWA_COMMONCONFIG_MASK_DCSUB_SWVAL   ((uint64_t)0x00000200U)
 
#define HWA_COMMONCONFIG_MASK_INTERFMAG_THRESHOLD   ((uint64_t)0x00000400U)
 
#define HWA_COMMONCONFIG_MASK_INTERFMAGDIFF_THRESHOLD   ((uint64_t)0x00000800U)
 
#define HWA_COMMONCONFIG_MASK_INTERFSUM_MAG   ((uint64_t)0x00001000U)
 
#define HWA_COMMONCONFIG_MASK_INTERFSUM_MAGDIFF   ((uint64_t)0x00002000U)
 
#define HWA_COMMONCONFIG_MASK_COMPLEXMULT_SCALEARRAY   ((uint64_t)0x00004000U)
 
#define HWA_COMMONCONFIG_MASK_COMPLEXMULT_SCALECONST   ((uint64_t)0x00008000U)
 
#define HWA_COMMONCONFIG_MASK_RECWIN_RESET   ((uint64_t)0x00010000U)
 
#define HWA_COMMONCONFIG_MASK_TWIDINCR_DELTA_FRAC   ((uint64_t)0x00020000U)
 
#define HWA_COMMONCONFIG_MASK_CHANCOMB_VEC_SIZE   ((uint64_t)0x00400000U)
 
#define HWA_COMMONCONFIG_MASK_ZEROINSERT_NUM_MASK   ((uint64_t)0x00800000U)
 
#define HWA_COMMONCONFIG_MASK_MAX2D_OFFSETBOTHDIM   ((uint64_t)0x01000000U)
 
#define HWA_COMMONCONFIG_MASK_CDFCNT_THRESHOLD   ((uint64_t)0x02000000U)
 
#define HWA_COMMONCONFIG_MASK_LOCALMAXDIMB_THRESHOLDSW   ((uint64_t)0x04000000U)
 
#define HWA_COMMONCONFIG_MASK_LOCALMAXDIMC_THRESHOLDSW   ((uint64_t)0x08000000U)
 
#define HWA_COMMONCONFIG_MASK_LOCALMAXDIMBTHRESH_OFFSET   ((uint64_t)0x10000000U)
 
#define HWA_COMMONCONFIG_MASK_LOCALMAXDIMCTHRESH_OFFSET   ((uint64_t)0x20000000U)
 
#define HWA_COMMONCONFIG_MASK_INTERF_MITG_WINDOW_PARAM   ((uint64_t)0x40000000U)
 
#define HWA_COMMONCONFIG_MASK_EGECOMRESS_KPARAM   ((uint64_t)0x80000000U)
 
#define HWA_COMMONCONFIG_MASK_CFAR_DET_THR   ((uint64_t)0x1000000000U)
 
#define HWA_SRC_SHUFFLE_AB_MODE_DISABLE   ((uint8_t)0U) /** 0-disable */
 
#define HWA_SRC_SHUFFLE_AB_MODE_ADIM   ((uint8_t)1U) /** 1-SHUFFLE_LUT is used for sample index re-ordering in A dimension */
 
#define HWA_SRC_SHUFFLE_AB_MODE_BDIM   ((uint8_t)2U) /** 2- SHUFFLE_LUT is used in B-dimension */
 
#define HWA_COMPLEX_MULTIPLY_MODE_DISABLE   ((uint8_t)0U) /** 0-disable */
 
#define HWA_COMPLEX_MULTIPLY_MODE_FREQ_SHIFTER   ((uint8_t)1U) /** 1-Freq Shifter mode, see \ref HWA_ComplexMultiply::freqShiftTwiddleIncr */
 
#define HWA_COMPLEX_MULTIPLY_MODE_SLOW_DFT   ((uint8_t)2U) /** 2-slow DFT mode, see \ref HWA_CommonConfig::modeCfg::slowDFT::startFreq */
 
#define HWA_COMPLEX_MULTIPLY_MODE_FFT_STITCHING   ((uint8_t)3U) /** 3-FFT stitching mode, see \ref HWA_CommonConfig::modeCfg::FFTstitching::twiddlePattern and HWA_CommonConfig::modeCfg::FFTstitching::winInterpolateMode */
 
#define HWA_COMPLEX_MULTIPLY_MODE_MAG_SQUARED   ((uint8_t)4U) /** 4-Magnitude Squared mode */
 
#define HWA_COMPLEX_MULTIPLY_MODE_SCALAR_MULT   ((uint8_t)5U) /** 5-Scalar Multiplication mode, see \ref HWA_CommonConfig::modeCfg::scalerMultiply::scaleCmultScaleEn */
 
#define HWA_COMPLEX_MULTIPLY_MODE_VECTOR_MULT   ((uint8_t)6U) /** 6-Vector Multiplication mode, see \ref HWA_CommonConfig::modeCfg::vectorMultiplyMode1::cmultScaleEn and HWA_CommonConfig::modeCfg::vectorMultiplyMode1::ramAddrOffset */
 
#define HWA_COMPLEX_MULTIPLY_MODE_VECTOR_MULT_2   ((uint8_t)7U) /** 7-Vector Multiplication mode 2, see \ref HWA_CommonConfig::modeCfg::vectorMultiplyMode2::ramAddrOffset */
 
#define HWA_COMPLEX_MULTIPLY_MODE_RECURSIVE_WIN   ((uint8_t)8U) /** 8- recursive windowing mode, see \ref HWA_CommonConfig::modeCfg::recursiveWin::recwinModeSel */
 
#define HWA_COMPLEX_MULTIPLY_MODE_LUT_FREQ_DEROTATE   ((uint8_t)9U) /** 9- LUT based frequency de-rotation mode, see \ref HWA_CommonConfig::modeCfg::lutFreqDerotate::ramAddrOffset and HWA_CommonConfig::modeCfg::lutFreqDerotate::ramIdxIncrMode */
 
#define HWA_COMPLEX_MULTIPLY_MODE_FREQSHIFT_FREQINCREMENT   ((uint8_t)10U) /** 10 - frequency shifter mode with frequency increment, see \ref HWA_CommonConfig::complexMultiplyConfig::twiddleDeltaFrac and \ref HWA_ComplexMultiply::twiddleIncr*/
 
#define HWA_FFT_STITCHING_TWID_PATTERN_4K   ((uint8_t)1U) /** 4K fft stitching twid factor pattern */
 
#define HWA_FFT_STITCHING_TWID_PATTERN_8K   ((uint8_t)2U) /** 8K fft stitching twid factor pattern */
 
#define HWA_RECURSIVE_WIN_MODE_SELECT_ITERATION_COUNT   ((uint8_t)0U) /** iteration count */
 
#define HWA_FFT_STITCHING_TWID_PATTERN_EXE_COUNT   ((uint8_t)1U) /** execution count */
 
#define HWA_WINDOW_MODE_18BITREAL   ((uint8_t)0U)
 
#define HWA_WINDOW_MODE_16BITREAL   ((uint8_t)1U)
 
#define HWA_WINDOW_MODE_COMPLEX   ((uint8_t)2U)
 
#define HWA_FFT3x_BFLY_SCALING_MSBSATURATED   ((uint8_t)0U)
 
#define HWA_FFT3x_BFLY_SCALING_MSBSATLSBRND   ((uint8_t)1U)
 
#define HWA_FFT3x_BFLY_SCALING_LSBROUNDED   ((uint8_t)2U)
 
#define HWA_DCEST_INTERFSUM_RESET_MODE_NOUPDATE   ((uint8_t)0U) /** Hold the internal accumulators without updating */
 
#define HWA_DCEST_INTERFSUM_RESET_MODE_SOFTWARERESET   ((uint8_t)1U) /** free-running without automatic reset, software can reset the accumulators by writing to either DC_EST_RESET_SW register for DC accumulator, or INTF_STATUS_RESET_SW for interference statistics */
 
#define HWA_DCEST_INTERFSUM_RESET_MODE_PARAMRESET   ((uint8_t)2U) /** Reset the internal accumulators at the start of parameter set (i.e per chirp accumulation) */
 
#define HWA_DCEST_INTERFSUM_RESET_MODE_PARAMRESET_ZEROLPCONT   ((uint8_t)3U) /** Reset the internal accumulators at the start of parameter set only if loop counter is 0 (i.e per frame accumulation) */
 
#define HWA_INTERFTHRESH_MODE_MAG_OR_MAGDIF   ((uint8_t)0U) /** interference threshold magnitude or Magnitude difference */
 
#define HWA_INTERFTHRESH_MODE_MAGDIFF   ((uint8_t)1U) /** interference threshold only magnitude difference */
 
#define HWA_INTERFTHRESH_MODE_MAG   ((uint8_t)2U) /** interference threshold only magnitude */
 
#define HWA_INTERFTHRESH_MODE_MAG_AND_MAGDIFF   ((uint8_t)3U) /** interference threshold magnitude AND magnitude difference */
 
#define HWA_DCSUB_SELECT_DCSW   ((uint8_t)0U) /** DC subtracted value comes from user defined through DC_I_SW[12] and DC_Q_SW[12] register */
 
#define HWA_DCSUB_SELECT_DCEST   ((uint8_t)1U) /** DC subtracted value comes from built-in DC estimation hardware, DC_EST_I_VAL[12] and DC_EST_I_VAL[12] registers */
 
#define HWA_INTERFTHRESH_SELECT_SW
 
#define HWA_INTERFTHRESH_SELECT_EST_AVERAGE
 
#define HWA_INTERFTHRESH_SELECT_EST_INDIVIDUAL
 
#define HWA_INTERFMITIGATION_PATH_ZEROOUT   ((uint8_t)0U) /** select the zero-out path in the interference mitigation module */
 
#define HWA_INTERFMITIGATION_PATH_WINDOWZEROOUT   ((uint8_t)1U) /** select the windowed zero-out path in the interference mitigation module */
 
#define HWA_INTERFMITIGATION_PATH_LINEARINTERPOLATION   ((uint8_t)2U) /** select the linear interpolation path path in the interference mitigation module */
 
#define HWA_INTERFMITIGATION_PATH_UNUSED   ((uint8_t)3U) /** un-used mode in the interference mitigation module */
 
#define HWA_LUT_FREQ_DEROTATE_RAMIDX_AUTOINCR_WRAPAROUND   ((uint8_t)0U) /** auto-increment mode, with wrap around */
 
#define HWA_LUT_FREQ_DEROTATE_RAMIDX_AUTOINCR_SATURATED   ((uint8_t)1U) /** auto-increment mode, with saturates at 63 */
 
#define HWA_LUT_FREQ_DEROTATE_RAMIDX_NONINCR   ((uint8_t)2U) /** non-increment mode */
 
#define HWA_HISTOGRAM_MODE_DISABLED   ((uint8_t)0U)
 
#define HWA_HISTOGRAM_MODE_HISTOGRAM   ((uint8_t)1U)
 
#define HWA_HISTOGRAM_MODE_CDF   ((uint8_t)2U)
 
#define HWA_HISTOGRAM_MODE_CDF_THRESHOLD   ((uint8_t)3U)
 
#define HWA_LOCALMAX_THRESH_BITMASK_BOTH_EN   ((uint8_t)0U)
 
#define HWA_LOCALMAX_THRESH_BITMASK_CDIM_EN   ((uint8_t)1U)
 
#define HWA_LOCALMAX_THRESH_BITMASK_BDIM_EN   ((uint8_t)2U)
 
#define HWA_LOCALMAX_THRESH_BITMASK_BOTH_DIS   ((uint8_t)3U)
 
#define HWA_LOCALMAX_THRESH_SELECT_DIMBREG_DIMCREG   ((uint8_t)0U)
 
#define HWA_LOCALMAX_THRESH_SELECT_DIMBRAM_DIMCREG   ((uint8_t)1U)
 
#define HWA_LOCALMAX_THRESH_SELECT_DIMBREG_DIMCRAM   ((uint8_t)2U)
 
#define HWA_LOCALMAX_THRESH_SELECT_DIMBRAM_DIMCRAM   ((uint8_t)3U)
 
#define HWA_COMPRESS_METHOD_EGE   ((uint8_t)0U)
 
#define HWA_COMPRESS_METHOD_BFP   ((uint8_t)1U)
 
#define HWA_CMP_DCMP_COMPRESS   ((uint8_t)0U)
 
#define HWA_CMP_DCMP_DECOMPRESS   ((uint8_t)1U)
 
#define HWA_COMPRESS_PATHSELECT_BOTHPASSES   ((uint8_t)3U)
 
#define HWA_COMPRESS_PATHSELECT_SECONDPASS   ((uint8_t)1U)
 
#define HWA_PARAMSET_CONTEXTSWITCH_DISABLE   (0U)
 disable the context switch in the paramset More...
 
#define HWA_PARAMSET_CONTEXTSWITCH_NONFORCE_ENABLE   (1U)
 context swtich is allowed at the end the a paramset, CONTEXTSW_EN register bit is set More...
 
#define HWA_PARAMSET_CONTEXTSWITCH_FORCE_ENABLE   (2U)
 after the paramset, the context switch is forced to happen wihthout the need of any trigger, the register FORCED_CONTEXTSW_EN in the parameter-set is set. More...
 
#define HWA_APP_MEMINIT_PARAM_RAM   (1U << 8U)
 Bit mask to specify PARAM RAM MEM BANK, used with HWA_initializeRAM() More...
 
#define HWA_APP_MEMINIT_WINDOW_RAM   (1U << 9U)
 Bit mask to specify PARAM RAM MEM BANK, used with HWA_initializeRAM() More...
 
#define HWA_APP_MEMINIT_PER_SAMPLE_MAX_VAL_EVEN_RAM   (1U << 10U)
 Bit mask to specify PARAM RAM MEM BANK, used with HWA_initializeRAM() More...
 
#define HWA_APP_MEMINIT_PER_SAMPLE_MAX_VAL_ODD_RAM   (1U << 11U)
 Bit mask to specify PARAM RAM MEM BANK, used with HWA_initializeRAM() More...
 
#define HWA_APP_MEMINIT_PER_ITER_MAX_VAL_RAM   (1U << 12U)
 Bit mask to specify PARAM RAM MEM BANK, used with HWA_initializeRAM() More...
 
#define HWA_APP_MEMINIT_HIST_EVEN_RAM   (1U << 13U)
 Bit mask to specify PARAM RAM MEM BANK, used with HWA_initializeRAM() More...
 
#define HWA_APP_MEMINIT_HIST_ODD_RAM   (1U << 14U)
 Bit mask to specify PARAM RAM MEM BANK, used with HWA_initializeRAM() More...
 
#define HWA_APP_MEMINIT_MEMBANK_ALL
 Bit mask to specify ALL MEM BANKs, used with HWA_initializeRAM() More...
 

Typedefs

typedef void * HWA_Handle
 A handle that is returned from a HWA_open() call. More...
 
typedef void(* HWA_ParamDone_IntHandlerFuncPTR) (uint32_t intrIdx, uint32_t paramSet, void *arg)
 HWA Interrupt callback function after every paramset completion. More...
 
typedef void(* HWA_Done_IntHandlerFuncPTR) (uint32_t threadIdx, void *arg)
 HWA Interrupt callback function after all paramsets completion. More...
 

Functions

void HWA_init (void)
 Function to initialize the HWA module. More...
 
void HWA_deinit (void)
 Function to deinitialize the HWA module. More...
 
HWA_Handle HWA_open (uint32_t index, HWA_OpenConfig *hwaCfg, int32_t *errCode)
 Function to initialize HWA specified by the particular index value. More...
 
int32_t HWA_close (HWA_Handle handle)
 Function to close a HWA peripheral specified by the HWA handle. More...
 
int32_t HWA_reset (HWA_Handle handle)
 Function to reset the internal state machine of the HWA. More...
 
int32_t HWA_initializeRAM (HWA_Handle handle, uint32_t ramMemBankMask)
 Function to initialize RAM memory banks in HWA. More...
 
DSSHWACCRegs * HWA_getCommonCtrlAddr (HWA_Handle handle)
 Function to returns the HWA common control base address. More...
 
DSSHWACCPARAMRegs * HWA_getParamSetAddr (HWA_Handle handle, uint8_t paramsetIdx)
 Function to returns the HWA paramSet base address. More...
 
int32_t HWA_configCommon (HWA_Handle handle, HWA_CommonConfig *commonConfig)
 Function to set the common HWA configuration parameters needed for the next operations/iterations/paramsets of HWA. More...
 
int32_t HWA_configParamSet (HWA_Handle handle, uint8_t paramsetIdx, HWA_ParamConfig *paramConfig, HWA_SrcDMAConfig *dmaConfig)
 Function to set the HWA configuration parameters for a given paramSet. More...
 
int32_t HWA_getDMAconfig (HWA_Handle handle, uint8_t dmaTriggerSrc, HWA_SrcDMAConfig *dmaConfig)
 Function to get the config to program the DMA for a given DMA Trigger channel. Application should use the returned config to program the DMA so that it can then in turn trigger the paramset. Application should make sure that the channel provided here in dmaTriggerSrc should match the HWA_ParamConfig::triggerSrc passed to HWA_configParamSet() More...
 
int32_t HWA_configRam (HWA_Handle handle, uint8_t ramType, uint8_t *data, uint32_t dataSize, uint32_t startIdx)
 Function to set the HWA RAM : HWA_RAM_TYPE_WINDOW_RAM, HWA_RAM_TYPE_VECTORMULTIPLY_RAM, HWA_RAM_TYPE_LUT_FREQ_DEROTATE_RAM or HWA_RAM_TYPE_SHUFFLE_RAM. More...
 
uint32_t HWA_getRamAddress (uint8_t ramType)
 Function to get the RAM starting address for one specified RAM type. More...
 
int32_t HWA_readRam (HWA_Handle handle, uint8_t ramType, uint8_t *data, uint32_t dataSize, uint32_t startIdx)
 Function to read the HWA 2D statistics output RAM, including HWA_RAM_TYPE_2DSTAT_ITER_VAL, HWA_RAM_TYPE_2DSTAT_ITER_IDX, HWA_RAM_TYPE_2DSTAT_SAMPLE_VAL, HWA_RAM_TYPE_2DSTAT_SAMPLE_IDX or HWA_RAM_TYPE_HISTOGRAM_RAM, except the HWA_RAM_TYPE_HIST_THRESH_RAM. More...
 
int32_t HWA_readHistThresholdRam (HWA_Handle handle, HWA_CdfThreshold *cdfThresholdResult, uint8_t numSampleIndices, uint8_t startSampleIdx)
 Function to read the HWA HWA_RAM_TYPE_HIST_THRESH_RAM RAM. More...
 
int32_t HWA_enableParamSetInterrupt (HWA_Handle handle, uint8_t paramsetIdx, HWA_InterruptConfig *intrConfig)
 Function to enable the CPU and/or DMA interrupt after a paramSet completion. The CPU interrupt for every paramset completion may not be supported on all devices - see HWA_Attrs::isConcurrentAccessAllowed. More...
 
int32_t HWA_paramSetDonePolling (HWA_Handle handle, uint8_t numParamSets, uint8_t *paramsetsArray)
 Function to poll the PARAM_DONE_SET_STATUS_0 and PARAM_DONE_SET_STATUS_1 registers to check if the specified paramsets are finished. More...
 
int32_t HWA_singleParamSetDonePolling (HWA_Handle handle, uint8_t paramsetIndex)
 Function to poll the PARAM_DONE_SET_STATUS_0 or PARAM_DONE_SET_STATUS_1 registers to check if one single specified paramset is finished. More...
 
int32_t HWA_enableDoneInterrupt (HWA_Handle handle, uint8_t threadIdx, HWA_Done_IntHandlerFuncPTR callbackFn, void *callbackArg)
 Function to enable the CPU interrupt after all programmed paramSets have been completed in the background or ALT thread. More...
 
int32_t HWA_disableParamSetInterrupt (HWA_Handle handle, uint8_t paramsetIdx, uint8_t interruptTypeFlag)
 Function to disable the CPU and/or DMA interrupt after a paramSet completion. More...
 
int32_t HWA_disableDoneInterrupt (HWA_Handle handle, uint8_t threadIdx)
 Function to disable the CPU interrupt after all programmed paramSets have been completed. More...
 
int32_t HWA_enable (HWA_Handle handle, uint8_t flagEnDis)
 Function to enable the state machine of the HWA. This should be called after paramset and RAM have been programmed. More...
 
int32_t HWA_enableContextSwitch (HWA_Handle handle, uint8_t flagEnDis)
 Function to enable or disable the context switching in hwa. More...
 
int32_t HWA_setSoftwareTrigger (HWA_Handle handle, uint8_t swTriggerType)
 Function to manually trigger the execution of the state machine via software, the software trigger through either FW2HWA_TRIG_0 or FW2HWA_TRIG_1 register if the trigger is set to HWA_TRIG_MODE_SOFTWARE from DSP/R5F, trigger is done through FW2HWA_TRIG_0 if the trigger is set to HWA_TRIG_MODE_SOFTWARE2 from DSP/R5F, trigger is done through FW2HWA_TRIG_1. More...
 
int32_t HWA_setContextswitchSoftwareTrigger (HWA_Handle handle)
 Function to manually trigger the execution of the state machine via software in context switch, the software trigger through CS_FW2ACC_TRIG register. More...
 
int32_t HWA_setContextswitchDMAManualTrigger (HWA_Handle handle, uint8_t idx)
 Function to manually trigger the execution of the state machine via DMA trigger in context switch. More...
 
int32_t HWA_softwareResetAccumulators (HWA_Handle handle, uint8_t accumulatortype)
 Function for sofware to reset the DC accumulators or interference statistics accumulators. More...
 
int32_t HWA_softwareResetRecursiveWinKvalue (HWA_Handle handle)
 Function resets the paramset counter used in recurise windowing mode with REC_WIN_MODE_SEL is set to 1. More...
 
int32_t HWA_softwareResetTwidIncrDeltaFrac (HWA_Handle handle)
 Function resets the execution counter if complex multiply is configured as frequency shifter mode with frequency increment (mode 10) More...
 
int32_t HWA_setDMA2ACCManualTrig (HWA_Handle handle, uint8_t idx)
 Function to manually trigger the execution of the state machine waiting on DMA via software. More...
 
int32_t HWA_setSourceAddress (HWA_Handle handle, uint16_t paramIdx, uint32_t sourceAddress)
 Function to set the source address for one paramset. More...
 
int32_t HWA_readClipStatus (HWA_Handle handle, uint16_t *clipStatusResult, uint8_t type)
 Function to read the Clip Status registers. More...
 
int32_t HWA_clearClipStatus (HWA_Handle handle, uint8_t type)
 Function to clear the Clip Status registers. More...
 
int32_t HWA_readStatsReg (HWA_Handle handle, HWA_Stats *pStats, uint8_t numIter)
 Function to read the 4 sets of 'MAX' statistics register. More...
 
int32_t HWA_readCFARPeakCountReg (HWA_Handle handle, uint8_t *pbuf, uint8_t size)
 Function to read the PEAKCNT register. More...
 
int32_t HWA_readDebugReg (HWA_Handle handle, HWA_DebugStats *pStats)
 Function to read the debug registers (paramcurr, loopcou, acc_trig_in_stat) More...
 
int32_t HWA_clearDebugReg (HWA_Handle handle)
 Function to clear the debug registers (acc_trig_in_clr) More...
 
int32_t HWA_getHWAMemInfo (HWA_Handle handle, HWA_MemInfo *memInfo)
 Function to get HWA processing Memory information including address, size and number of banks. More...
 
int32_t HWA_getDMAChanIndex (HWA_Handle handle, uint8_t edmaChanId, uint8_t *hwaDestChan)
 Function to get the dma destination index with a given EDMA channel number This function assumes the EDMA channel number is from the first EDMA instance. More...
 
int32_t HWA_getEDMAChanId (HWA_Handle handle, uint8_t hwaDMAdestChan)
 Function to get the edma EDMA channel number from a given HWA paramset destination channel. This function assumes the EDMA channel number is from the first EDMA instance. More...
 
int32_t HWA_readDCEstimateReg (HWA_Handle handle, cmplx32ImRe_t *pbuf, uint8_t startIdx, uint8_t size)
 Function to read the DC_EST_I/Q register. More...
 
int32_t HWA_readIntfAccReg (HWA_Handle handle, uint64_t *accBuf, uint8_t type, uint8_t startIdx, uint8_t size)
 Function to read the interference threshold MAG or MAGDIFF Accumulator register. More...
 
int32_t HWA_readDCAccReg (HWA_Handle handle, cmplx64ImRe_t *accbuf, uint8_t startIdx, uint8_t size)
 Function to read the DC estimation accumulator register,. More...
 
int32_t HWA_readInterfChirpCountReg (HWA_Handle handle, uint16_t *numInterfSamplesChirp)
 Function to read the number of samples that exceeded the threshold in a chirp. More...
 
int32_t HWA_readInterfFrameCountReg (HWA_Handle handle, uint32_t *numInterfSamplesFrame)
 Function to read the number of samples that exceeded the threshold in a frame. More...
 
int32_t HWA_readInterfThreshReg (HWA_Handle handle, uint32_t *pbuf, uint8_t startIdx, uint8_t size, uint8_t type)
 Function to read the interference statistics INTF_LOC_THRESH_MAG_VAL or INTF_LOC_THRESH_MAG_VAL registers. More...
 
int32_t HWA_controlPeripheralSuspendMode (HWA_Handle handle, uint8_t flagEnDis)
 Function to control the suspend mode of the peripheral when the controlling processor (where this driver is instantiated) is halted. More...
 
int32_t HWA_configureSingleStep (HWA_Handle handle, uint8_t flagEnDis)
 Function to enable/disable single-stepping approach which pauses the HWA execution after each param-set. More...
 
int32_t HWA_triggerSingleStep (HWA_Handle handle)
 Function to Trigger single-step. This triggers state machine to execute one parameter-set at a time and wait for the next single step trigger. More...
 

Variables

HWA_Attrs gHwaAttrs []
 Externally defined driver configuration array. More...
 
HWA_RAMAttrs gHwaRamCfg [HWA_NUM_RAMS]
 Externally defined driver RAM configuration array. More...
 
HWA_Object gHwaObject []
 Externally defined driver object. More...
 
HWA_Object * gHwaObjectPtr []
 Externally defined driver object pointer. More...
 
uint32_t gHwaConfigNum
 Externally defined driver configuration array size. More...
 

Macro Definition Documentation

◆ HWADRV_ADDR_TRANSLATE_CPU_TO_HWA

#define HWADRV_ADDR_TRANSLATE_CPU_TO_HWA (   x)    (uint32_t)((uint32_t)(x) & 0x000FFFFFU)

transfer the CPU address to HWA address

◆ HWA_NUM_RXCHANNELS

#define HWA_NUM_RXCHANNELS   (12U)

Number of RX channels in pre-processing block.

◆ HWA_NUM_INTERFMITG_WINARRAY

#define HWA_NUM_INTERFMITG_WINARRAY   (5U)

Number of programmable array of window parameters in interference mitigation block.

◆ HWA_BPMPATTERN_LENGTH_INWORDS

#define HWA_BPMPATTERN_LENGTH_INWORDS   (8U)

The length of BPM Pattern sequence in words.

◆ HWA_CHANCOMB_LENGTH_INWORDS

#define HWA_CHANCOMB_LENGTH_INWORDS   (8U)

The length of channel combining vector in words.

◆ HWA_ZEROINSERT_LENGTH_INWORDS

#define HWA_ZEROINSERT_LENGTH_INWORDS   (8U)

The length of zero insert mask in words.

◆ HWA_NUM_RAMS

#define HWA_NUM_RAMS   (10U)

The number of RAM types in HWA.

◆ HWA_MAXNUM_LOOPS

#define HWA_MAXNUM_LOOPS   (4095U)

The maximum number of loops in HWA.

◆ HWA_CMP_K_ARR_LEN

#define HWA_CMP_K_ARR_LEN   (8U)

The length of EGE compression/decompression K-paramseters array.

Variable Documentation

◆ gHwaAttrs

HWA_Attrs gHwaAttrs[]
extern

Externally defined driver configuration array.

◆ gHwaRamCfg

HWA_RAMAttrs gHwaRamCfg[HWA_NUM_RAMS]
extern

Externally defined driver RAM configuration array.

◆ gHwaObject

HWA_Object gHwaObject[]
extern

Externally defined driver object.

◆ gHwaObjectPtr

HWA_Object* gHwaObjectPtr[]
extern

Externally defined driver object pointer.

◆ gHwaConfigNum

uint32_t gHwaConfigNum
extern

Externally defined driver configuration array size.