HWA interrupt default priority, applied only to the processors, which support hardware priority, e.g R5F.
Macros | |
| #define | HWA_DONE_INTERRUPT_PRIORITY (1U) |
| Default HWA background thread done interrupt priority. More... | |
| #define | HWA_ALTDONE_INTERRUPT_PRIORITY (1U) |
| Default HWA background thread done interrupt priority. More... | |
| #define | HWA_PARAMSETDONE_INTERRUPT1_PRIORITY (1U) |
| Default HWA paramset done interrupt 1 priority. More... | |
| #define | HWA_PARAMSETDONE_INTERRUPT2_PRIORITY (1U) |
| Default HWA paramset done interrupt 2 priority. More... | |
| #define | HWA_LOCAL_RAM_ERR_PRIORITY (1U) |
| Default HWA local ram error interrupt priority. More... | |
| #define HWA_DONE_INTERRUPT_PRIORITY (1U) |
Default HWA background thread done interrupt priority.
| #define HWA_ALTDONE_INTERRUPT_PRIORITY (1U) |
Default HWA background thread done interrupt priority.
| #define HWA_PARAMSETDONE_INTERRUPT1_PRIORITY (1U) |
Default HWA paramset done interrupt 1 priority.
| #define HWA_PARAMSETDONE_INTERRUPT2_PRIORITY (1U) |
Default HWA paramset done interrupt 2 priority.
| #define HWA_LOCAL_RAM_ERR_PRIORITY (1U) |
Default HWA local ram error interrupt priority.