The HWA driver provides APIs to configure, trigger and obtain results from the hardware accelerator
Sub Modules | |
HWA Driver Error Codes | |
The section has a list of all the error codes which are generated by the HWA Driver module. | |
HWA Driver External Data Structures | |
The section has a list of all the data structures which are exposed to the application. | |
HWA Driver External Functions | |
The section has a list of all the exported API which the applications need to invoke in order to use the driver. | |