Macros that define values for histogram computation mode.
Macros | |
#define | HWA_HISTOGRAM_MODE_DISABLED ((uint8_t)0U) |
#define | HWA_HISTOGRAM_MODE_HISTOGRAM ((uint8_t)1U) |
#define | HWA_HISTOGRAM_MODE_CDF ((uint8_t)2U) |
#define | HWA_HISTOGRAM_MODE_CDF_THRESHOLD ((uint8_t)3U) |
#define HWA_HISTOGRAM_MODE_DISABLED ((uint8_t)0U) |
disable
#define HWA_HISTOGRAM_MODE_HISTOGRAM ((uint8_t)1U) |
Statistics output - Histogram computation
#define HWA_HISTOGRAM_MODE_CDF ((uint8_t)2U) |
Statistics output - CDF computation
#define HWA_HISTOGRAM_MODE_CDF_THRESHOLD ((uint8_t)3U) |
Statistics output - CDF threshold computation, user specified the threshold via HWA_CommonConfig::advStatConfig::cdfCntThresh