AM273x MCU+ SDK  09.02.00

Introduction

Macros that define values for the shuffled addressing mode.

Macros

#define HWA_SRC_SHUFFLE_AB_MODE_DISABLE   ((uint8_t)0U) /** 0-disable */
 
#define HWA_SRC_SHUFFLE_AB_MODE_ADIM   ((uint8_t)1U) /** 1-SHUFFLE_LUT is used for sample index re-ordering in A dimension */
 
#define HWA_SRC_SHUFFLE_AB_MODE_BDIM   ((uint8_t)2U) /** 2- SHUFFLE_LUT is used in B-dimension */
 

Macro Definition Documentation

◆ HWA_SRC_SHUFFLE_AB_MODE_DISABLE

#define HWA_SRC_SHUFFLE_AB_MODE_DISABLE   ((uint8_t)0U) /** 0-disable */

◆ HWA_SRC_SHUFFLE_AB_MODE_ADIM

#define HWA_SRC_SHUFFLE_AB_MODE_ADIM   ((uint8_t)1U) /** 1-SHUFFLE_LUT is used for sample index re-ordering in A dimension */

◆ HWA_SRC_SHUFFLE_AB_MODE_BDIM

#define HWA_SRC_SHUFFLE_AB_MODE_BDIM   ((uint8_t)2U) /** 2- SHUFFLE_LUT is used in B-dimension */