HWA RAM Parameters.
HWA parameters are used to with the HWA_configRam() call.
Data Fields | |
uint32_t | ramBaseAddress |
uint32_t | ramSizeInBytes |
uint32_t HWA_RAMAttrs::ramBaseAddress |
HWA RAM base address
uint32_t HWA_RAMAttrs::ramSizeInBytes |
HWA RAM size in bytes