4.1. ZED Stereo Camera ROS Node
This is a stereo camera ROS node for the ZED camera, based on the OpenCV VideoCapture API. The ROS node publishes left and right raw images and their camera_info.
4.1.1. Usage
Obtain the factory camera calibration data file for your ZED camera with a script provided.
cd $SDK_DIR/tools/stereo_camera ./download_calib_file.sh <serial_number>
Replace
<serial_number>with the serial number of the ZED camera (found on the original box). Place the downloaded calibration data file (SNxxxx.conf) under the$SDK_DIR/ros1/drivers/zed_capture/configfolder.Generate
camera_infoYAML files and undistortion/rectification look-up-table (LUT) files, which are required in offloading the undistortion/rectification on the VPAC/LDC hardware accelerator. It is recommended to perform the following steps in the Robotics SDK ROS 1 container on the Ubuntu PC, and then “scp” the output artifacts to the target Linux filesystem, under/opt/robotics_sdk/ros1/drivers/zed_capture/config.Run the following script:
cd $SDK_DIR/tools/stereo_camera python3 generate_rect_map.py -i SNxxxx.conf -m <camera_mode> -p <output_folder_path>
Replace
SNxxxx.confwith the factory calibration data file obtained from Step 1.<camera_mode>is the camera mode. Valid camera mode are: 2K, FHD, FHD2, HD, HD2, VGA (seeLaunch File Parameterssection for description). If the-margument is not provided, the tool will iterate by default for the following three camera modes: HD, HD2, FHD, and FHD2.
This script parses the calibration data and generates the following files under
<output_folder_path>:<SN_string>_<camera_mode>_camera_info_{left,right}.yaml:camera_infofor left and right raw image,<SN_string>_<camera_mode>_remap_LUT_{left,right}.bin: undistortion/rectification remap LUT for left and right raw images.
Build the ZED camera ROS node
cd $ROS_WS colcon build --base-paths /opt/robotics_sdk/ros2 --cmake-force-configure source install/setup.bash
Launch the ZED camera node: Update
zed_sn_strinlaunch/zed_capture_launch.py, or pass as a launch argument as follows:ros2 launch zed_capture zed_capture_launch.py zed_sn_str:=SNxxxxx
4.1.2. Stereo Camera Calibration
For cases where the ZED cameras needs to be recalibrated for some reason, we provides a OpenCV based calibration tool. For more information, refer to Stereo Camera Calibration.
4.1.3. Launch File Parameters
Parameter |
Description |
Value |
|---|---|---|
zed_sn_str |
ZED camera serial number string, which should start with ‘SN’ followed by the serial number |
string |
cam_id |
Camera device number. Use |
string |
camera_mode |
ZED camera mode |
‘2K’ (2208x1242) |
_ |
_ |
‘FHD’ (1920x1080) |
_ |
_ |
‘FHD2’ (1920x1024) |
_ |
_ |
‘HD’ (1280x720) |
_ |
_ |
‘HD2’ (1280x720) |
_ |
_ |
‘VGA’ (672x376) |
frame_rate |
Frame rate at which raw images are published |
int |
encoding |
Image encoding |
‘yuv422’ (default) or ‘bgr8’ |
‘FHD2’ is a newly added mode that provides a resolution of 1920x1024 resolution that is supported by the stereo depth engine (SDE) hardware accelerator. The images are obtained by cropping top and bottom evenly the original 1080p images captured from the ‘FHD’ mode.
‘HD2’ is a newly added mode that provides a resolution of 720p for experiments that need a longer focal length than the native ‘HD’. The images are obtained by center-cropping the original 1080p images captured from the ‘FHD’ mode.
When encoding is set to ‘yuv422’, the pixel format YUV422::YUYV from the ZED camera is converted to YUV422::UYVY format, considering the compatibility with LDC hardware accelerator.