223 #ifndef __attribute__ 224 #define __attribute__() 229 #define TISCI_BIT(n) (1UL << (n)) 237 #ifndef SYSFW_DEVGRPS_H 250 #define DEVGRP_ALL (0x00U) 253 #define DEVGRP_00 ((0x01U) << 0U) 255 #define DEVGRP_01 ((0x01U) << 1U) 257 #define DEVGRP_02 ((0x01U) << 2U) 259 #define DEVGRP_03 ((0x01U) << 3U) 261 #define DEVGRP_04 ((0x01U) << 4U) 263 #define DEVGRP_05 ((0x01U) << 5U) 265 #define DEVGRP_06 ((0x01U) << 6U) 270 #define DEVGRP_DMSC ((0x01U) << 7U) 272 #define DEVGRP_DMSC_ALL (0xFFU) 277 #if defined(SOC_J721E) || defined(SOC_J7200) 278 #define SCICLIENT_COMMON_X509_HEADER_ADDR (0x41cffb00) 279 #elif defined(SOC_J721S2) 280 #define SCICLIENT_COMMON_X509_HEADER_ADDR (0x41cfdb00) 282 #define SCICLIENT_COMMON_X509_HEADER_ADDR (0x41cffb00) 285 #define SCISERVER_COMMON_X509_HEADER_ADDR \ 286 SCICLIENT_COMMON_X509_HEADER_ADDR 292 #define MAX_NUM_DEVGRPS (8U) 299 #if defined (SOC_AM65XX) 300 #include <ti/drv/sciclient/soc/sysfw/include/am65x/tisci_resasg_types.h> 301 #include <ti/drv/sciclient/soc/sysfw/include/am65x/tisci_hosts.h> 302 #include <ti/drv/sciclient/soc/sysfw/include/am65x/tisci_sec_proxy.h> 303 #include <ti/drv/sciclient/soc/sysfw/include/am65x/tisci_boardcfg_constraints.h> 304 #include <ti/drv/sciclient/soc/sysfw/include/am65x/tisci_clocks.h> 305 #include <ti/drv/sciclient/soc/sysfw/include/am65x_sr2/tisci_clocks.h> 307 #if defined (SOC_J721E) 308 #include <ti/drv/sciclient/soc/sysfw/include/j721e/tisci_resasg_types.h> 309 #include <ti/drv/sciclient/soc/sysfw/include/j721e/tisci_hosts.h> 310 #include <ti/drv/sciclient/soc/sysfw/include/j721e/tisci_sec_proxy.h> 311 #include <ti/drv/sciclient/soc/sysfw/include/j721e/tisci_boardcfg_constraints.h> 313 #if defined (SOC_J7200) 314 #include <ti/drv/sciclient/soc/sysfw/include/j7200/tisci_resasg_types.h> 315 #include <ti/drv/sciclient/soc/sysfw/include/j7200/tisci_hosts.h> 316 #include <ti/drv/sciclient/soc/sysfw/include/j7200/tisci_sec_proxy.h> 317 #include <ti/drv/sciclient/soc/sysfw/include/j7200/tisci_boardcfg_constraints.h> 319 #if defined (SOC_AM64X) 320 #include <ti/drv/sciclient/soc/sysfw/include/am64x/tisci_resasg_types.h> 321 #include <ti/drv/sciclient/soc/sysfw/include/am64x/tisci_hosts.h> 322 #include <ti/drv/sciclient/soc/sysfw/include/am64x/tisci_sec_proxy.h> 323 #include <ti/drv/sciclient/soc/sysfw/include/am64x/tisci_boardcfg_constraints.h> 325 #if defined (SOC_J721S2) 326 #include <ti/drv/sciclient/soc/sysfw/include/j721s2/tisci_resasg_types.h> 327 #include <ti/drv/sciclient/soc/sysfw/include/j721s2/tisci_hosts.h> 328 #include <ti/drv/sciclient/soc/sysfw/include/j721s2/tisci_sec_proxy.h> 329 #include <ti/drv/sciclient/soc/sysfw/include/j721s2/tisci_boardcfg_constraints.h> 332 #define TISCI_HOST_ID_DMSC2DM TISCI_HOST_ID_TIFS2DM 334 #define TISCI_SEC_PROXY_DM2DMSC_WRITE_NOTIFY_RESP_THREAD_ID \ 335 TISCI_SEC_PROXY_DM2TIFS_WRITE_NOTIFY_RESP_THREAD_ID 336 #define TISCI_SEC_PROXY_DM2DMSC_READ_RESPONSE_THREAD_ID \ 337 TISCI_SEC_PROXY_DM2TIFS_READ_RESPONSE_THREAD_ID 362 #include <ti/drv/sciclient/soc/sciclient_soc_priv.h> 393 #define SCICLIENT_SERVICE_OPERATION_MODE_POLLED (0U) 394 #define SCICLIENT_SERVICE_OPERATION_MODE_INTERRUPT (1U) 406 #define SCICLIENT_SERVICE_WAIT_FOREVER (0xFFFFFFFFU) 407 #define SCICLIENT_SERVICE_NO_WAIT (0x0U) 411 #define SCICLIENT_FT_PASS (0xA5A5U) 413 #define SCICLIENT_FT_FAIL (0x5A5AU) 704 uint8_t * pCommonHeader, uint8_t * pBoardCfgHeader,
720 uint8_t * pCommonHeader,
uint32_t boardCfgLowSize
Definition: sciclient.h:503
int32_t Sciclient_init(const Sciclient_ConfigPrms_t *pCfgPrms)
This API is called once for registering interrupts and creating semaphore handles to be able to talk ...
int32_t Sciclient_getDefaultBoardCfgInfo(Sciclient_DefaultBoardCfgInfo_t *pBoardCfgInfo)
API to get the default board config info.
This file contains the definition of all the shim layer functions which request DMSC for generic serv...
This file contains the definition of all the message IDs, message formats to be able to interact with...
Input parameters for Sciclient_service function.
Definition: sciclient.h:493
struct tisci_header hdr
Definition: tisci_core.h:438
int32_t Sciclient_boardCfgPrepHeader(uint8_t *pCommonHeader, uint8_t *pBoardCfgHeader, const Sciclient_BoardCfgPrms_t *pInPmPrms, const Sciclient_BoardCfgPrms_t *pInRmPrms)
Prepare the header for the board configuration. This API is typically only used by SBL where it will ...
Output parameters for Sciclient_service function.
Definition: sciclient.h:476
This file contains the definition of all the message IDs, message formats to be able to interact with...
const uint8_t * pReqPayload
Definition: sciclient.h:460
const uint32_t * boardCfgLowSec
Definition: sciclient.h:499
int32_t Sciclient_abiCheck(void)
void Sciclient_TisciMsgSetAckResp(struct tisci_header *hdr)
Send the Response in Ack. Used only with Sciserver or Sciclient Direct.
const uint32_t * boardCfgLowPm
Definition: sciclient.h:501
uint32_t timeout
Definition: sciclient.h:464
SCICLIENT Low Level Driver SOC specific file.
This file contains the definition of all the message IDs, message formats to be able to interact with...
uint8_t domgrp_t
Defines the sysfw DOMGRP type. This is meant to be used in code or data structures that require disti...
Definition: sciclient.h:235
uint8_t devgrp_t
Defines the sysfw DEVGRP type. This is meant to be used in code or data structures that require disti...
Definition: sciclient.h:242
uint32_t opModeFlag
Definition: sciclient.h:426
Sciclient_BoardCfgPrms_t inRmPrms
Definition: sciclient.h:445
uint32_t flags
Definition: sciclient.h:478
int32_t Sciclient_deinit(void)
De-initialization of sciclient. This de-initialization is specific to the application....
This file contains the definition of all the message IDs, message formats to be able to interact with...
uint8_t * pRespPayload
Definition: sciclient.h:480
uint16_t messageType
Definition: sciclient.h:454
uint32_t reqPayloadSize
Definition: sciclient.h:462
void Sciclient_TisciMsgSetNakResp(struct tisci_header *hdr)
Send the Response in NAK. Used only with Sciserver or Sciclient Direct.
Wrapper function to send the board configuration message to DMSC.
uint32_t c66xRatRegion
Definition: sciclient.h:438
uint32_t boardCfgLowRmSize
Definition: sciclient.h:505
uint32_t isSecureMode
Definition: sciclient.h:434
This file contains the definition of all the message IDs, message formats to be able to interact with...
int32_t Sciclient_boardCfgParseHeader(uint8_t *pCommonHeader, Sciclient_BoardCfgPrms_t *pInPmPrms, Sciclient_BoardCfgPrms_t *pInRmPrms)
Parse the header left behind by the SBL in the SCISERVER. This is used in the SCISERVER App to read t...
const uint32_t * boardCfgLow
Definition: sciclient.h:495
uint8_t skipLocalBoardCfgProcess
Definition: sciclient.h:440
uint8_t forwardStatus
Definition: sciclient.h:467
Initialization parameters for sciclient. Pointer to this is passed to Sciclient_init.
Definition: sciclient.h:424
int32_t Sciclient_service(const Sciclient_ReqPrm_t *pReqPrm, Sciclient_RespPrm_t *pRespPrm)
This API allows communicating with the System firmware which can be called to perform various functio...
Sciclient_BoardCfgPrms_t inPmPrms
Definition: sciclient.h:443
Parameters for Sciclient_boardCfg Pointer to this is passed to Sciclient_boardCfg.
Definition: sciclient_boardcfg.h:58
uint32_t boardCfgLowSecSize
Definition: sciclient.h:507
uint32_t respPayloadSize
Definition: sciclient.h:486
This file contains the definition of all the message IDs, message formats to be able to interact with...
const uint32_t * boardCfgLowRm
Definition: sciclient.h:497
uint32_t flags
Definition: sciclient.h:456
uint32_t boardCfgLowPmSize
Definition: sciclient.h:509
Sciclient_BoardCfgPrms_t * pBoardCfgPrms
Definition: sciclient.h:430
int32_t Sciclient_loadFirmware(const uint32_t *pSciclient_firmware)
Loads the DMSC firmware. This is typically called by SBL. Load firmware does not require calling the ...
Input parameters for Sciclient_service function.
Definition: sciclient.h:452
int32_t Sciclient_configPrmsInit(Sciclient_ConfigPrms_t *pCfgPrms)
Sciclient_ConfigPrms_t structure init function.