![]() |
PDK API Guide for J721E
|
Wrapper function to send the board configuration message to DMSC.
Go to the source code of this file.
Data Structures | |
struct | Sciclient_BoardCfgPrms_t |
Parameters for Sciclient_boardCfg Pointer to this is passed to Sciclient_boardCfg. More... | |
Functions | |
int32_t | Sciclient_boardCfg (const Sciclient_BoardCfgPrms_t *pInPrms) |
One time board configuration to be done from R5. More... | |
int32_t | Sciclient_boardCfgPm (const Sciclient_BoardCfgPrms_t *pInPrms) |
One time board configuration to be done from R5 for PM. User needs to define a section ".boardcfg_data" in the linker file for the default configuration, which needs to be present in OCMRAM . If user provides custom board_cfg, then the data must be present on OCMRAM. More... | |
int32_t | Sciclient_boardCfgRm (const Sciclient_BoardCfgPrms_t *pInPrms) |
One time board configuration to be done from R5 for RM . User needs to define a section ".boardcfg_data" in the linker file for the default configuration, which needs to be present in OCMRAM . If user provides custom board_cfg, then the data must be present on OCMRAM. More... | |
int32_t | Sciclient_boardCfgSec (const Sciclient_BoardCfgPrms_t *pInPrms) |
One time board configuration to be done from R5 for SECURITY User needs to define a section ".boardcfg_data" in the linker file for the default configuration, which needs to be present in OCMRAM . If user provides custom board_cfg, then the data must be present on OCMRAM. More... | |
int32_t Sciclient_boardCfg | ( | const Sciclient_BoardCfgPrms_t * | pInPrms | ) |
One time board configuration to be done from R5.
User needs to define a section ".boardcfg_data" in the linker file for the default configuration, which needs to be present in OCMRAM . If user provides custom board_cfg, then the data must be present on OCMRAM.
pInPrms | [IN] Pointer to Sciclient_BoardCfgPrms_t . NULL results in default config. |
int32_t Sciclient_boardCfgPm | ( | const Sciclient_BoardCfgPrms_t * | pInPrms | ) |
One time board configuration to be done from R5 for PM. User needs to define a section ".boardcfg_data" in the linker file for the default configuration, which needs to be present in OCMRAM . If user provides custom board_cfg, then the data must be present on OCMRAM.
pInPrms | [IN] Pointer to #Sciclient_BoardCfgPrms_t . NULL results in default config. |
int32_t Sciclient_boardCfgRm | ( | const Sciclient_BoardCfgPrms_t * | pInPrms | ) |
One time board configuration to be done from R5 for RM . User needs to define a section ".boardcfg_data" in the linker file for the default configuration, which needs to be present in OCMRAM . If user provides custom board_cfg, then the data must be present on OCMRAM.
pInPrms | [IN] Pointer to #Sciclient_BoardCfgPrms_t . NULL results in default config. |
int32_t Sciclient_boardCfgSec | ( | const Sciclient_BoardCfgPrms_t * | pInPrms | ) |
One time board configuration to be done from R5 for SECURITY User needs to define a section ".boardcfg_data" in the linker file for the default configuration, which needs to be present in OCMRAM . If user provides custom board_cfg, then the data must be present on OCMRAM.
pInPrms | [IN] Pointer to #Sciclient_BoardCfgPrms_t . NULL results in default config. |