![]() |
PDK API Guide for J721E
|
Go to the source code of this file.
Data Structures | |
struct | tisci_msg_fwl_change_owner_info_req |
This file contains: More... | |
struct | tisci_msg_fwl_change_owner_info_resp |
Response for a change owner operation. More... | |
struct | tisci_msg_fwl_set_firewall_region_req |
Request for configuring the firewall permissions. More... | |
struct | tisci_msg_fwl_set_firewall_region_resp |
Response for configuring the firewall permissions. More... | |
struct | tisci_msg_fwl_get_firewall_region_req |
Request for retrieving the firewall permissions. More... | |
struct | tisci_msg_fwl_get_firewall_region_resp |
Response for retrieving the firewall permissions. More... | |
Functions | |
struct tisci_msg_fwl_change_owner_info_req | __attribute__ ((__packed__)) |
Variables | |
struct tisci_header | hdr |
uint16_t | fwl_id |
uint16_t | region |
uint8_t | owner_index |
uint8_t | owner_privid |
uint16_t | owner_permission_bits |
uint32_t | n_permission_regs |
uint32_t | control |
uint32_t | permissions [FWL_MAX_PRIVID_SLOTS] |
uint64_t | start_address |
uint64_t | end_address |
struct tisci_header hdr |
uint16_t fwl_id |
uint16_t region |
uint8_t owner_index |
uint8_t owner_privid |
uint16_t owner_permission_bits |
uint32_t n_permission_regs |
uint32_t control |
uint32_t permissions |
uint64_t start_address |
uint64_t end_address |