PDK API Guide for J721E
|
Go to the source code of this file.
Data Structures | |
struct | tisci_msg_set_device_req |
Set the desired state of the device. More... | |
struct | tisci_msg_set_device_resp |
Empty response for TISCI_MSG_SET_DEVICE. More... | |
struct | tisci_msg_get_device_req |
Request to get device based on id. More... | |
struct | tisci_msg_get_device_resp |
Response to get device request. More... | |
struct | tisci_msg_set_device_resets_req |
Set the desired state of the resets of a device. More... | |
struct | tisci_msg_set_device_resets_resp |
Empty response for TISCI_MSG_SET_DEVICE_RESETS. More... | |
struct | tisci_msg_device_drop_powerup_ref_req |
Drop any remaining powerup device references. More... | |
struct | tisci_msg_device_drop_powerup_ref_resp |
Empty response for TISCI_MSG_DEVICE_DROP_POWERUP_REF. More... | |
Macros | |
#define | TISCI_MSG_FLAG_DEVICE_WAKE_ENABLED TISCI_BIT(8) |
This file contains: More... | |
#define | TISCI_MSG_FLAG_DEVICE_RESET_ISO TISCI_BIT(9) |
#define | TISCI_MSG_FLAG_DEVICE_EXCLUSIVE TISCI_BIT(10) |
#define | TISCI_MSG_VALUE_DEVICE_SW_STATE_AUTO_OFF 0 |
#define | TISCI_MSG_VALUE_DEVICE_SW_STATE_RETENTION 1 |
#define | TISCI_MSG_VALUE_DEVICE_SW_STATE_ON 2 |
#define | TISCI_MSG_VALUE_DEVICE_HW_STATE_OFF 0 |
#define | TISCI_MSG_VALUE_DEVICE_HW_STATE_ON 1 |
#define | TISCI_MSG_VALUE_DEVICE_HW_STATE_TRANS 2 |
Functions | |
struct tisci_msg_set_device_req | __attribute__ ((__packed__)) |
Variables | |
struct tisci_header | hdr |
uint32_t | id |
uint32_t | reserved |
uint8_t | state |
uint32_t | context_loss_count |
uint32_t | resets |
uint8_t | programmed_state |
uint8_t | current_state |
struct tisci_header hdr |
uint32_t id |
uint32_t reserved |
uint8_t state |
uint32_t context_loss_count |
uint32_t resets |
uint8_t programmed_state |
uint8_t current_state |