PDK API Guide for J721E
|
Set the desired state of the resets of a device.
hdr | TISCI header. |
id | Indicates which device to modify |
resets | A bit field of resets for the device. The meaning, behavior, and usage of the reset flags are device specific. Altough the flags can be set independently of device state, the firmware will control when resets are actually set to insure compliance with the SoC specific reset requirements. |
Data Fields | |
struct tisci_header | hdr |
uint32_t | id |
uint32_t | resets |
struct tisci_header tisci_msg_set_device_resets_req::hdr |
uint32_t tisci_msg_set_device_resets_req::id |
uint32_t tisci_msg_set_device_resets_req::resets |