PDK API Guide for J721E
|
This file contains the definition of all the message IDs, message formats to be able to interact with the System Controller firmware for OTP Key programming.
Go to the source code of this file.
Functions | |
int32_t | Sciclient_otpProcessKeyCfg (uint32_t *otpKeyCfgAddr, uint32_t timeout, uint32_t *debug_response) |
Message to request a processor Provides a means for either the “recovery master” host or another host in the permitted access list to request for a physical processor control. More... | |