TI-RTOS Drivers
tidrivers_cc32xx_2_16_01_13
|
CCamera_Config | Camera Global configuration |
CCamera_FxnTable | The definition of a Camera function table that contains the required set of functions to control a specific Camera driver implementation |
CCamera_Params | Camera Parameters |
CCameraCC3200DMA_HWAttrs | CameraCC3200DMA Hardware attributes |
CCameraCC3200DMA_Object | CameraCC3200DMA Object |
CClockP_FreqHz | Frequency-in-hertz struct |
CClockP_Params | Basic ClockP Parameters |
CDIR | |
Cdiskio_fxns | |
CEMAC_Config | EMAC Global configuration |
CEMAC_FxnTable | EMAC Function table structure |
CFATFS | |
CFIL | |
CFILINFO | |
CGPIOCC3200_Config | GPIO device specific driver configuration structure |
CHwiP_Params | Basic HwiP Parameters |
CI2C_Config | I2C Global configuration |
CI2C_FxnTable | The definition of a I2C function table that contains the required set of functions to control a specific I2C driver implementation |
CI2C_Params | I2C Parameters |
CI2C_Transaction | I2C transaction |
CI2CCC3200_HWAttrs | I2CCC3200 Hardware attributes |
CI2CCC3200_Object | I2CCC3200 Object |
CI2S_BufDesc | I2S buffer descriptor for issue/reclaim mode |
CI2S_Config | I2S Global configuration |
CI2S_FxnTable | The definition of a I2S function table that contains the required set of functions to control a specific I2S driver implementation |
CI2S_Params | Basic I2S Parameters |
CI2SCC3200DMA_HWAttrs | I2SCC3200DMA Hardware attributes |
CI2SCC3200DMA_Object | I2SCC3200DMA Object |
CI2SCC3200DMA_SerialPinConfig | CC3200 Serial Pin Configuration |
CI2SCC3200DMA_SerialPinParams | CC3200 specific I2S Parameters |
CI2SCC3200DMA_SerialPinVars | I2SCC3200DMA Serial pin variables |
CList_Elem | |
CList_List | |
CMutexP_Params | Basic MutexP Parameters |
CNVS_Attrs | NVS attributes |
CNVS_Config | NVS Global configuration |
CNVS_FxnTable | The definition of an NVS function table that contains the required set of functions to control a specific NVS driver implementation |
CNVS_Params | NVS Parameters |
CNVSCC3200_CmdSetCopyBlockArgs | NVSCC3200 command structure for setting copy block |
CNVSCC3200_HWAttrs | NVSCC3200 attributes |
CNVSCC3200_Object | |
CPIN_State_s | Underlying data structure for type PIN_State |
CPower_NotifyObj | Power notify object structure |
CPowerCC3200_Config | Power global configuration |
CPowerCC3200_MCURegisters | MCU core registers that need to be save on entering LPDS |
CPowerCC3200_ModuleState | Internal module state |
CPowerCC3200_NVICRegisters | NVIC registers that need to be save on entering LPDS |
CPowerCC3200_SaveRegisters | Struct of context registers to save on entering LPDS |
CPowerCC3200_Wakeup | For wakeup from LPDS or shutdown configuration |
CPWM_Config | PWM Global configuration |
CPWM_FxnTable | The definition of a PWM function table that contains the required set of functions to control a specific PWM driver implementation |
CPWM_Params | PWM Parameters |
CPWMTimerCC3200_HWAttrs | PWMTimerCC3200 Hardware attributes |
CPWMTimerCC3200_Object | PWMTimerCC3200 Object |
CRingBuf_Object | |
CSDSPI_Config | SDSPI Global configuration |
CSDSPI_FxnTable | The definition of a SDSPI function table that contains the required set of functions to control a specific SDSPI driver implementation |
CSDSPI_Params | SDSPI Parameters |
CSDSPICC3200_HWAttrs | SDSPICC3200 Hardware attributes |
CSDSPICC3200_Object | SDSPICC3200 Object |
CSemaphoreP_Params | Basic SemaphoreP Parameters |
CSPI_Config | SPI Global configuration |
CSPI_FxnTable | The definition of a SPI function table that contains the required set of functions to control a specific SPI driver implementation |
CSPI_Params | SPI Parameters |
CSPI_Transaction | A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat frames are sent and received from the buffers pointed to txBuf and rxBuf. The arg variable is an user-definable argument which gets passed to the SPI_CallbackFxn when the SPI driver is in SPI_MODE_CALLBACK |
CSPICC3200DMA_HWAttrs | SPICC3200DMA Hardware attributes |
CSPICC3200DMA_Object | SPICC3200DMA Object |
CUART_Config | UART Global configuration |
CUART_FxnTable | The definition of a UART function table that contains the required set of functions to control a specific UART driver implementation |
CUART_Params | UART Parameters |
CUARTCC3200_FxnSet | Complement set of read functions to be used by the UART ISR and UARTCC3200_read(). Internal use only |
CUARTCC3200_HWAttrs | UARTCC3200 Hardware attributes |
CUARTCC3200_Object | UARTCC3200 Object |
CUARTCC3200DMA_HWAttrs | UARTCC3200DMA Hardware attributes |
CUARTCC3200DMA_Object | UARTCC3200DMA Object |
CUSBMSCHFatFs_Config | USBMSCHFatFs Global configuration |
CUSBMSCHFatFs_FxnTable | The definition of a USBMSCHFatFs function table that contains the required set of functions to control a specific USBMSCHFatFs driver implementation |
CUSBMSCHFatFs_Params | USBMSCHFatFs Parameters |
CWatchdog_Config | Watchdog Global configuration |
CWatchdog_FxnTable | The definition of a Watchdog function table that contains the required set of functions to control a specific Watchdog driver implementation |
CWatchdog_Params | Watchdog Parameters |
CWatchdogCC3200_HWAttrs | Watchdog hardware attributes for CC3200 |
CWatchdogCC3200_Object | Watchdog Object for CC3200 |
CWiFi_Config | WiFi Global configuration |
CWiFi_FxnTable | The definition of a WiFi function table that contains the required set of functions to control a specific WiFi driver implementation |
CWiFi_Params | WiFi Parameters |
CWiFiCC3200_HWAttrs | WiFiCC3200 Hardware attributes |
CWiFiCC3200_Object | WiFiCC3200 Object |