Engine_AlgDesc | Descriptor for an alg. This object can be passed to Engine_addAlg() , to dynamically add an alg to an engine |
Engine_AlgInfo | Properties of an Engine algorithm |
Engine_AlgInfo2 | Properties of an Engine algorithm |
Engine_Attrs | Attributes of an Engine |
Engine_Desc | This structure is passed to Engine_add() , and contains parameters to specify an engine |
Engine_DllAlgDesc | Descriptor for a dynamically loaded alg. A dynamic library for a codec must export a function that fills in a structure of this type |
IALG_Fxns | Defines the fields and methods that must be supplied by all XDAIS algorithms |
IALG_MemRec | Memory records |
IALG_Obj | Algorithm instance object definition |
IALG_Params | Algorithm instance creation parameters |
IALG_Status | Pointer to algorithm specific status structure |
IAUDDEC1_DynamicParams | This structure defines the codec parameters that can be modified after creation via control() calls |
IAUDDEC1_Fxns | Defines all of the operations on IAUDDEC1 objects |
IAUDDEC1_InArgs | Defines the input arguments for all IAUDDEC1 instance process function |
IAUDDEC1_Obj | This must be the first field of all IAUDDEC1 instance objects |
IAUDDEC1_OutArgs | Defines the run time output arguments for all IAUDDEC1 instance objects |
IAUDDEC1_Params | Defines the creation time parameters for all IAUDDEC1 instance objects |
IAUDDEC1_Status | Defines instance status parameters (read-only) |
IAUDDEC_DynamicParams | This structure defines the codec parameters that can be modified after creation via control() calls |
IAUDDEC_Fxns | Defines all of the operations on IAUDDEC objects |
IAUDDEC_InArgs | Defines the input arguments for all IAUDDEC instance process function |
IAUDDEC_Obj | This must be the first field of all IAUDDEC instance objects |
IAUDDEC_OutArgs | Defines the run time output arguments for all IAUDDEC instance objects |
IAUDDEC_Params | Defines the creation time parameters for all IAUDDEC instance objects |
IAUDDEC_Status | Defines instance status parameters (read-only) |
IAUDENC1_DynamicParams | This structure defines the algorithm parameters that can be modified after creation via control() calls |
IAUDENC1_Fxns | Defines all of the operations on IAUDENC1 objects |
IAUDENC1_InArgs | Defines the input arguments for all IAUDENC1 instance process function |
IAUDENC1_Obj | This must be the first field of all IAUDENC1 instance objects |
IAUDENC1_OutArgs | Defines the run time output arguments for all IAUDENC1 instance objects |
IAUDENC1_Params | Defines the creation time parameters for all IAUDENC1 instance objects |
IAUDENC1_Status | Defines instance status parameters (read-only) |
IAUDENC_DynamicParams | This structure defines the algorithm parameters that can be modified after creation via control() calls |
IAUDENC_Fxns | Defines all of the operations on IAUDENC objects |
IAUDENC_InArgs | Defines the input arguments for all IAUDENC instance process function |
IAUDENC_Obj | This must be the first field of all IAUDENC instance objects |
IAUDENC_OutArgs | Defines the run time output arguments for all IAUDENC instance objects |
IAUDENC_Params | Defines the creation time parameters for all IAUDENC instance objects |
IAUDENC_Status | Defines instance status parameters (read-only) |
IIMGDEC1_CodecClassConfig | Definition of IIMGDEC1 codec class configurable parameters |
IIMGDEC1_DynamicParams | This structure defines the codec parameters that can be modified after creation via control() calls |
IIMGDEC1_Fxns | Defines all of the operations on IIMGDEC1 objects |
IIMGDEC1_InArgs | Defines the input arguments for all IIMGDEC1 instance process() function |
IIMGDEC1_Obj | This must be the first field of all IIMGDEC1 instance objects |
IIMGDEC1_OutArgs | Defines the run time output arguments for all IIMGDEC1 instance objects |
IIMGDEC1_Params | Defines the creation time parameters for all IIMGDEC1 instance objects |
IIMGDEC1_Status | Defines instance status parameters |
IIMGDEC_CodecClassConfig | Definition of IIMGDEC codec class configurable parameters |
IIMGDEC_DynamicParams | This structure defines the codec parameters that can be modified after creation via control() calls |
IIMGDEC_Fxns | Defines all of the operations on IIMGDEC objects |
IIMGDEC_InArgs | Defines the input arguments for all IIMGDEC instance process() function |
IIMGDEC_Obj | This must be the first field of all IIMGDEC instance objects |
IIMGDEC_OutArgs | Defines the run time output arguments for all IIMGDEC instance objects |
IIMGDEC_Params | Defines the creation time parameters for all IIMGDEC instance objects |
IIMGDEC_Status | Defines instance status parameters (read-only) |
IIMGENC1_CodecClassConfig | Definition of IIMGENC1 codec class configurable parameters |
IIMGENC1_DynamicParams | This structure defines the algorithm parameters that can be modified after creation via control() calls |
IIMGENC1_Fxns | Defines all of the operations on IIMGENC1 objects |
IIMGENC1_InArgs | Defines the input arguments for all IIMGENC1 instance process() function |
IIMGENC1_Obj | This must be the first field of all IIMGENC1 instance objects |
IIMGENC1_OutArgs | Defines the run time output arguments for all IIMGENC1 instance objects |
IIMGENC1_Params | Defines the creation time parameters for all IIMGENC1 instance objects |
IIMGENC1_Status | Defines instance status parameters |
IIMGENC_CodecClassConfig | Definition of IIMGENC codec class configurable parameters |
IIMGENC_DynamicParams | This structure defines the algorithm parameters that can be modified after creation via control() calls |
IIMGENC_Fxns | Defines all of the operations on IIMGENC objects |
IIMGENC_InArgs | Defines the input arguments for all IIMGENC instance process() function |
IIMGENC_Obj | This must be the first field of all IIMGENC instance objects |
IIMGENC_OutArgs | Defines the run time output arguments for all IIMGENC instance objects |
IIMGENC_Params | Defines the creation time parameters for all IIMGENC instance objects |
IIMGENC_Status | Defines instance status parameters (read-only) |
ISPHDEC1_DynamicParams | This structure defines the codec parameters that can be modified after creation via ISPHDEC1_Fxns.control() |
ISPHDEC1_Fxns | Defines all of the operations on ISPHDEC1 objects |
ISPHDEC1_InArgs | Defines the input arguments for all ISPHDEC1 instance process function |
ISPHDEC1_Obj | This must be the first field of all ISPHDEC1 instance objects |
ISPHDEC1_OutArgs | Defines the run time output arguments for all ISPHDEC1 instance objects |
ISPHDEC1_Params | Defines the creation time parameters for all ISPHDEC1 instance objects |
ISPHDEC1_Status | Defines instance status parameters |
ISPHDEC_DynamicParams | This structure defines the codec parameters that can be modified after creation via control() calls |
ISPHDEC_Fxns | Defines all of the operations on ISPHDEC objects |
ISPHDEC_InArgs | Defines the input arguments for all ISPHDEC instance process function |
ISPHDEC_Obj | This must be the first field of all ISPHDEC instance objects |
ISPHDEC_OutArgs | Defines the run time output arguments for all ISPHDEC instance objects |
ISPHDEC_Params | Defines the creation time parameters for all ISPHDEC instance objects |
ISPHDEC_Status | Defines instance status parameters (read-only) |
ISPHENC1_DynamicParams | This structure defines the codec parameters that can be modified after creation via ISPHENC1_Fxns.control() |
ISPHENC1_Fxns | Defines all of the operations on ISPHENC1 objects |
ISPHENC1_InArgs | Defines the input arguments for all ISPHENC1 instance process function |
ISPHENC1_Obj | This must be the first field of all ISPHENC1 instance objects |
ISPHENC1_OutArgs | Defines the run time output arguments for all ISPHENC1 instance objects |
ISPHENC1_Params | Defines the creation time parameters for all ISPHENC1 instance objects |
ISPHENC1_Status | Defines instance status parameters |
ISPHENC_DynamicParams | This structure defines the codec parameters that can be modified after creation via control() calls |
ISPHENC_Fxns | Defines all of the operations on ISPHENC objects |
ISPHENC_InArgs | Defines the input arguments for all ISPHENC instance process function |
ISPHENC_Obj | This must be the first field of all ISPHENC instance objects |
ISPHENC_OutArgs | Defines the run time output arguments for all ISPHENC instance objects |
ISPHENC_Params | Defines the creation time parameters for all ISPHENC instance objects |
ISPHENC_Status | Defines instance status parameters (read-only) |
IUNIVERSAL_CodecClassConfig | Definition of IUNIVERSAL codec class configurable parameters |
IUNIVERSAL_DynamicParams | This structure defines the codec parameters that can be modified after creation via control() calls |
IUNIVERSAL_Fxns | Defines all of the operations on IUNIVERSAL objects |
IUNIVERSAL_InArgs | Defines the input arguments for all IUNIVERSAL instance process function |
IUNIVERSAL_Obj | This must be the first field of all IUNIVERSAL instance objects |
IUNIVERSAL_OutArgs | Defines the run time output arguments for all IUNIVERSAL instance objects |
IUNIVERSAL_Params | Defines the creation time parameters for all IUNIVERSAL instance objects |
IUNIVERSAL_Status | Defines instance status parameters (read-only) |
IVIDANALYTICS_DynamicParams | This structure defines the algorithm parameters that can be modified after creation via control() calls |
IVIDANALYTICS_Fxns | Defines all of the operations on IVIDANALYTICS objects |
IVIDANALYTICS_Grid | Access modes used to declare how the algorithm accessed buffers |
IVIDANALYTICS_InArgs | Defines the input arguments for all IVIDANALYTICS instance process function |
IVIDANALYTICS_Obj | This must be the first field of all IVIDANALYTICS instance objects |
IVIDANALYTICS_OutArgs | Defines the run time output arguments for all IVIDANALYTICS instance objects |
IVIDANALYTICS_Params | Defines the creation time parameters for all IVIDANALYTICS instance objects |
IVIDANALYTICS_Rule | Analytics rule |
IVIDANALYTICS_Status | Defines instance status parameters |
IVIDDEC1_CodecClassConfig | Definition of IVIDDEC1 codec class configurable parameters |
IVIDDEC1_DynamicParams | This structure defines the codec parameters that can be modified after creation via control() calls |
IVIDDEC1_Fxns | Defines all of the operations on IVIDDEC1 objects |
IVIDDEC1_InArgs | Defines the input arguments for all IVIDDEC1 instance process function |
IVIDDEC1_Obj | This must be the first field of all IVIDDEC1 instance objects |
IVIDDEC1_OutArgs | Defines the run time output arguments for all IVIDDEC1 instance objects |
IVIDDEC1_Params | Defines the creation time parameters for all IVIDDEC1 instance objects |
IVIDDEC1_Status | Defines instance status parameters |
IVIDDEC2_CodecClassConfig | Definition of IVIDDEC2 codec class configurable parameters |
IVIDDEC2_DynamicParams | This structure defines the codec parameters that can be modified after creation via control() calls |
IVIDDEC2_Fxns | Defines all of the operations on IVIDDEC2 objects |
IVIDDEC2_InArgs | Defines the input arguments for all IVIDDEC2 instance process function |
IVIDDEC2_Obj | This must be the first field of all IVIDDEC2 instance objects |
IVIDDEC2_OutArgs | Defines the run time output arguments for all IVIDDEC2 instance objects |
IVIDDEC2_Params | Defines the creation time parameters for all IVIDDEC2 instance objects |
IVIDDEC2_Status | Defines instance status parameters |
IVIDDEC2BACK_CodecClassConfig | Definition of IVIDDEC2BACK codec class configurable parameters |
IVIDDEC2BACK_Fxns | Defines all of the operations on IVIDDEC2BACK objects |
IVIDDEC2BACK_Obj | This must be the first field of all IVIDDEC2BACK instance objects |
IVIDDEC2FRONT_Fxns | Defines all of the operations on IVIDDEC2FRONT objects |
IVIDDEC2FRONT_Obj | This must be the first field of all IVIDDEC2FRONT instance objects |
IVIDDEC2FRONT_OutArgs | Defines the run time output arguments for all IVIDDEC2FRONT instance objects |
IVIDDEC2FRONT_Status | Defines instance status parameters |
IVIDDEC3_CodecClassConfig | Definition of IVIDDEC3 codec class configurable parameters |
IVIDDEC3_DynamicParams | This structure defines the algorithm parameters that can be modified after creation via IVIDDEC3_Fxns.control() calls |
IVIDDEC3_Fxns | Defines all of the operations on IVIDDEC3 objects |
IVIDDEC3_InArgs | Defines the input arguments for all IVIDDEC3 instance process function |
IVIDDEC3_Obj | This must be the first field of all IVIDDEC3 instance objects |
IVIDDEC3_OutArgs | Defines the run time output arguments for all IVIDDEC3 instance objects |
IVIDDEC3_Params | Defines the creation time parameters for all IVIDDEC3 instance objects |
IVIDDEC3_Status | Defines instance status parameters |
IVIDDEC_CodecClassConfig | Definition of VIDDEC codec class configurable parameters |
IVIDDEC_DynamicParams | This structure defines the codec parameters that can be modified after creation via control() calls |
IVIDDEC_Fxns | Defines all of the operations on IVIDDEC objects |
IVIDDEC_InArgs | Defines the input arguments for all IVIDDEC instance process function |
IVIDDEC_Obj | This must be the first field of all IVIDDEC instance objects |
IVIDDEC_OutArgs | Defines the run time output arguments for all IVIDDEC instance objects |
IVIDDEC_Params | Defines the creation time parameters for all IVIDDEC instance objects |
IVIDDEC_Status | Defines instance status parameters |
IVIDENC1_CodecClassConfig | Definition of IVIDENC1 codec class configurable parameters |
IVIDENC1_DynamicParams | This structure defines the algorithm parameters that can be modified after creation via control() calls |
IVIDENC1_Fxns | Defines all of the operations on IVIDENC1 objects |
IVIDENC1_InArgs | Defines the input arguments for all IVIDENC1 instance process function |
IVIDENC1_MbData | Defines the structure that contains macroblock related encoding parameter estimates |
IVIDENC1_Obj | This must be the first field of all IVIDENC1 instance objects |
IVIDENC1_OutArgs | Defines the run time output arguments for all IVIDENC1 instance objects |
IVIDENC1_Params | Defines the creation time parameters for all IVIDENC1 instance objects |
IVIDENC1_Status | Defines instance status parameters |
IVIDENC2_CodecClassConfig | Definition of IVIDENC2 codec class configurable parameters |
IVIDENC2_DynamicParams | This structure defines the algorithm parameters that can be modified after creation via control() calls |
IVIDENC2_Fxns | Defines all of the operations on IVIDENC2 objects |
IVIDENC2_InArgs | Defines the input arguments for all IVIDENC2 instance process function |
IVIDENC2_Obj | This must be the first field of all IVIDENC2 instance objects |
IVIDENC2_OutArgs | Defines the run time output arguments for all IVIDENC2 instance objects |
IVIDENC2_Params | Defines the creation time parameters for all IVIDENC2 instance objects |
IVIDENC2_Status | Defines instance status parameters |
IVIDENC_CodecClassConfig | Definition of IVIDENC codec class configurable parameters |
IVIDENC_DynamicParams | This structure defines the codec parameters that can be modified after creation via control() calls |
IVIDENC_Fxns | Defines all of the operations on IVIDENC objects |
IVIDENC_InArgs | Defines the input arguments for all IVIDENC instance process function |
IVIDENC_Obj | This must be the first field of all IVIDENC instance objects |
IVIDENC_OutArgs | Defines the run time output arguments for all IVIDENC instance objects |
IVIDENC_Params | Defines the creation time parameters for all IVIDENC instance objects |
IVIDENC_Status | Defines instance status parameters (read-only) |
IVIDEO1_BufDesc | Detailed buffer descriptor for video buffers |
IVIDEO1_BufDescIn | Buffer descriptor for input video buffers |
IVIDEO2_BufDesc | Detailed buffer descriptor for video buffers |
IVIDEO_BufDesc | Buffer descriptor for video buffers |
IVIDTRANSCODE_DynamicParams | This structure defines the codec parameters that can be modified after creation via control() calls |
IVIDTRANSCODE_Fxns | Defines all of the operations on IVIDTRANSCODE objects |
IVIDTRANSCODE_InArgs | Defines the input arguments for all IVIDTRANSCODE instance process function |
IVIDTRANSCODE_Obj | This must be the first field of all IVIDTRANSCODE instance objects |
IVIDTRANSCODE_OutArgs | Defines the run time output arguments for all IVIDTRANSCODE instance objects |
IVIDTRANSCODE_Params | Defines the creation time parameters for all IVIDTRANSCODE instance objects |
IVIDTRANSCODE_Status | Defines instance status parameters |
Server_MemStat | Information for a memory heap of a remote DSP server |
ti_sdo_ce_osal_Memory_AllocParams | Parameters for ti_sdo_ce_osal_Memory_alloc() & ti_sdo_ce_osal_Memory_free() |
VISA_MsgHeader | VISA message header |
xdc_runtime_Memory_Stats | |
XDM1_AlgBufInfo | Buffer information descriptor for input and output buffers |
XDM1_BufDesc | Buffer descriptor |
XDM1_SingleBufDesc | Single buffer descriptor |
XDM2_BufDesc | Buffer descriptor |
XDM2_BufSize | Union describing a buffer size |
XDM2_SingleBufDesc | Single buffer descriptor |
XDM_AlgBufInfo | Buffer information descriptor for input and output buffers |
XDM_BufDesc | Buffer descriptor for multiple buffers |
XDM_Context | Context used by split codecs |
XDM_ContextInfo | Buffer information descriptor for input and output buffers |
XDM_DataSyncDesc | Descriptor for the chunk of data being transferred in one call to putData or getData |
XDM_Date | Date and time |
XDM_Point | 2-dimensional point |
XDM_Rect | Rectangle |
XDM_SingleBufDesc | Single buffer descriptor |